Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Update Library does NOT update schematic or board
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 188 subscribers
  • Views 2345 views
  • Users 0 members are here
Related

Update Library does NOT update schematic or board

e14 Contributor
e14 Contributor over 15 years ago

Update Library (specific) or Update All Libraries does not update

schematic or board with library changes.

The only work-around is to open the schematic and "pretend" to add the

revised component, acknowledge the "updated" messages, and then escape

(cancel) the addition.

This is unacceptable behavior.

Eagle should check for updated devices/packages whenever a board is

loaded and prompt for update or not.  And, Update Library should WORK!!!

 

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 15 years ago

    Am 18.05.2011 03:00, schrieb Marvin Dawson:

    Update Library (specific) or Update All Libraries does not update

    schematic or board with library changes.

    The only work-around is to open the schematic and "pretend" to add the

    revised component, acknowledge the "updated" messages, and then escape

    (cancel) the addition.

    This is unacceptable behavior.

    Eagle should check for updated devices/packages whenever a board is

    loaded and prompt for update or not. And, Update Library should WORK!!!

     

    Are you sure that you are editing the same library as you are using

    with the ADD command. Could there be two different versions of this

    library?

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Richard_H

    Richard Hammerl wrote:

    Am 18.05.2011 03:00, schrieb Marvin Dawson:

    >> Update Library (specific) or Update All Libraries does not update

    >> schematic or board with library changes.

    >> The only work-around is to open the schematic and "pretend" to add the

    >> revised component, acknowledge the "updated" messages, and then escape

    >> (cancel) the addition.

    >> This is unacceptable behavior.

    >> Eagle should check for updated devices/packages whenever a board is

    >> loaded and prompt for update or not. And, Update Library should WORK!!!

     

    Are you sure that you are editing the same library as you are using

    with the ADD command. Could there be two different versions of this

    library?

     

    Thanks, everyone for all the suggestions.

    There was only one (network) copy of the shared library.

    I believe that the problem was likely due to our naming the library with

    an @ sign at the beginning.  This was done in order to move it up

    towards the top of the library listings, making it easier to find.

    However, appending the @ sign to the beginning appears to have caused

    Eagle to not find or update the library.

    UPDATE @library_name or UPDATE ALL was probably looking for

    library_name, without the leading @ sign character.

    We have renamed our library with a leading 0 (zero) to hopefully resolve

    these problems.  Eagle should probably caution or not permit library

    names that begin with @ character.

    We have had similar problems when someone named a new device "NAME.DEV".

      Eagle appended .dev to it, resulting in "NAME.DEV.dev", and it was

    nearly impossible to correct.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Am 21.05.2011 19:18, schrieb Marvin Dawson:

    Richard Hammerl wrote:

    >> Am 18.05.2011 03:00, schrieb Marvin Dawson:

    >>> Update Library (specific) or Update All Libraries does not update

    >>> schematic or board with library changes.

    >>> The only work-around is to open the schematic and "pretend" to add the

    >>> revised component, acknowledge the "updated" messages, and then escape

    >>> (cancel) the addition.

    >>> This is unacceptable behavior.

    >>> Eagle should check for updated devices/packages whenever a board is

    >>> loaded and prompt for update or not. And, Update Library should WORK!!!

    >>

    >> Are you sure that you are editing the same library as you are using

    >> with the ADD command. Could there be two different versions of this

    >> library?

    >>

    Thanks, everyone for all the suggestions.

    There was only one (network) copy of the shared library.

    I believe that the problem was likely due to our naming the library with

    an @ sign at the beginning. This was done in order to move it up towards

    the top of the library listings, making it easier to find.

    However, appending the @ sign to the beginning appears to have caused

    Eagle to not find or update the library.

    UPDATE @library_name or UPDATE ALL was probably looking for

    library_name, without the leading @ sign character.

    We have renamed our library with a leading 0 (zero) to hopefully resolve

    these problems. Eagle should probably caution or not permit library

    names that begin with @ character.

    We have had similar problems when someone named a new device "NAME.DEV".

    Eagle appended .dev to it, resulting in "NAME.DEV.dev", and it was

    nearly impossible to correct.

     

    The library names must exactly match otherwise UPDATE does not work.

     

    In case you want to rename a device/package/symbol in a library you

    can use, for example, EXPORT SCRIPT to write the whole library file

    in a script file. Now you can edit it with a text editor and correct

    for example the name.

    After modifying and saving the script file, open a new lbr file and

    use SCRIPT to import the script file.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Am 21.05.2011 19:18, schrieb Marvin Dawson:

    Richard Hammerl wrote:

    >> Am 18.05.2011 03:00, schrieb Marvin Dawson:

    >>> Update Library (specific) or Update All Libraries does not update

    >>> schematic or board with library changes.

    >>> The only work-around is to open the schematic and "pretend" to add the

    >>> revised component, acknowledge the "updated" messages, and then escape

    >>> (cancel) the addition.

    >>> This is unacceptable behavior.

    >>> Eagle should check for updated devices/packages whenever a board is

    >>> loaded and prompt for update or not. And, Update Library should WORK!!!

    >>

    >> Are you sure that you are editing the same library as you are using

    >> with the ADD command. Could there be two different versions of this

    >> library?

    >>

    Thanks, everyone for all the suggestions.

    There was only one (network) copy of the shared library.

    I believe that the problem was likely due to our naming the library with

    an @ sign at the beginning. This was done in order to move it up towards

    the top of the library listings, making it easier to find.

    However, appending the @ sign to the beginning appears to have caused

    Eagle to not find or update the library.

    UPDATE @library_name or UPDATE ALL was probably looking for

    library_name, without the leading @ sign character.

    We have renamed our library with a leading 0 (zero) to hopefully resolve

    these problems. Eagle should probably caution or not permit library

    names that begin with @ character.

    We have had similar problems when someone named a new device "NAME.DEV".

    Eagle appended .dev to it, resulting in "NAME.DEV.dev", and it was

    nearly impossible to correct.

     

    The library names must exactly match otherwise UPDATE does not work.

     

    In case you want to rename a device/package/symbol in a library you

    can use, for example, EXPORT SCRIPT to write the whole library file

    in a script file. Now you can edit it with a text editor and correct

    for example the name.

    After modifying and saving the script file, open a new lbr file and

    use SCRIPT to import the script file.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm