Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Update Library does NOT update schematic or board
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 188 subscribers
  • Views 2335 views
  • Users 0 members are here
Related

Update Library does NOT update schematic or board

e14 Contributor
e14 Contributor over 15 years ago

Update Library (specific) or Update All Libraries does not update

schematic or board with library changes.

The only work-around is to open the schematic and "pretend" to add the

revised component, acknowledge the "updated" messages, and then escape

(cancel) the addition.

This is unacceptable behavior.

Eagle should check for updated devices/packages whenever a board is

loaded and prompt for update or not.  And, Update Library should WORK!!!

 

  • Sign in to reply
  • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Am 21.05.2011 19:18, schrieb Marvin Dawson:

    Richard Hammerl wrote:

    >> Am 18.05.2011 03:00, schrieb Marvin Dawson:

    >>> Update Library (specific) or Update All Libraries does not update

    >>> schematic or board with library changes.

    >>> The only work-around is to open the schematic and "pretend" to add the

    >>> revised component, acknowledge the "updated" messages, and then escape

    >>> (cancel) the addition.

    >>> This is unacceptable behavior.

    >>> Eagle should check for updated devices/packages whenever a board is

    >>> loaded and prompt for update or not. And, Update Library should WORK!!!

    >>

    >> Are you sure that you are editing the same library as you are using

    >> with the ADD command. Could there be two different versions of this

    >> library?

    >>

    Thanks, everyone for all the suggestions.

    There was only one (network) copy of the shared library.

    I believe that the problem was likely due to our naming the library with

    an @ sign at the beginning. This was done in order to move it up towards

    the top of the library listings, making it easier to find.

    However, appending the @ sign to the beginning appears to have caused

    Eagle to not find or update the library.

    UPDATE @library_name or UPDATE ALL was probably looking for

    library_name, without the leading @ sign character.

    We have renamed our library with a leading 0 (zero) to hopefully resolve

    these problems. Eagle should probably caution or not permit library

    names that begin with @ character.

    We have had similar problems when someone named a new device "NAME.DEV".

    Eagle appended .dev to it, resulting in "NAME.DEV.dev", and it was

    nearly impossible to correct.

     

    The library names must exactly match otherwise UPDATE does not work.

     

    In case you want to rename a device/package/symbol in a library you

    can use, for example, EXPORT SCRIPT to write the whole library file

    in a script file. Now you can edit it with a text editor and correct

    for example the name.

    After modifying and saving the script file, open a new lbr file and

    use SCRIPT to import the script file.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Richard_H

    Richard Hammerl wrote:

    Am 18.05.2011 03:00, schrieb Marvin Dawson:

    >> Update Library (specific) or Update All Libraries does not update

    >> schematic or board with library changes.

    >> The only work-around is to open the schematic and "pretend" to add the

    >> revised component, acknowledge the "updated" messages, and then escape

    >> (cancel) the addition.

    >> This is unacceptable behavior.

    >> Eagle should check for updated devices/packages whenever a board is

    >> loaded and prompt for update or not. And, Update Library should WORK!!!

     

    Are you sure that you are editing the same library as you are using

    with the ADD command. Could there be two different versions of this

    library?

     

    Thanks, everyone for all the suggestions.

    There was only one (network) copy of the shared library.

    I believe that the problem was likely due to our naming the library with

    an @ sign at the beginning.  This was done in order to move it up

    towards the top of the library listings, making it easier to find.

    However, appending the @ sign to the beginning appears to have caused

    Eagle to not find or update the library.

    UPDATE @library_name or UPDATE ALL was probably looking for

    library_name, without the leading @ sign character.

    We have renamed our library with a leading 0 (zero) to hopefully resolve

    these problems.  Eagle should probably caution or not permit library

    names that begin with @ character.

    We have had similar problems when someone named a new device "NAME.DEV".

      Eagle appended .dev to it, resulting in "NAME.DEV.dev", and it was

    nearly impossible to correct.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Richard_H

    On 5/19/2011 7:54 AM, Richard Hammerl wrote:

    Am 19.05.2011 13:16, schrieb Jim Littlefield:

    >> On 5/19/2011 3:39 AM, Richard Hammerl wrote:

    >>> Am 18.05.2011 19:44, schrieb Ing. J.M. Rafetseder:

    >>>> After editing did you: use *, enter (command line)? Editing takes the

    >>>> lbr out of use (grey dot), so an update seems not to work.

    >>>> r

    >>>

    >>> That's not the case. Editing a library does not mark it "not in use".

    >>> Could you check this please again as I can't reproduce this?

    >>>

    >>

    >> I have also seen this behavior (Editing a library seems to make it "not

    >> used") although it does not happen all the time. Using 5.10.

    >>

    >> Jim

    >>

    >

    Seems to be very srange, I never have seen this. But please keep an eye

    on this. Perhaps you can check out when this happens.....

     

     

    Thanks....I had always assumed (probably correctly) that I was doing

    something wrong.   Now that I know that at least one other user has seen

    the same sort of thing I will try to be more vigilant about what I can

    do to make it happen.   If I come up with a reproducible sequence of

    steps will let you know.

     

    Jim

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Richard_H

    Richard Hammerl wrote on Thu, 19 May 2011 03:39

    Am 18.05.2011 19:44, schrieb Ing. J.M. Rafetseder:

    After editing did you: use *, enter (command line)? Editing takes

    the

    lbr out of use (grey dot), so an update seems not to work.

    r

     

    That's not the case. Editing a library does not mark it "not in use".

    Could you check this please again as I can't reproduce this?

     

     

    I would agree with Richard, normally editing the library has no effect on

    the libraries that are being used.  I use only one library and edit it

    often.  Once the library is setup to be used I never have to touch that

    setting again.

     

    Maybe there's a bug somewhere, but this is not normal behaviour.  I've done

    more than 100 boards and never seen this.

     

    Cheers,

     

    James.

    --

    James Morrison  ~~~  Stratford Digital

     

    Specializing in CadSoft EAGLE

    • Online Sales to North America

    • Electronic Design Services

    • EAGLE Enterprise Toolkit

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Am 19.05.2011 13:16, schrieb Jim Littlefield:

    On 5/19/2011 3:39 AM, Richard Hammerl wrote:

    >> Am 18.05.2011 19:44, schrieb Ing. J.M. Rafetseder:

    >>> After editing did you: use *, enter (command line)? Editing takes the

    >>> lbr out of use (grey dot), so an update seems not to work.

    >>> r

    >>

    >> That's not the case. Editing a library does not mark it "not in use".

    >> Could you check this please again as I can't reproduce this?

    >>

    >

    I have also seen this behavior (Editing a library seems to make it "not

    used") although it does not happen all the time. Using 5.10.

     

    Jim

     

     

    Seems to be very srange, I never have seen this. But please keep an eye

    on this. Perhaps you can check out when this happens.....

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Richard_H

    On 5/19/2011 3:39 AM, Richard Hammerl wrote:

    Am 18.05.2011 19:44, schrieb Ing. J.M. Rafetseder:

    >> After editing did you: use *, enter (command line)? Editing takes the

    >> lbr out of use (grey dot), so an update seems not to work.

    >> r

     

    That's not the case. Editing a library does not mark it "not in use".

    Could you check this please again as I can't reproduce this?

     

     

    I have also seen this behavior (Editing a library seems to make it "not

    used") although it does not happen all the time.  Using 5.10.

     

    Jim

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago

    Am 18.05.2011 03:00, schrieb Marvin Dawson:

    Update Library (specific) or Update All Libraries does not update

    schematic or board with library changes.

    The only work-around is to open the schematic and "pretend" to add the

    revised component, acknowledge the "updated" messages, and then escape

    (cancel) the addition.

    This is unacceptable behavior.

    Eagle should check for updated devices/packages whenever a board is

    loaded and prompt for update or not. And, Update Library should WORK!!!

     

    Are you sure that you are editing the same library as you are using

    with the ADD command. Could there be two different versions of this

    library?

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Am 18.05.2011 19:44, schrieb Ing. J.M. Rafetseder:

    After editing did you: use *, enter (command line)? Editing takes the

    lbr out of use (grey dot), so an update seems not to work.

    r

     

    That's not the case. Editing a library does not mark it "not in use".

    Could you check this please again as I can't reproduce this?

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Ing. J.M. Rafetseder wrote:

    After editing did you: use *, enter (command line)? Editing takes the

    lbr out of use (grey dot), so an update seems not to work.

    r

    I will have to check, but why would editing the library mark it not for

    use?  Why would you want to edit a library and then not use it?

    Seems silly.

    We have most all of our devices in one library, so that they are easier

    to find and control, so we edit it a lot, and want the changes updated

    in the schematics and boards.

     

    Any suggestions to make the updates easier and prevent the library from

    being marked not for use?

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    After editing did you: use *, enter (command line)?  Editing takes the lbr

    out of use (grey dot), so an update seems not to work.

    r