Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Can someone please help me make a custom library componant ?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 188 subscribers
  • Views 1234 views
  • Users 0 members are here
  • custom
  • device
Related

Can someone please help me make a custom library componant ?

e14 Contributor
e14 Contributor over 15 years ago

I am not the greatest at building custom componants in eagle . Can someone please make me this componant i need . I am willing to pay if need be . The componant i need is a Sharp PQ12rd21 voltage regulator . It is a to-220.4 package . I need the whole device made which includes the package ,symbol and finished device . Iv tried a few times with no luck and have read several tutorials on making one .

 

Here is the datasheet for it with dimensions .

 

http://pdf1.alldatasheet.com/datasheet-pdf/view/43421/SHARP/PQ12RD21.html

 

 

If you can make one package with the mounting hole and another with just the pins that would be great .

 

Thanks in advance .

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi Chris,

     

    Are you sure you want to use that part, its seems a bit old? 1996?

     

    It also is OBSOLETE according to mouser?

     

    Are you already "Committed" to using this part?

     

    What I suggest is just start with a 3 pin regulator( in the library , look

    for "TO-220" , and save that part as your device, then just duplicate one

    of the pins/pads in the package,

     

    Add an extra pin in the symbol for the on/off switch, then connect it.

     

    If you are not committed to that part, then look for something more

    "POPULAR" and more than likely you will find a suitable part in the

    library,

     

    Do you need the ON OFF Switch?

     

    Remember that you don't need an "exact" matching part number, you will just

    need the correct SYMBOL & FOOTPRINT( package ) to make up your device.

     

    I also suggest to have a go, cause if you don't learn it now , when are you

    going to?

     

    Dave M

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi Chris,

     

    Are you sure you want to use that part, its seems a bit old? 1996?

     

    It also is OBSOLETE according to mouser?

     

    Are you already "Committed" to using this part?

     

    What I suggest is just start with a 3 pin regulator( in the library , look

    for "TO-220" , and save that part as your device, then just duplicate one

    of the pins/pads in the package,

     

    Add an extra pin in the symbol for the on/off switch, then connect it.

     

    If you are not committed to that part, then look for something more

    "POPULAR" and more than likely you will find a suitable part in the

    library,

     

    Do you need the ON OFF Switch?

     

    Remember that you don't need an "exact" matching part number, you will just

    need the correct SYMBOL & FOOTPRINT( package ) to make up your device.

     

    I also suggest to have a go, cause if you don't learn it now , when are you

    going to?

     

    Dave M

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.