Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Can someone please help me make a custom library componant ?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 188 subscribers
  • Views 1213 views
  • Users 0 members are here
  • custom
  • device
Related

Can someone please help me make a custom library componant ?

e14 Contributor
e14 Contributor over 14 years ago

I am not the greatest at building custom componants in eagle . Can someone please make me this componant i need . I am willing to pay if need be . The componant i need is a Sharp PQ12rd21 voltage regulator . It is a to-220.4 package . I need the whole device made which includes the package ,symbol and finished device . Iv tried a few times with no luck and have read several tutorials on making one .

 

Here is the datasheet for it with dimensions .

 

http://pdf1.alldatasheet.com/datasheet-pdf/view/43421/SHARP/PQ12RD21.html

 

 

If you can make one package with the mounting hole and another with just the pins that would be great .

 

Thanks in advance .

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 09/07/2011 06:30 AM, chris nisbett wrote:

    Attachment ? Im not seeing it . So your basically saying just draw a

    wire on the brestrict layer through the middle of the smd pads ?

     

    Yep... Exactly.

     

    The snapshot was in the message.  It's even attached to the message I

    got back.  Some problems have been reported regarding attachments when

    you're using the web interface.  If you use the NNTP news groups, all

    works well.

     

       - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Attachment ? Im not seeing it . So your basically saying just draw a wire on the brestrict layer through the middle of the smd pads ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 09/04/2011 06:10 AM, Maciej Kucia wrote:

    You can draw rect on bRestrict (or tRestrict for top) layer to keep plane away.

     

     

    You don't even need a rectangle.  All you need is a wire on the

    appropriate restrict layer.  In the attached snapshot, the polygon has

    an isolate value of 25 mils and the bRestrict wire is .15 mm wide.  The

    distance between the edge of the restrict wire and the pad is about 21.6

    mils which is less than the isolate value of the enclosing polygon.

     

    Enjoy,

        - Chuck

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Sweet . Thank a bunch .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    You can draw rect on bRestrict (or tRestrict for top) layer to keep plane away.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    One more question . I am trying to do a ground copper pour on the bottom side with polygon but having a problem . The problem is i have 1206 smd componants and the copper pour is going through the middle of the 1206 pad . The only way i can get the copper pour to stay out of the middle of the smd's is set the isolate to above 40mil . Is there a way i can just i can just keep out the pour over those specific smd's and be able to set the isolate back down to around 12mil ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks i got it to work . Now how do i delete all the bad ones and the extra list of vregs in that folder ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Am 03.09.2011 10:30, schrieb chris nisbett:

    I have tried a few times now and i got the package and symbol built and connected them but when i save it saves as like a library folder somehow and contains like a bunch of other regs . It shows up in the control panel but when i go to use it its not on the list . Somethings very weird . I dont know what im doing wrong but i spent the last 6 hours trying to get it but cant . I have 3 different ones now but none will work .

     

     

    Seems that you must put your library "IN USE" by clicking the use icon

    on the very top of the screen and then select your library.

    If you see your library in the control panel you can activate it by

    clicking the little Dot "O" between the library name and the

    description. It will become green  image

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    chris nisbett wrote on Sat, 03 September 2011 15:15

    Yes i am commited to the part . Its one of the best regs iv ever used

    and have several thousand on hand as well as use them on almost

    everything .

     

     

     

    Hi Chris,

     

    Well thats committed alright,!!!

     

    Ok,

     

    So firstly

     

    Q1) Do you have your OWN library set up. If Not, I suggested that you do

    that and start putting your own parts in there!

     

    Now, follow some of the video tutorials there are a few details which is

    easier to watch than to explain.

     

    I went through the same pain of creating parts myself, and I can tell you,

    its not the actual DRAWING of the parts thats difficult, its the stupid

    navigation ( or lack of ) thats the issue its really *** to be honest.!

     

    For a start, when you view the Symbols or packages in a library , you only

    get a list of part numbers, you don' get a preview, so this is an issue.

     

    Also, it would be handy to have a forward and back button on the library

    editor, as its too easy to get lost. (I guess I could code this up myself

    and add some buttons to the toolbar)

     

    This library editor needs improvement but for now you just have to put up

    with it.

     

    As I stated earlier , try to find a part that close as possible to what you

    want, then copy the SYMBOL, and the PACKAGE separately, ( using GROUP, CUT

    and PASTE commands) and put this into your own library, if you copy a part

    from another library, you will get all the parts, which is annoying.

     

    there are some pertty bad videos on the cadsoft website.

     

    Dave M

     

     

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    I have tried a few times now and i got the package and symbol built and connected them but when i save it saves as like a library folder somehow and contains like a bunch of other regs . It shows up in the control panel but when i go to use it its not on the list . Somethings very weird . I dont know what im doing wrong but i spent the last 6 hours trying to get it but cant . I have 3 different ones now but none will work .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>