Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) DRC rules for specific board area or chip
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 189 subscribers
  • Views 466 views
  • Users 0 members are here
Related

DRC rules for specific board area or chip

cosborne2000
cosborne2000 over 14 years ago

Is there any way to create different DRC rules for specific areas or chips on a board?

 

For example, I would like to setup a large width on the ground net but this trace needs to neck down to connect to various chips.

Fine pitch devices also require a narrow trace width to connect.

 

Currently I have to approve all the errors on the fine pitch devices but is there a more efficient way?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    cosborne2000 <communitymanager@premierfarnell.com> wrote:

    Is there any way to create different DRC rules for specific areas or chips on a board?

     

    For example, I would like to setup a large width on the ground net but

    this trace needs to neck down to connect to various chips.

    Fine pitch devices also require a narrow trace width to connect.

     

    Currently I have to approve all the errors on the fine pitch devices but

    is there a more efficient way?

     

     

    Have a look at classes.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cosborne2000
    cosborne2000 over 14 years ago in reply to e14 Contributor

    Maybe there's a section I'm missing.

     

    For example: I want a 12 width/12 clearance rule for the GND net but I need an exception for the neck down on fine pitch or BGA packages.

    Is there any way I can avoid all the DRC errors that occur at the chip?

    If I set for the tighter rules for the chip then this rule applies to the whole board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to cosborne2000

    cosborne2000 schrieb:

     

    For example: I want a 12 width/12 clearance rule for the GND net but

    I need an exception for the neck down on fine pitch or BGA packages.

    Is there any way I can avoid all the DRC errors that occur at the

    chip? If I set for the tighter rules for the chip then this rule

    applies to the whole board.

     

    "Exceptions" from the DRC settings are currently not supported/possible

    with EAGLE.

     

    In such situations, I normally use the coarser DRC settings for the

    board and then "accept" all DRC complaints in the fine pitch area since

    I know it's OK there. (To be sure, you yould run a "finepitch" DRC before.)

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cosborne2000
    cosborne2000 over 14 years ago in reply to e14 Contributor

    Any idea if V6 will handle neck downs?

     

    With fine pitch high pin count chips you can have a long list of exceptions.  It wouldn't be a big deal but if I make any type of adjustment to the chip position the DRC exceptions don't follow.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • cosborne2000
    cosborne2000 over 14 years ago in reply to e14 Contributor

    Any idea if V6 will handle neck downs?

     

    With fine pitch high pin count chips you can have a long list of exceptions.  It wouldn't be a big deal but if I make any type of adjustment to the chip position the DRC exceptions don't follow.