Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Is it possible?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 188 subscribers
  • Views 715 views
  • Users 0 members are here
Related

Is it possible?

e14 Contributor
e14 Contributor over 14 years ago

Good Evening Everyone,

 

I drew a simple schematic with standard LM317T power supply, a 20-pin encoder chip and a 5 pin Receiver chip. I admit I used the auto route feature (trying to save time) and converted it to a board as usual. I went ahead and made my pcb only to find that the routing was completed incorrectly!

One of the nets went directly from one pin on the encoder to one pin on the Receiver chip. I rechecked by schematic. The board should connect these two pins, but instead it goes to a completely different pin on the Rx. Also, my schematic shows clearly that pin #2 should have no connection made to it at all, but there is a connecting net to pin #2, while pin #3 is left unconnected on the board. I have checked and there are no jumper wires I am over looking. It seems to me that the program V5.11.0 just didn't convert it correctly. Is this possible.

Thanks,

 

Jeff

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Am 05.12.2011 02:56, schrieb Jeff Morrissey:

    Good Evening Everyone,

     

    I drew a simple schematic with standard LM317T power supply, a 20-pin encoder chip and a 5 pin Receiver chip. I admit I used the auto route feature (trying to save time) and converted it to a board as usual. I went ahead and made my pcb only to find that the routing was completed incorrectly!

    One of the nets went directly from one pin on the encoder to one pin on the Receiver chip. I rechecked by schematic. The board should connect these two pins, but instead it goes to a completely different pin on the Rx. Also, my schematic shows clearly that pin #2 should have no connection made to it at all, but there is a connecting net to pin #2, while pin #3 is left unconnected on the board. I have checked and there are no jumper wires I am over looking. It seems to me that the program V5.11.0 just didn't convert it correctly. Is this possible.

    Thanks,

     

    Jeff

     

    Zip the files and post them here. With your explanaination nobody can

    follow what actually happened.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    Am 05.12.2011 02:56, schrieb Jeff Morrissey:

    Good Evening Everyone,

     

    I drew a simple schematic with standard LM317T power supply, a 20-pin encoder chip and a 5 pin Receiver chip. I admit I used the auto route feature (trying to save time) and converted it to a board as usual. I went ahead and made my pcb only to find that the routing was completed incorrectly!

    One of the nets went directly from one pin on the encoder to one pin on the Receiver chip. I rechecked by schematic. The board should connect these two pins, but instead it goes to a completely different pin on the Rx. Also, my schematic shows clearly that pin #2 should have no connection made to it at all, but there is a connecting net to pin #2, while pin #3 is left unconnected on the board. I have checked and there are no jumper wires I am over looking. It seems to me that the program V5.11.0 just didn't convert it correctly. Is this possible.

    Thanks,

     

    Jeff

     

    Zip the files and post them here. With your explanaination nobody can

    follow what actually happened.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Joern,

    I managed to Zip the sch. file and board file with the WinZip program, but the program is asking me what http address to send it to. I don't know exactly what that address is. Might you tell me?

    Thanks,

     

    Jeff