Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Is there any problems with this board?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 189 subscribers
  • Views 532 views
  • Users 0 members are here
Related

Is there any problems with this board?

e14 Contributor
e14 Contributor over 14 years ago

This is my first board.  I did some research on using eaglecad and used what i learned from the tutorials to put in this design.  Is there anything that stands out that might not work ? The circuit will operate at 5 volts.  The maximum current is about 700mA.

 

Thanks,

 

Jake

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hi Jake,

     

    At first sight, it seems to me that there is a clearance problem below 2nd chip on top, from left. Two vias are overlapping each other.

     

    You shell use various built-in checks (ERC, DRC) to find basic errors in your design.

     

    I'd guess that you're not dealing with high frequency signals, so you are very free to use much wider traces (and also keep your traces paths, which are not optimal now). My suggestion would definitelly be to make your traces wider.

     

     

    Your question is very simple (and general), but any short answer might be misleading... For example, minimum traces width is related also to base material (laminate) used during PCB production - eg. standard copper layout thickness is 70 or 35 microns.

    Furthermore, temperature is also a variable in this calculation, so, your working environment might request increased minimum traces width.

     

     

    I was lucky to find a great book years ago, when I started with PCBs design. It's title is "High Speed Digital Design: A Handbook Of Black Magic". Highly recommended ! It includes various easy to follow practical guidelines.

    After reading this book, you will most likely route your PCBs by hand, without any autorouter...  ;-)

     

     

    Good luck,  Ivan.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hi Jake,

     

    At first sight, it seems to me that there is a clearance problem below 2nd chip on top, from left. Two vias are overlapping each other.

     

    You shell use various built-in checks (ERC, DRC) to find basic errors in your design.

     

    I'd guess that you're not dealing with high frequency signals, so you are very free to use much wider traces (and also keep your traces paths, which are not optimal now). My suggestion would definitelly be to make your traces wider.

     

     

    Your question is very simple (and general), but any short answer might be misleading... For example, minimum traces width is related also to base material (laminate) used during PCB production - eg. standard copper layout thickness is 70 or 35 microns.

    Furthermore, temperature is also a variable in this calculation, so, your working environment might request increased minimum traces width.

     

     

    I was lucky to find a great book years ago, when I started with PCBs design. It's title is "High Speed Digital Design: A Handbook Of Black Magic". Highly recommended ! It includes various easy to follow practical guidelines.

    After reading this book, you will most likely route your PCBs by hand, without any autorouter...  ;-)

     

     

    Good luck,  Ivan.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Ivan,

     

    Thank you for your input! It's appreciated.  I have already submitted my gerber files to the board house so it's too late for me to make modifications.  Like i said this is my first time.  If there is anything wrong it's going to be a learning expeirence.  Also a 110$ mistake >_< .  I think i am going to researsh the book u suggest, I need help image

     

    Thanks again,

     

    Jake