Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) embedding version control information in schematic and board
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 190 subscribers
  • Views 1009 views
  • Users 0 members are here
Related

embedding version control information in schematic and board

e14 Contributor
e14 Contributor over 13 years ago

hi all,

 

after I've finally upgraded to eagle 6, I'm now experimenting with

putting my eagle files under version control (subversion in my case).

 

One of subversions features is putting revision information into the

files by keyword expansion.

As eagle now uses XML formatted files this now works without problems.

 

Just put for instance "$URL:$" or "$Revision:$" into a text and

subversion will replace it with "$URL: ULP ulp-name ulp-parameters ..."

 

Both solution would solve my immediate needs.

 

 

What do you think?

--

 

Lorenz

 

  • Sign in to reply
  • Cancel
Parents
  • dukepro
    dukepro over 13 years ago

    On 02/21/2013 10:44 AM, Lorenz wrote:

    ...

     

     

    Just put for instance "$URL:$" or "$Revision:$" into a text and

    subversion will replace it with "$URL: <path to file in repository> $"

    and "$Revision 12345 $"  every time the file is checked out, checked

    in or updated.

     

    Other change management systems could be covered with regular expression

    (RE) substitution.  The substitution could be included in an attribute's

    value as well as in a text value.

     

    As a global attribute, the goal is to set the attribute REVISION (for

    example) to a value of "12345", which is only known after the file is

    checked into the change management system.  The value of the attribute

    as saved could be something on the order of:

     

        "$Revision:$|/[0-9]+/"

     

    The first part, "$Revision:$" would expand to a real revision number

    such as "$Revision: 12345$" as supplied by the change management

    system.  Thus, when the file is loaded by Eagle, the value of the

    attribute would be

     

        "$Revision: 12345$|/[0-9]+/"

     

    The pipe symbol would cause Eagle to pipe that text into the RE enclosed

    in the slashes.  In this case, only one or more digits would be

    included, resulting in the value of "12345".  Thus the value displayed

    would be the result of the RE.

     

    This has been discussed in the past in the suggest news group and

    cleaner solutions have been proposed.  See the thread titled "/regular

    expression search & replace support for text variables/" in

    eagle.suggest.eng dated March 5th, 2013.  Recapping part of that

    discussion...

     

    Shamelessly stealing some built-in functions from GNU Make, a more

    generic form could be:

     

    $(subst

    from

    ,

    to

    ,

    text

    )

        Replace from with to in text.

     

    $(patsubst

    pattern

    ,

    replacement

    ,

    text

    )

        Replace words matching pattern with replacement in text.

     

    See

    http://www.gnu.org/software/make/manual/html_node/Quick-Reference.html#Quick-Reference

     

    Eagle would have to maintain the formula for the attribute's value.  As

    such, an additional formula property may need to be added to UL_TEXT

    and UL_ATTRIBUTE objects that would contain the as-saved value.  The

    value property would return the calculated value, just as it does now.

     

    Employing the above, the saved formula for the attribute or text would be:

     

        $(patsubst .\(+\).,\1,$Revision: 12345$)

     

    The change management system would replace the /text/ portion with

    appropriate values.

     

    While I mention only a REVISION attribute, other attributes could be

    defined with their own formulas such as path in the repository, last

    check-in time stamp, or author.

     

    Jorge,  Does Cadsoft have any input on this?

     

        - Chuck

     

     

    Attachments:
    0250.att1.html.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 13 years ago in reply to dukepro

    On 6/11/2013 11:12 AM, Chuck Huber wrote:

     

     

    Jorge,  Does Cadsoft have any input on this?

     

    I'm not very familiar with subversion to be honest, I generally use

    Bazaar and then maybe only one percent of it's functionality. On top

    of that I can speak on behalf of the developers.

     

    But from what I can tell an easy solution would be two use two

    attributes and a ULP. The idea would be that you would use one

    Attribute in the manner described, with the additional text. You would

    then use a ULP to read that string in EAGLE strip the extra characters

    (through an RE or simple string methods) and write that to the second

    attribute which is the one that would be displayed on the layout.

     

    This would look correct and use the functionality available in

    subversion without changing EAGLE. The downside is that you have an

    extraneous attribute.

     

    I will ask the devs to take a look at this thread and post their

    comments.

     

    hth,

    Jorge Garcia

         - Chuck

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 13 years ago in reply to autodeskguest

    Jorge Garcia wrote:

    On 6/11/2013 11:12 AM, Chuck Huber wrote:

    Jorge,  Does Cadsoft have any input on this?

     

    I'm not very familiar with subversion to be honest, I generally use

    Bazaar and then maybe only one percent of it's functionality. On top

    of that I can speak on behalf of the developers.

     

    But from what I can tell an easy solution would be two use two

    attributes and a ULP. The idea would be that you would use one

    Attribute in the manner described, with the additional text. You would

    then use a ULP to read that string in EAGLE strip the extra characters

    (through an RE or simple string methods) and write that to the second

    attribute which is the one that would be displayed on the layout.

     

    This would look correct and use the functionality available in

    subversion without changing EAGLE. The downside is that you have an

    extraneous attribute.

     

    The ULP solutuion has at least two disadvantages:

     

    1) By running the ULP the file is changed, so that the version control

    system (VC, not necessarily subversion) sees and flags it as changed.

     

    2) you need to run the ULP to get the desired result. You can't just

    check-out the file and be done.

     

     

     

    For subversion at least there will be a solution as soon as V1.8.x is

    released (see:  "howto get 'clean' subversion revision info into

    global eagle properties" from 2013-06-11 in this news group).

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 13 years ago in reply to autodeskguest

    Jorge Garcia wrote:

    On 6/11/2013 11:12 AM, Chuck Huber wrote:

    Jorge,  Does Cadsoft have any input on this?

     

    I'm not very familiar with subversion to be honest, I generally use

    Bazaar and then maybe only one percent of it's functionality. On top

    of that I can speak on behalf of the developers.

     

    But from what I can tell an easy solution would be two use two

    attributes and a ULP. The idea would be that you would use one

    Attribute in the manner described, with the additional text. You would

    then use a ULP to read that string in EAGLE strip the extra characters

    (through an RE or simple string methods) and write that to the second

    attribute which is the one that would be displayed on the layout.

     

    This would look correct and use the functionality available in

    subversion without changing EAGLE. The downside is that you have an

    extraneous attribute.

     

    The ULP solutuion has at least two disadvantages:

     

    1) By running the ULP the file is changed, so that the version control

    system (VC, not necessarily subversion) sees and flags it as changed.

     

    2) you need to run the ULP to get the desired result. You can't just

    check-out the file and be done.

     

     

     

    For subversion at least there will be a solution as soon as V1.8.x is

    released (see:  "howto get 'clean' subversion revision info into

    global eagle properties" from 2013-06-11 in this news group).

    --

     

    Lorenz