Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Eagle 100x80mm routing area
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 522 views
  • Users 0 members are here
Related

Eagle 100x80mm routing area

e14 Contributor
e14 Contributor over 13 years ago

I was wondering if there is anyway to see where the available routing area is during layout?

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 13 years ago

    On 03/11/2013 10:48 AM, Scott Runnals wrote:

    I was wondering if there is anyway to see where the available routing area is during layout?

     

    Strictly speaking, it's the component placement area, not the routing

    area. You can route traces outside the 100x80 area, but you can't place

    components outside that area.

     

    The distinction can be important. My current project barely fits inside

    the 160mm x 100mm component placement area of Eagle Standard edition.

    I've made my board somewhat bigger so I have room to route traces to

    components placed such that their pins are right on the edge of the

    placement area.

     

    As others have said, when you create a board from a schematic using the

    Light or Standard editions, Eagle automatically creates a board contour

    in layer 20. It's just a "wire" in layer 20 with no special attributes.

    I change this contour line to another layer (I use layer 49 - Reference)

    and to another style (dash-dot) to make it distinctive. I then create my

    new board contour in layer 20 so the board house knows the dimensions of

    the board.

     

    If you're not seeing a 100mm x 80mm board contour pre-drawn for you, I'd

    guess you're creating a board without a schematic. In that case Eagle

    doesn't pre-draw the board contour. You can easily draw one yourself. If

    you want precise positioning, set the grid to mm or use the command line.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 13 years ago

    On 03/11/2013 10:48 AM, Scott Runnals wrote:

    I was wondering if there is anyway to see where the available routing area is during layout?

     

    Strictly speaking, it's the component placement area, not the routing

    area. You can route traces outside the 100x80 area, but you can't place

    components outside that area.

     

    The distinction can be important. My current project barely fits inside

    the 160mm x 100mm component placement area of Eagle Standard edition.

    I've made my board somewhat bigger so I have room to route traces to

    components placed such that their pins are right on the edge of the

    placement area.

     

    As others have said, when you create a board from a schematic using the

    Light or Standard editions, Eagle automatically creates a board contour

    in layer 20. It's just a "wire" in layer 20 with no special attributes.

    I change this contour line to another layer (I use layer 49 - Reference)

    and to another style (dash-dot) to make it distinctive. I then create my

    new board contour in layer 20 so the board house knows the dimensions of

    the board.

     

    If you're not seeing a 100mm x 80mm board contour pre-drawn for you, I'd

    guess you're creating a board without a schematic. In that case Eagle

    doesn't pre-draw the board contour. You can easily draw one yourself. If

    you want precise positioning, set the grid to mm or use the command line.