Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) How do I change a board outline shape/size in Eagle Cad Light?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 189 subscribers
  • Views 5204 views
  • Users 0 members are here
Related

How do I change a board outline shape/size in Eagle Cad Light?

japper
japper over 13 years ago

I am using the latest version of Eaglecad light (6.4.0) and I am attempting to make a shield for the Olimexino board.

 

I have taken an existing schematic and PCB layout  of the Olimexino board in order to get the correct spacing

of the pins that I want this pcb to plug into on the Olimexino PCB.

 

Wasn't sure how to import the pins for the spacing/locations so I saved the Olimexino schematioc and board

as a different file name and added my schematic to theOlimexino schematic.

 

Then I removed the Olimexino components (except the pins that i want to use) from the schematic and added my components.

 

I open the board file and the spacing looks correct for the pins that I want and then I had to remove all of the components

that I did not want from the original Olimexino board layout.

 

My ratslist is shown on the board screen but  I would like to change the dimensions of the PCB in the layout section of Eaglecad

to make more room for my circuits.

 

I made the board dimensions larger in the Eagle board layout section manually but then when I try to move a component onto the

newly addded area I get a message that states that the light version of eagle can't perform the requested action. Some objects extend

outside the allowed board areas.

 

How can I change the size of this PCB without loosing the spacing/location of the pins?

 

Thanks

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to e14 Contributor

    On 7/22/2015 4:06 PM, Edgar Gutierrez wrote:

    So I can not Draw a board from -50,-40 to 50,40? even is it is same area

    than 100x80 ?

     

    Hi Edgar,

     

    That's correct, EAGLE defines the work area using a rectangle whose

    bottom left corner is at 0,0 and top right corner is at 100mm, 80mm.

     

    hth,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    So I can not Draw a board from -50,-40 to 50,40? even is it is same area than 100x80 ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • japper
    japper over 13 years ago in reply to autodeskguest

    I just recently returned to this schematic and opened both the schematic and the layout and added a few components but

    the layout did not pick up the parts that I added to the schematic.

     

    Is there a way to get these added to the layout as well?

     

     

    thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 13 years ago in reply to e14 Contributor

    *Provide Customers with Professional Lighting Luminaire Design and

    Manufacturing Fulfilling the Professional, Functional and Cultural

    Requirements*

     

    *Induction lamps have the advantages of high brightness, high lumen

    efficiency, low-energy consumption, no flicker and long service life,

    possessing outstanding characteristics and excellent luminous effects.

    However, only the use of professional lamps can completely reveal the

    advantages of induction lamps, and only the use of professional lamps

    could be more useful from cultural and functional perspective.*

     

    *The induction lamp-related products available on the market have a

    relatively low professional degree, and the phenomenon of putting

    different types of matching lamps together can been observed everywhere.

    Applications in most cases, where other lighting fixture are far-fetched

    for induction lamps, void the advantages and characteristics of

    induction lamp, as well as its essential differences from conventional

    lighting products. In addition to that, the luminous efficiency is

    suppressed, and the differences in heat radiation shall result in

    shortening the use- life, lowering the energy-saving efficiency and

    seriously impacting the overall quality of products.*

     

    *In terms of functionality, lamps may need to withstand intensive

    vibration, air pressure, rain and snow, acid dust erosion, potential

    explosions and other events based on different environmental conditions;

    From cultural point of view, a lamp is an artistic expression meant to

    create the local social environment and pleasant atmosphere, as well as

    a best way to engage the innovative experience and customers’ individual

    demand. Clients’ individual needs can only be met with professional

    design and lean manufacturing, where the professional matching products

    of induction lamps (http://www.lvd.cc/inductionlamps.html) could be

    provided from the perspective of expertise, functionality and culture.*

     

    *Hongyuan has gathered a lot of experience in the illumination

    brightness and distribution curve flux design, overall lighting planning

    and other lamp designs, with profound technical strength. The company

    has developed and produced various professional products of induction

    lamps, including street lamps, tunnel lights, high bays, explosion-proof

    lamps, flood lights, underground lamps, down-lights, yard lamps, ceiling

    lamps and so on. The company makes its technology and services move

    forward to stand in the forefront of the market to listen to the actual

    demands of customers directly, then designs and makes customized

    products especially for them. If it reaches a certain production volume,

    the company can provide free designs for customers, as well as to meet

    the focal needs of high level and high standard from customers in the

    one-stop services provided by Hongyuan.*

     

    *The LVD manufacturing base covers an area of nearly 200mu (about 13.34

    acres), with the complete manufacturing cycle of research and

    development, and production of ballasts, PCB, glass bulbs and tubes,

    lamps, fixtures and packages, and it always controls all aspects and

    phases of production on its own, which closely reflects the strict

    requirements of Hongyuan for product quality and their stringent

    attitude for being highly responsible for customers.*

     

    *LVD Mold Workshops have a complete set of mold equipments with high

    standard and high level, creating various lamp molds completely adherent

    the design of lamps, and then use a whole set of production proceedings

    to test the mold process and mass-production, to ensure the product

    quality of manufacturing in enormous quantities. In fabrication, the

    lean production makes the product quality penetrate into every detail,

    to show the excellent quality of Hongyuan’s induction lamps, hoping

    customers to be satisfied because the product quality meeting or

    exceeding their expectations upon experiencing our products.*

     

    *A team of professional designers in Hongyuan are working hard to meet

    the multiple demands of customers, with the working principles of

    Customized Design, Professional manufacturing and policy of aiming at

    customers’ demands, supporting the concept of green and energy-efficient

    lighting products is spread to the global market better through

    induction lamps (http://www.lvd.cc/inductionlamps.html), which are

    making more and more contributions to the green illumination.*

     

    Website: http://en.lvd.cc

    Tel:  (8621)-59174276

    Email:sxl@shhongyuan.com (mailto:sxl@shhongyuan.com)

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/79240#79240

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to autodeskguest

    image i had the same problem and this explanation made my undestanding beter to the software that i am trying to learn

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 13 years ago in reply to japper

    Another question...

     

    I am done with my schematics and have run the CAM processor.

     

    Afterwards, I decided to view my gerber files on a viewer before sending

    these out to the fab house but

    I noticed that there is not board outline in the gerber viewer.

     

    When  I did the wire (0 0)(100 0)(100 80)(0 80)(0 0); to find how much

    room that I had,

    I then moved this so it was smaller and deleted the board outline that

    was smaller.

     

    Looking at my PCB in Eagle, the brd file looks like this:

     

    and looking at the gerbers in a viewer, they look like this:

     

     

     

    What am I missing and how do I create a board outline that is set to the

    values of the wire that  I created so that I have a board outline on my

    PCB?

     

    thanks

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/75533#75533

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 13 years ago in reply to japper

    A couple more questions...

     

    1. I noticed that the objects that  iadded do not line up with teh grid.

    How do I change the resolution of the grid or snap these items to the

    grid in EagleCad light 6.4?

     

    2. I have some grouped items on my borad layout that I would like to

    ungroup and delete certain items.

    How do I do this in EagleCad light 6.4?

     

    thanks again

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/75128#75128

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • japper
    japper over 13 years ago in reply to autodeskguest

    Warren-

     

    I had to remove a few things on my PCB layout to fit within the boundries but the 100 x 80 was more than large enough space.

     

    Thank you very much for your help!

    Jeff p

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 13 years ago

    Hi

     

    Great to see you took time to describe your problem using many words.

     

    Your approach was sound enough but could have been easier.

    If you have the board and schematic open at the same time, as you remove

    the unwanted Olimexino parts from the schematic they are removed from the

    board at the same time.

     

    Eagle light has a board size restriction of 100mm x 80 mm. If you attempt

    to place a part origin or part pad outside of that area you get the error

    you received. You can have other lines outside that area.

     

    Knowing what you wanted to do, I would do the following for that Olimexino

    board, at the start.

    1. Move all of it further into the permitted area

    Enter into the command line

    Group all;

    move (>0 0)(10 10);

    2. Manually MOVE that jumper table down below the Y=0 axis with a GROUP

    then MOVE with CTL key depressed and right mouse.

     

    3. Draw an outline that shows you the 100*80mm restriction.

    grid mm;

    layer tDoc;

    wire (0 0)(100 0)(100 80)(0 80)(0 0);

     

    4. Now you can easily group and move the board to where you want it within

    the limitations of the light version.

     

    To answer your question another way, you could group singly (See HELP

    GROUP) each of the pin headers and move them as a group. They will retain

    their relation ship to each other

     

    HTH

    Warren

     

     

     

     

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.