Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) How do I change a board outline shape/size in Eagle Cad Light?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 189 subscribers
  • Views 5207 views
  • Users 0 members are here
Related

How do I change a board outline shape/size in Eagle Cad Light?

japper
japper over 13 years ago

I am using the latest version of Eaglecad light (6.4.0) and I am attempting to make a shield for the Olimexino board.

 

I have taken an existing schematic and PCB layout  of the Olimexino board in order to get the correct spacing

of the pins that I want this pcb to plug into on the Olimexino PCB.

 

Wasn't sure how to import the pins for the spacing/locations so I saved the Olimexino schematioc and board

as a different file name and added my schematic to theOlimexino schematic.

 

Then I removed the Olimexino components (except the pins that i want to use) from the schematic and added my components.

 

I open the board file and the spacing looks correct for the pins that I want and then I had to remove all of the components

that I did not want from the original Olimexino board layout.

 

My ratslist is shown on the board screen but  I would like to change the dimensions of the PCB in the layout section of Eaglecad

to make more room for my circuits.

 

I made the board dimensions larger in the Eagle board layout section manually but then when I try to move a component onto the

newly addded area I get a message that states that the light version of eagle can't perform the requested action. Some objects extend

outside the allowed board areas.

 

How can I change the size of this PCB without loosing the spacing/location of the pins?

 

Thanks

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 13 years ago

    Hi

     

    Great to see you took time to describe your problem using many words.

     

    Your approach was sound enough but could have been easier.

    If you have the board and schematic open at the same time, as you remove

    the unwanted Olimexino parts from the schematic they are removed from the

    board at the same time.

     

    Eagle light has a board size restriction of 100mm x 80 mm. If you attempt

    to place a part origin or part pad outside of that area you get the error

    you received. You can have other lines outside that area.

     

    Knowing what you wanted to do, I would do the following for that Olimexino

    board, at the start.

    1. Move all of it further into the permitted area

    Enter into the command line

    Group all;

    move (>0 0)(10 10);

    2. Manually MOVE that jumper table down below the Y=0 axis with a GROUP

    then MOVE with CTL key depressed and right mouse.

     

    3. Draw an outline that shows you the 100*80mm restriction.

    grid mm;

    layer tDoc;

    wire (0 0)(100 0)(100 80)(0 80)(0 0);

     

    4. Now you can easily group and move the board to where you want it within

    the limitations of the light version.

     

    To answer your question another way, you could group singly (See HELP

    GROUP) each of the pin headers and move them as a group. They will retain

    their relation ship to each other

     

    HTH

    Warren

     

     

     

     

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • japper
    japper over 13 years ago in reply to autodeskguest

    I just recently returned to this schematic and opened both the schematic and the layout and added a few components but

    the layout did not pick up the parts that I added to the schematic.

     

    Is there a way to get these added to the layout as well?

     

     

    thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • japper
    japper over 13 years ago in reply to autodeskguest

    I just recently returned to this schematic and opened both the schematic and the layout and added a few components but

    the layout did not pick up the parts that I added to the schematic.

     

    Is there a way to get these added to the layout as well?

     

     

    thank you