EAGLE User Chat (English) Irregular SMD shape
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
  • Replies 5 replies
  • Subscribers 177 subscribers
  • Views 1011 views
  • Users 0 members are here
Related

Irregular SMD shape

autodeskguest
autodeskguest over 17 years ago

Hello,

   I am trying to built a Linear Tech part which has DFN14

package(http://www.linear.com/designtools/packaging/dfn/DE14.pdf).  The

central pad is no rectangular.  When I place an SMD pad, it is

rectangular and cannot be mitered. Does this mean I need to use a

polygon and draw the shape in the signal, cream and stop layers? If so,

how far does the solder mask be from the actual pad?

 

Thank you,

 

-- A

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Amer wrote:

    Type "help smd" into the command line of your library editor (without

    the quotes).  Look for the roundness parameter.  I think that is what

    you are looking for.  It's ok if the pad on the board is rounded on all

    four corners while the part has one corner chamfered.

     

      Tom Sneddon

     

    Thank you.  That will work.  Is this the only way to make irregularly

    shaped SMDs?

    With the roundness parameter, how do you make sure that you have a

    specific radius?

    You can not add "named" copper to a lib footprint without DRC errors but

    you can make the soldermask and cream layers to the shape you need and

    then add a polygon for the ground plane under the part and it will be a

    better heat sink then just that pad.

     

    Paul R.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Amer wrote:

    Type "help smd" into the command line of your library editor (without

    the quotes).  Look for the roundness parameter.  I think that is what

    you are looking for.  It's ok if the pad on the board is rounded on all

    four corners while the part has one corner chamfered.

     

      Tom Sneddon

     

    Thank you.  That will work.  Is this the only way to make irregularly

    shaped SMDs?

    With the roundness parameter, how do you make sure that you have a

    specific radius?

    You can not add "named" copper to a lib footprint without DRC errors but

    you can make the soldermask and cream layers to the shape you need and

    then add a polygon for the ground plane under the part and it will be a

    better heat sink then just that pad.

     

    Paul R.