EAGLE User Chat (English) Draw block diagrams with Eagle?
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
  • Replies 12 replies
  • Subscribers 177 subscribers
  • Views 3205 views
  • Users 0 members are here
Related

Draw block diagrams with Eagle?

autodeskguest
autodeskguest over 17 years ago

Hello Folks,

 

So far I used to draw block diagrams with other (more mechanical) CAD

software but that gets old. Is there a fairly easy way to do that with

Eagle?

 

It's not about anything being ERC-proof at all, just to illustrate the

function of electronic devices. Boxes, text, lines with arrows at one

end and such.

 

--

Regards, Joerg

 

http://www.analogconsultants.com/

 

"gmail" domain blocked because of excessive spam.

Use another domain or send PM.

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Brownie wrote:

    Joerg wrote:

     

    Brownie wrote:

    Joerg wrote:

     

    Brownie wrote:

    Joerg wrote:

     

    Hello Folks,

     

    So far I used to draw block diagrams with other (more mechanical) CAD

    software but that gets old. Is there a fairly easy way to do that with

    Eagle?

     

    It's not about anything being ERC-proof at all, just to illustrate the

    function of electronic devices. Boxes, text, lines with arrows at one

    end and such.

     

    Hi Joerg,

    We have done many mechanical design drawings with Eagle.

    When we have a project that requires schematics, PCB, system wiring

    diagrams and mechanical drawings for machining assemblies and panels,

    we do it all with eagle.  just don't have the time to learn several

    programs for one project.

    Mechanicals are easy.  We have a Template Sheet that is part of every

    project requiring any mechanical drawings.  The template has various

    Arrows (for pointing and dimensions), Line Stiles, Valves, Screws,

    Springs, and other oddball stuff not found in the usual PCB project.

    The new 5.0 makes this even easier because of the thumbnails and sheet

    reshuffling.  We just copy the needed part to the worksheet.

    We even have Symbol sheets of CNC Ladder, Pneumatic/Hydraulic and

    Software Flow Chart stuff.

    We build all of this stuff with WIRES so they are easy to Resize to

    fit the application at hand.  Even Circles and Arcs will resize in 5.0

    Best of all, we only create the component once for all time use.

    This all may have been a bore, or maybe useful.

    Not boring at all, this is interesting. I'll have to look at how

    templates are done, so far I have only created library parts. The manual

    doesn't mention templates. But even with a library it could be done,

    except that you can't resize parts easily which I'll have to do at least

    with the boxes. But those can be sketched directly with the wire

    command.

     

    Thanks, Brownie.

     

    Joerg,

    We refer to our component sheets internally as templates but the

    manual nay not mention this.  Our Templates are nothing more than a

    schematic sheet with the various components drawn in.

    An Eagle Library (maybe call it Special_symbols.lib) could be used,

    BUT our applications often require resizing of the symbols and I don't

    think this is possible with library parts.

    Our Template Sheets are defined in our Skeleton Eaglerc and .EPF files

    so that they will auto-load with all new projects.  The sheets can be

    deleted when the project is done.

     

    Aha. So you are basically drawing a sample schematic which gets dragged

    along as a sheet, parts are picked from there and then deleted at the

    end. Pretty clever.

     

    And yes, I believe that's the only way to keep things resizeable because

    the library editor in Eagle is IMHO, ahem, a bit on the clumsy side.

     

    Joerg,

    It's even easier.  The template sheets are deleted.

     

     

    Yes, that's how I understood it. Another option if not too many parts

    are needed would be to have the common symbols on one sheet

    "symbols.sch", copy that to a file "my_new_block_diagram.sch", copy and

    paste within the sheet and at the end group-delete all the seed symbols

    and rescale to screen.

     

    So yeah, looks like Eagle can do this. Thanks for the hint.

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Brownie wrote:

    Joerg wrote:

     

    Brownie wrote:

    Joerg wrote:

     

    Brownie wrote:

    Joerg wrote:

     

    Hello Folks,

     

    So far I used to draw block diagrams with other (more mechanical) CAD

    software but that gets old. Is there a fairly easy way to do that with

    Eagle?

     

    It's not about anything being ERC-proof at all, just to illustrate the

    function of electronic devices. Boxes, text, lines with arrows at one

    end and such.

     

    Hi Joerg,

    We have done many mechanical design drawings with Eagle.

    When we have a project that requires schematics, PCB, system wiring

    diagrams and mechanical drawings for machining assemblies and panels,

    we do it all with eagle.  just don't have the time to learn several

    programs for one project.

    Mechanicals are easy.  We have a Template Sheet that is part of every

    project requiring any mechanical drawings.  The template has various

    Arrows (for pointing and dimensions), Line Stiles, Valves, Screws,

    Springs, and other oddball stuff not found in the usual PCB project.

    The new 5.0 makes this even easier because of the thumbnails and sheet

    reshuffling.  We just copy the needed part to the worksheet.

    We even have Symbol sheets of CNC Ladder, Pneumatic/Hydraulic and

    Software Flow Chart stuff.

    We build all of this stuff with WIRES so they are easy to Resize to

    fit the application at hand.  Even Circles and Arcs will resize in 5.0

    Best of all, we only create the component once for all time use.

    This all may have been a bore, or maybe useful.

    Not boring at all, this is interesting. I'll have to look at how

    templates are done, so far I have only created library parts. The manual

    doesn't mention templates. But even with a library it could be done,

    except that you can't resize parts easily which I'll have to do at least

    with the boxes. But those can be sketched directly with the wire

    command.

     

    Thanks, Brownie.

     

    Joerg,

    We refer to our component sheets internally as templates but the

    manual nay not mention this.  Our Templates are nothing more than a

    schematic sheet with the various components drawn in.

    An Eagle Library (maybe call it Special_symbols.lib) could be used,

    BUT our applications often require resizing of the symbols and I don't

    think this is possible with library parts.

    Our Template Sheets are defined in our Skeleton Eaglerc and .EPF files

    so that they will auto-load with all new projects.  The sheets can be

    deleted when the project is done.

     

    Aha. So you are basically drawing a sample schematic which gets dragged

    along as a sheet, parts are picked from there and then deleted at the

    end. Pretty clever.

     

    And yes, I believe that's the only way to keep things resizeable because

    the library editor in Eagle is IMHO, ahem, a bit on the clumsy side.

     

    Joerg,

    It's even easier.  The template sheets are deleted.

     

     

    Yes, that's how I understood it. Another option if not too many parts

    are needed would be to have the common symbols on one sheet

    "symbols.sch", copy that to a file "my_new_block_diagram.sch", copy and

    paste within the sheet and at the end group-delete all the seed symbols

    and rescale to screen.

     

    So yeah, looks like Eagle can do this. Thanks for the hint.

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/