EAGLE User Chat (English) Power plane questions
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
  • Replies 5 replies
  • Subscribers 179 subscribers
  • Views 598 views
  • Users 0 members are here
Related

Power plane questions

autodeskguest
autodeskguest over 17 years ago

EAGLE users,

 

Working on my first four layer board and have a few questions about the

power plane polygons.

 

The Vdd & DGND planes overlap each other, with one being slightly

smaller (for visibility), and are both in slightly from the board edge

to prevent shorts when panelized.

 

Question 1:

There are now a few rectangular areas inside those polygons where I'd

like have neither plane plated-- "voids" in those areas as it were.  How

is that done?  Not sure where that kind of editing is covered in the

manual, or where to find an example.

 

Question 2:

I have several through vias that tap off either Vdd or DGND to provide

power for a top or bottom trace (or both) as needed.  What I'm not

seeing are the "thermal" connect areas.  Pretty sure the connection is

being made since vias high light correctly when selected.  But given the

expense of 4 layer board, I'd like to be sure it's correct!

 

Thanks in advance for your help.

 

Just as a FYI, I've also noticed displaying/hiding the fills doesn't

seem to work (or work consistently) with such overlapping polygons.  For

now, if it does show up when not needed, exiting & restarting EAGLE

hides the  fill.  Also in working on a test area, I see the fill does

not show up unless there is a through hole part inside the area.

 

Thanks

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    KR wrote:

    Question 1:

    There are now a few rectangular areas inside those polygons where I'd

    like have neither plane plated-- "voids" in those areas as it were. How is

    that done?  Not sure where that kind of editing is covered in

    the manual, or where to find an example.

     

    There was a recent question about this same topic, by someone who wanted a

    single void area in the middle of a polygon.  I suggested that two

    overlapping polygons can be used to leave a void area between them (think

    two U-shaped polygons with the legs facing and overlapping each other).

    Someone else suggested a single polygon could be drawn, although it seems to

    be tricky to do without getting DRC complaints.

     

    --

    Bert Menkveld

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    KR wrote:

    Question 1:

    There are now a few rectangular areas inside those polygons where I'd

    like have neither plane plated-- "voids" in those areas as it were. How is

    that done?  Not sure where that kind of editing is covered in

    the manual, or where to find an example.

     

    There was a recent question about this same topic, by someone who wanted a

    single void area in the middle of a polygon.  I suggested that two

    overlapping polygons can be used to leave a void area between them (think

    two U-shaped polygons with the legs facing and overlapping each other).

    Someone else suggested a single polygon could be drawn, although it seems to

    be tricky to do without getting DRC complaints.

     

    --

    Bert Menkveld