EAGLE User Chat (English) Power plane questions
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
  • Replies 5 replies
  • Subscribers 179 subscribers
  • Views 599 views
  • Users 0 members are here
Related

Power plane questions

autodeskguest
autodeskguest over 17 years ago

EAGLE users,

 

Working on my first four layer board and have a few questions about the

power plane polygons.

 

The Vdd & DGND planes overlap each other, with one being slightly

smaller (for visibility), and are both in slightly from the board edge

to prevent shorts when panelized.

 

Question 1:

There are now a few rectangular areas inside those polygons where I'd

like have neither plane plated-- "voids" in those areas as it were.  How

is that done?  Not sure where that kind of editing is covered in the

manual, or where to find an example.

 

Question 2:

I have several through vias that tap off either Vdd or DGND to provide

power for a top or bottom trace (or both) as needed.  What I'm not

seeing are the "thermal" connect areas.  Pretty sure the connection is

being made since vias high light correctly when selected.  But given the

expense of 4 layer board, I'd like to be sure it's correct!

 

Thanks in advance for your help.

 

Just as a FYI, I've also noticed displaying/hiding the fills doesn't

seem to work (or work consistently) with such overlapping polygons.  For

now, if it does show up when not needed, exiting & restarting EAGLE

hides the  fill.  Also in working on a test area, I see the fill does

not show up unless there is a through hole part inside the area.

 

Thanks

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    James,

     

    Thanks for your feedback.

    I understand what you are saying with ripup & ratsnest commands.  Before

    putting in the full power planes, I tried some small, non overlapping,

    test power plane polygons. Individually, the ripup & ratsnest commands

    worked correctly.  The code apparently gets confused with overlapping

    polygons.  Exiting and restarting EAGLE is the only way I found to

    remove BOTH fills.  As previously mentioned, while a little

    inconvenient, it's not a big deal, as I don't need to clear the fills

    very often.

     

    Right now, creating voids inside the existing polygons and not being

    able to verify the thermal connections are the greater concerns.

     

     

    Ken

     

     

    James Morrison wrote:

    On 2008/May/01 12:49 PM, in article fvcsc1$tn1$1@cheetah.cadsoft.de, "KR"

    <k.rusnok@maccor.com> wrote:

     

    For

    now, if it does show up when not needed, exiting & restarting EAGLE

    hides the  fill.

     

    Hello KR,

     

    If you want to "hide" the fill of a polygon then you need to use the ripup

    command.  This actually removes the copper pour and just leaves the outline.

    There is no way to hide just polygons (I have made this suggestion before,

    maybe in the next version).

     

    Further to this, there is an option to process polygons with the ratsnest.

    If you turn this off then the polygons won't be poured when you run the

    ratsnest.  Of course, they won't be connected either so the remaining

    airwires will be counted incorrectly.  But this is handy in some situations.

     

    Cheers,

     

    James.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    James,

     

    Thanks for your feedback.

    I understand what you are saying with ripup & ratsnest commands.  Before

    putting in the full power planes, I tried some small, non overlapping,

    test power plane polygons. Individually, the ripup & ratsnest commands

    worked correctly.  The code apparently gets confused with overlapping

    polygons.  Exiting and restarting EAGLE is the only way I found to

    remove BOTH fills.  As previously mentioned, while a little

    inconvenient, it's not a big deal, as I don't need to clear the fills

    very often.

     

    Right now, creating voids inside the existing polygons and not being

    able to verify the thermal connections are the greater concerns.

     

     

    Ken

     

     

    James Morrison wrote:

    On 2008/May/01 12:49 PM, in article fvcsc1$tn1$1@cheetah.cadsoft.de, "KR"

    <k.rusnok@maccor.com> wrote:

     

    For

    now, if it does show up when not needed, exiting & restarting EAGLE

    hides the  fill.

     

    Hello KR,

     

    If you want to "hide" the fill of a polygon then you need to use the ripup

    command.  This actually removes the copper pour and just leaves the outline.

    There is no way to hide just polygons (I have made this suggestion before,

    maybe in the next version).

     

    Further to this, there is an option to process polygons with the ratsnest.

    If you turn this off then the polygons won't be poured when you run the

    ratsnest.  Of course, they won't be connected either so the remaining

    airwires will be counted incorrectly.  But this is handy in some situations.

     

    Cheers,

     

    James.