EAGLE User Chat (English) Power plane questions
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
  • Replies 5 replies
  • Subscribers 179 subscribers
  • Views 597 views
  • Users 0 members are here
Related

Power plane questions

autodeskguest
autodeskguest over 17 years ago

EAGLE users,

 

Working on my first four layer board and have a few questions about the

power plane polygons.

 

The Vdd & DGND planes overlap each other, with one being slightly

smaller (for visibility), and are both in slightly from the board edge

to prevent shorts when panelized.

 

Question 1:

There are now a few rectangular areas inside those polygons where I'd

like have neither plane plated-- "voids" in those areas as it were.  How

is that done?  Not sure where that kind of editing is covered in the

manual, or where to find an example.

 

Question 2:

I have several through vias that tap off either Vdd or DGND to provide

power for a top or bottom trace (or both) as needed.  What I'm not

seeing are the "thermal" connect areas.  Pretty sure the connection is

being made since vias high light correctly when selected.  But given the

expense of 4 layer board, I'd like to be sure it's correct!

 

Thanks in advance for your help.

 

Just as a FYI, I've also noticed displaying/hiding the fills doesn't

seem to work (or work consistently) with such overlapping polygons.  For

now, if it does show up when not needed, exiting & restarting EAGLE

hides the  fill.  Also in working on a test area, I see the fill does

not show up unless there is a through hole part inside the area.

 

Thanks

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Bert,

     

    Thanks for your comments.

     

    Drawing new polygons around the void area:

    That's sort of what I thought would be a good workaround.  Yes, it's

    more work and not as intuitive, but the bottom line for all of us is

    getting the layout DONE!

     

    Perhaps on a future release, polygons will have a "fill or void" option.

     

     

    Ken

     

     

     

    Bert Menkveld wrote:

    KR wrote:

    Question 1:

    There are now a few rectangular areas inside those polygons where I'd

    like have neither plane plated-- "voids" in those areas as it were. How is

    that done?  Not sure where that kind of editing is covered in

    the manual, or where to find an example.

     

    There was a recent question about this same topic, by someone who wanted a

    single void area in the middle of a polygon.  I suggested that two

    overlapping polygons can be used to leave a void area between them (think

    two U-shaped polygons with the legs facing and overlapping each other).

    Someone else suggested a single polygon could be drawn, although it seems to

    be tricky to do without getting DRC complaints.

     

    --

    Bert Menkveld

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Bert,

     

    Thanks for your comments.

     

    Drawing new polygons around the void area:

    That's sort of what I thought would be a good workaround.  Yes, it's

    more work and not as intuitive, but the bottom line for all of us is

    getting the layout DONE!

     

    Perhaps on a future release, polygons will have a "fill or void" option.

     

     

    Ken

     

     

     

    Bert Menkveld wrote:

    KR wrote:

    Question 1:

    There are now a few rectangular areas inside those polygons where I'd

    like have neither plane plated-- "voids" in those areas as it were. How is

    that done?  Not sure where that kind of editing is covered in

    the manual, or where to find an example.

     

    There was a recent question about this same topic, by someone who wanted a

    single void area in the middle of a polygon.  I suggested that two

    overlapping polygons can be used to leave a void area between them (think

    two U-shaped polygons with the legs facing and overlapping each other).

    Someone else suggested a single polygon could be drawn, although it seems to

    be tricky to do without getting DRC complaints.

     

    --

    Bert Menkveld

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • autodeskguest
    autodeskguest over 17 years ago in reply to autodeskguest

    It is quite easy to create a void in a polygon, I do it often

    Use the SPLIT command to change the polygon outline, drive it to the

    void area you want, use it to draw the perimeter of the void, nearly

    until you close it (one grid pitch before).Then make it go back to the

    edge of the board. After that change to a smaller grid and move one edge

    of the remaining void channel so that it nearly overlaps the other, and

    it's done. Don't overlap exactly the segments, the polygon would be illegal.

    With the same method you can create any kind of void in a polygon, a

    wire-like void allows power / signal ground separation with only a small

    bridge for connection

     

    Christian Magne

     

    KR wrote:

    Bert,

     

    Thanks for your comments.

     

    Drawing new polygons around the void area:

    That's sort of what I thought would be a good workaround.  Yes, it's

    more work and not as intuitive, but the bottom line for all of us is

    getting the layout DONE!

     

    Perhaps on a future release, polygons will have a "fill or void" option.

     

     

    Ken

     

     

     

    Bert Menkveld wrote:

    KR wrote:

    Question 1:

    There are now a few rectangular areas inside those polygons where I'd

    like have neither plane plated-- "voids" in those areas as it were.

    How is that done?  Not sure where that kind of editing is covered in

    the manual, or where to find an example.

     

    There was a recent question about this same topic, by someone who

    wanted a single void area in the middle of a polygon.  I suggested

    that two overlapping polygons can be used to leave a void area between

    them (think two U-shaped polygons with the legs facing and overlapping

    each other). Someone else suggested a single polygon could be drawn,

    although it seems to be tricky to do without getting DRC complaints.

     

    --

    Bert Menkveld