EAGLE User Chat (English) Copper Pours - Manufacturability of PCB
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
  • Replies 9 replies
  • Subscribers 180 subscribers
  • Views 954 views
  • Users 0 members are here
Related

Copper Pours - Manufacturability of PCB

autodeskguest
autodeskguest over 17 years ago

Hi -

 

I've got a PCB with a fair number of sensitive analog parts on it so I've

flooded a large area of the top layer of the board with a copper ground

plane using the Polygon feature of Eagle.  Another large section of the

board has been left without the top layer copper plane.  All is OK with this

and the PCB is about ready to manufacture.

 

It occurred to me that this could be problematic in the PCB manufacturing

process.  Having half the board covered with copper where the traces are

isolated by a narrow gap and then the other half with narrow traces and all

the surrounding copper removed could present problems for the etching

process.

 

On the other hand, removing less copper by leaving large copper pours should

be more environmentally friendly.

 

Do PCB manufacturers have a preference one way or the other?  (I've checked

a number of PCB vendors websites and haven't really found any information.)

 

Sincerely,

 

John

 

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Paul Romanyszyn wrote:

    John M. Jarvis wrote:

    Hi -

     

    I've got a PCB with a fair number of sensitive analog parts on it so

    I've flooded a large area of the top layer of the board with a copper

    ground plane using the Polygon feature of Eagle.  Another large

    section of the board has been left without the top layer copper

    plane.  All is OK with this and the PCB is about ready to manufacture.

     

    It occurred to me that this could be problematic in the PCB

    manufacturing process.  Having half the board covered with copper

    where the traces are isolated by a narrow gap and then the other half

    with narrow traces and all the surrounding copper removed could

    present problems for the etching process.

     

    This should not affect the etching process. Large copper areas in some

    areas may affect the board and make it warp when you solder it by wave

    or reflow methods. I think with proper preheating it won't be a problem.

     

    On the other hand, removing less copper by leaving large copper pours

    should be more environmentally friendly.

     

    I fill both the top and bottom with ground and power polygons

     

    Filled with ground highlighted.

    http://arcelectronicsinc.com/testinfo/componentside.png

     

    Filled with +5 highlighted

    http://arcelectronicsinc.com/testinfo/plus5.png

    Do PCB manufacturers have a preference one way or the other?  (I've

    checked a number of PCB vendors websites and haven't really found any

    information.)

     

    Sincerely,

     

    John

     

     

     

     

    Paul R.

     

    You can check with the PCB manufacture to see if they can add thieving

    to the areas void of copper. This could help with preventing board

    warpage and overetching of the areas with large amounts of copper.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Paul Romanyszyn wrote:

    John M. Jarvis wrote:

    Hi -

     

    I've got a PCB with a fair number of sensitive analog parts on it so

    I've flooded a large area of the top layer of the board with a copper

    ground plane using the Polygon feature of Eagle.  Another large

    section of the board has been left without the top layer copper

    plane.  All is OK with this and the PCB is about ready to manufacture.

     

    It occurred to me that this could be problematic in the PCB

    manufacturing process.  Having half the board covered with copper

    where the traces are isolated by a narrow gap and then the other half

    with narrow traces and all the surrounding copper removed could

    present problems for the etching process.

     

    This should not affect the etching process. Large copper areas in some

    areas may affect the board and make it warp when you solder it by wave

    or reflow methods. I think with proper preheating it won't be a problem.

     

    On the other hand, removing less copper by leaving large copper pours

    should be more environmentally friendly.

     

    I fill both the top and bottom with ground and power polygons

     

    Filled with ground highlighted.

    http://arcelectronicsinc.com/testinfo/componentside.png

     

    Filled with +5 highlighted

    http://arcelectronicsinc.com/testinfo/plus5.png

    Do PCB manufacturers have a preference one way or the other?  (I've

    checked a number of PCB vendors websites and haven't really found any

    information.)

     

    Sincerely,

     

    John

     

     

     

     

    Paul R.

     

    You can check with the PCB manufacture to see if they can add thieving

    to the areas void of copper. This could help with preventing board

    warpage and overetching of the areas with large amounts of copper.