EAGLE User Chat (English) Copper Pours - Manufacturability of PCB
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
  • Replies 9 replies
  • Subscribers 180 subscribers
  • Views 949 views
  • Users 0 members are here
Related

Copper Pours - Manufacturability of PCB

autodeskguest
autodeskguest over 17 years ago

Hi -

 

I've got a PCB with a fair number of sensitive analog parts on it so I've

flooded a large area of the top layer of the board with a copper ground

plane using the Polygon feature of Eagle.  Another large section of the

board has been left without the top layer copper plane.  All is OK with this

and the PCB is about ready to manufacture.

 

It occurred to me that this could be problematic in the PCB manufacturing

process.  Having half the board covered with copper where the traces are

isolated by a narrow gap and then the other half with narrow traces and all

the surrounding copper removed could present problems for the etching

process.

 

On the other hand, removing less copper by leaving large copper pours should

be more environmentally friendly.

 

Do PCB manufacturers have a preference one way or the other?  (I've checked

a number of PCB vendors websites and haven't really found any information.)

 

Sincerely,

 

John

 

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

     

    "Terri Miller" <tmiller@sunstone.com> wrote in message

    news:g1jq62$5o7$1@cheetah.cadsoft.de...

    Hello,

     

    Tilmann explained this very well.  Many manufacturers do add thieving

    areas for designs like this as well.  I will add (from a manufacturing

    standpoint) when using crosshatching be sure that it does not violate the

    minimum trace/space requirements of your fab house.

     

    Terri

     

     

    Thank you all for the helpful information.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

     

    "Terri Miller" <tmiller@sunstone.com> wrote in message

    news:g1jq62$5o7$1@cheetah.cadsoft.de...

    Hello,

     

    Tilmann explained this very well.  Many manufacturers do add thieving

    areas for designs like this as well.  I will add (from a manufacturing

    standpoint) when using crosshatching be sure that it does not violate the

    minimum trace/space requirements of your fab house.

     

    Terri

     

     

    Thank you all for the helpful information.