Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Can't Access Library Through Add Command in v4.16 on Win7sp1
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 189 subscribers
  • Views 707 views
  • Users 0 members are here
Related

Can't Access Library Through Add Command in v4.16 on Win7sp1

e14 Contributor
e14 Contributor over 13 years ago

I'm trying to use Eagle v4.16 on a newer computer with Windows 7, Service Pack 1, working on files I had created on another computer (XP).  Working on the boards/schematics is fine, but I can't add anything from the library. 

 

The library and all its parts show up on the Control Panel, but the Add window shows up empty.  The Options directories now show "$EAGLEDIR\lbr;C:\Program Files\Eagle 4.16\lbr" (I added the second part to see if it helped--it didn't). 

 

Any suggestions?

 

Thanks in advance.

Jan W

  • Sign in to reply
  • Cancel
Parents
  • AnalogNotes
    AnalogNotes over 13 years ago

    Did you try "use"?

     

    EDIT: more specifically, you could try "use *;" and then all libraries should show up in the Add dialog...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to AnalogNotes

    I am having the same problem using v6.5.0 freeware on Window Vista. I have tried USE to no avail. Any thoughts out there? Could this be a limitation of freeware?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Harvey:

     

    Be aware that I'm using the old version 4.1, and that yours may be different, but if you go to the Control Panel, you can open the Library and hopefully see all the devices listed there.  On my version, there's a series of little green dots to the right of all the devices, which will be either big (used) or small (not used).  You can either click on the green dot to change its Use status, or you can right-click on the folder or the Libraries word to get a dialog box, which lists "New Folder", "Rename", etc., below which are the choices "Use All" and "Use None"--this will select the whole library.  Then when you try to Add something, the "Used" items should show up in the box. 

     

    See how that works.

     

    Jan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Thanks for the information. I was able to follow the procedure you suggested. However I still cannot access my library from the schematic editor.

    From within the schematic editor I can choose to "USE" my library (it shows up in the list). However hen I use "ADD" to get my part the my library does not show up in that list.

     

    There may be something wrong with the installation. When using the schematic editor the program frequently crashes subsequent to a mouse click.

    I have tried removing and reinstalling with no success. At this point the program is unusable.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Thanks for the information. I was able to follow the procedure you suggested. However I still cannot access my library from the schematic editor.

    From within the schematic editor I can choose to "USE" my library (it shows up in the list). However hen I use "ADD" to get my part the my library does not show up in that list.

     

    There may be something wrong with the installation. When using the schematic editor the program frequently crashes subsequent to a mouse click.

    I have tried removing and reinstalling with no success. At this point the program is unusable.