EAGLE User Chat (English) Elektro, use inch or mm in europe?
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
  • Replies 2 replies
  • Subscribers 181 subscribers
  • Views 524 views
  • Users 0 members are here
Related

Elektro, use inch or mm in europe?

autodeskguest
autodeskguest over 17 years ago

Is the elektro-library based on inch or mm grid? The german tutorial says

that inch-grid should be used. I've expected the Germans to use mm in their

drawing standard for elektro schemes. Thought IEC-standards used the metric

system.

//Bjørn, Norway

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 17 years ago

    Bjørn Birkeland schrieb:

    Is the elektro-library based on inch or mm grid? The german tutorial says

    that inch-grid should be used. I've expected the Germans to use mm in their

    drawing standard for elektro schemes. Thought IEC-standards used the metric

    system.

    //Bjørn, Norway

     

     

     

    The inch grid is the default in the EAGLE Schematic editor. This

    is for historic reasons. All Symbols in the electronic (and also

    in the electrical) libraries are drawn in 0.1 inch grid.

    Of course the hardware is mostly made in mm grid, but this has

    nothing to do with the Schematic drawing.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 17 years ago

    Bjørn Birkeland schrieb:

    Is the elektro-library based on inch or mm grid? The german tutorial says

    that inch-grid should be used. I've expected the Germans to use mm in their

    drawing standard for elektro schemes. Thought IEC-standards used the metric

    system.

    //Bjørn, Norway

     

     

     

    The inch grid is the default in the EAGLE Schematic editor. This

    is for historic reasons. All Symbols in the electronic (and also

    in the electrical) libraries are drawn in 0.1 inch grid.

    Of course the hardware is mostly made in mm grid, but this has

    nothing to do with the Schematic drawing.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm