Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Problem in moving parts after routing!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 189 subscribers
  • Views 1007 views
  • Users 0 members are here
Related

Problem in moving parts after routing!

e14 Contributor
e14 Contributor over 12 years ago

Hi all, can anyone help with my slight problem.

 

I have created a layout, used the ratsnest function to clear up the paths and then hit autoroute to generate the tracks. All is good at this point.

I then needed to move some of the component positions. Moving the parts is causing the tracks to folow very odd paths and hiting ratsnest is not correcting the problem.

 

Am I right in thinking that the ratsnest function will not work after an autoroute function has taken place?

 

How do I fix this?

 

(I hope my explanation is not too vague)

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 12 years ago

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/89396#89396

     

    Ratsnest affects only the airwires (well polygons too).

    You will need to manually unroute the undesired tracks and then you can

    autoroute or manually route.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • thomaser
    thomaser over 12 years ago in reply to autodeskguest

    When you ripup the traces to reroute, be mindful of the small fragments that sometimes popup that are buried in the pad as it snaps to your routing grid. They can be particularly frustrating at times. I see them pop up where vias were placed as well and they may be on inner layers. They may require ripping up a via and rerouting to eliminate the unwanted fragment. I use the practive when manually routing to connect until the ratsnest shows nothing to do. I route all my boards manually due to autorouters not being able to handle the type of signals and circuits I work with.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • thomaser
    thomaser over 12 years ago in reply to autodeskguest

    When you ripup the traces to reroute, be mindful of the small fragments that sometimes popup that are buried in the pad as it snaps to your routing grid. They can be particularly frustrating at times. I see them pop up where vias were placed as well and they may be on inner layers. They may require ripping up a via and rerouting to eliminate the unwanted fragment. I use the practive when manually routing to connect until the ratsnest shows nothing to do. I route all my boards manually due to autorouters not being able to handle the type of signals and circuits I work with.