EAGLE User Chat (English) Inverted silk
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
  • Replies 3 replies
  • Subscribers 179 subscribers
  • Views 442 views
  • Users 0 members are here
Related

Inverted silk

autodeskguest
autodeskguest over 17 years ago

Hi guys,

 

Is there any existing idea or ULP to easily make inverted (negative) top

silk layer (or any).

Thanks in advance.

 

Zoly

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Zoly wrote:

    I export the positive image file - then use a graphics package to invert

    the PCB area and print using MS-Paint (only because it allows you to

    declare the dpi print so you can get the right scale/size) For graphic

    edit I use a geriatric but excellent program - paint shop pro 4... image

    Anton

     

    Thanks for your input, I will try out your the paint shop version.

    In the mean time, I had trouble with MS-paint (I though about this since it

    has the direct inverting function built in), but the fairly large exported

    monocolor BMP file to keep the detailed result is continuously crashing the

    MS-paint on my "not actually low end PC" (core2 duo 6800 Extreme with 4G

    ram, and lots of HDD, fully updated winXP-pro.)

    Also I called the board house, and asked them if they could do the inverted

    silk, they did not say no, but they stated this will create a huge delay

    caused by possible confusion in the CAM department, multi pre-approvals have

    to be presented, involving regional sales guy too ......blah.... (not the

    easy way)

     

    I am still seeking a possible ULP, that someone might have came across with.

     

    Best Regards,

    Zoly

     

     

    Hi Zoly,

     

    Try playing with eagle's export (File - Export - Image) - you can

    specify the DPI there, depending on the detail in your pcb, you may be

    able to get away with a lower DPI - say 200 or so which will reduce your

    file size. From the browse button you can also change the format from

    bmp (which is big) to say PNG or Tiff which have lossless compression.

    Select the layer you want as per printing. (I use eagle ver 4.16r2)

     

    Remember to set MS-Paint with the same DPI as you export the file with

    .. sounds obvious but ...

     

    Hope that helps... image

     

    Kind regards

    Anton

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Zoly wrote:

    I export the positive image file - then use a graphics package to invert

    the PCB area and print using MS-Paint (only because it allows you to

    declare the dpi print so you can get the right scale/size) For graphic

    edit I use a geriatric but excellent program - paint shop pro 4... image

    Anton

     

    Thanks for your input, I will try out your the paint shop version.

    In the mean time, I had trouble with MS-paint (I though about this since it

    has the direct inverting function built in), but the fairly large exported

    monocolor BMP file to keep the detailed result is continuously crashing the

    MS-paint on my "not actually low end PC" (core2 duo 6800 Extreme with 4G

    ram, and lots of HDD, fully updated winXP-pro.)

    Also I called the board house, and asked them if they could do the inverted

    silk, they did not say no, but they stated this will create a huge delay

    caused by possible confusion in the CAM department, multi pre-approvals have

    to be presented, involving regional sales guy too ......blah.... (not the

    easy way)

     

    I am still seeking a possible ULP, that someone might have came across with.

     

    Best Regards,

    Zoly

     

     

    Hi Zoly,

     

    Try playing with eagle's export (File - Export - Image) - you can

    specify the DPI there, depending on the detail in your pcb, you may be

    able to get away with a lower DPI - say 200 or so which will reduce your

    file size. From the browse button you can also change the format from

    bmp (which is big) to say PNG or Tiff which have lossless compression.

    Select the layer you want as per printing. (I use eagle ver 4.16r2)

     

    Remember to set MS-Paint with the same DPI as you export the file with

    .. sounds obvious but ...

     

    Hope that helps... image

     

    Kind regards

    Anton