EAGLE User Chat (English) gerber data
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
  • Replies 5 replies
  • Subscribers 177 subscribers
  • Views 489 views
  • Users 0 members are here
Related

gerber data

autodeskguest
autodeskguest over 17 years ago

Hi,

 

I am experimenting with changing the drill sizes when running

drillcfg.ulp, to use fewer drills, I've edited some of the drills

the same, and then run excellon.cam and gerb274x.cam.

 

T01 0.016in

T02 0.028in

T03 0.028in

T04 0.040in

T05 0.040in

T06 0.050in

T07 0.055in

T08 0.055in

T09 0.070in

T10 0.070in

T11 0.087in

T12 0.087in

T13 0.100in

T14 0.120in

T15 0.120in

T16 0.140in

T17 0.170in

T18 0.236in

 

I am noticing when I load the *.cmp and *.drd gerbers in GC-Prevue that

the drill diameters don't match the values in the drl drill rack file.

 

After I generate the gerbers, the *.drd file still has these values at

the top of it for the drill diameters:

 

T01C0.0160

T02C0.0240

T03C0.0280

T04C0.0315

T05C0.0360

T06C0.0400

T07C0.0470

T08C0.0492

T09C0.0590

T10C0.0591

T11C0.0660

T12C0.0790

T13C0.0827

T14C0.1000

T15C0.1181

T16C0.1200

T17C0.1378

T18C0.1700

T19C0.2360

 

To save on drills, since editing the drl file didnt change the drd file

drills, should I make these drill diameter changes in the drd file after

the gerbers are generated?

 

cheers,

Jamie

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Richard Herman wrote:

    Jamie Morken schreef:

    Hi,

     

    I am experimenting with changing the drill sizes when running

    drillcfg.ulp, to use fewer drills, I've edited some of the drills

    the same, and then run excellon.cam and gerb274x.cam.

     

    T01 0.016in

    T02 0.028in

    T03 0.028in

    T04 0.040in

    T05 0.040in

    T06 0.050in

    T07 0.055in

    T08 0.055in

    T09 0.070in

    T10 0.070in

    T11 0.087in

    T12 0.087in

    T13 0.100in

    T14 0.120in

    T15 0.120in

    T16 0.140in

    T17 0.170in

    T18 0.236in

     

    I am noticing when I load the *.cmp and *.drd gerbers in GC-Prevue that

    the drill diameters don't match the values in the drl drill rack file.

     

    After I generate the gerbers, the *.drd file still has these values at

    the top of it for the drill diameters:

     

    T01C0.0160

    T02C0.0240

    T03C0.0280

    T04C0.0315

    T05C0.0360

    T06C0.0400

    T07C0.0470

    T08C0.0492

    T09C0.0590

    T10C0.0591

    T11C0.0660

    T12C0.0790

    T13C0.0827

    T14C0.1000

    T15C0.1181

    T16C0.1200

    T17C0.1378

    T18C0.1700

    T19C0.2360

     

    To save on drills, since editing the drl file didnt change the drd file

    drills, should I make these drill diameter changes in the drd file after

    the gerbers are generated?

     

    cheers,

    Jamie

     

    Hello Jamie,

     

    Im not 100% sure about this but i believe that with versions > 4.12 you

    don't need (want) to use drillcfg.ulp. These values are included in the

    .drd when you run the post 4.12 version of excellon.cam. if you still

    want to use drilcfg.ulp you should try another excellon cam file (that

    doesn't include the drill info). Not sure how that is called though; I'm

    still on 4.09, so i am unable to check that.

     

    I am 100% sure that the subject came up before in this NG of the support

    NG. If you search you should find it.

     

    HTH

    Richard Herman.

     

     

    Thanks Tilmann and Richard, yes drillcfg.ulp isn't used by the

    excellon.cam in 4.16 onwards it looks like.

     

    cheers,

    Jamie

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Richard Herman wrote:

    Jamie Morken schreef:

    Hi,

     

    I am experimenting with changing the drill sizes when running

    drillcfg.ulp, to use fewer drills, I've edited some of the drills

    the same, and then run excellon.cam and gerb274x.cam.

     

    T01 0.016in

    T02 0.028in

    T03 0.028in

    T04 0.040in

    T05 0.040in

    T06 0.050in

    T07 0.055in

    T08 0.055in

    T09 0.070in

    T10 0.070in

    T11 0.087in

    T12 0.087in

    T13 0.100in

    T14 0.120in

    T15 0.120in

    T16 0.140in

    T17 0.170in

    T18 0.236in

     

    I am noticing when I load the *.cmp and *.drd gerbers in GC-Prevue that

    the drill diameters don't match the values in the drl drill rack file.

     

    After I generate the gerbers, the *.drd file still has these values at

    the top of it for the drill diameters:

     

    T01C0.0160

    T02C0.0240

    T03C0.0280

    T04C0.0315

    T05C0.0360

    T06C0.0400

    T07C0.0470

    T08C0.0492

    T09C0.0590

    T10C0.0591

    T11C0.0660

    T12C0.0790

    T13C0.0827

    T14C0.1000

    T15C0.1181

    T16C0.1200

    T17C0.1378

    T18C0.1700

    T19C0.2360

     

    To save on drills, since editing the drl file didnt change the drd file

    drills, should I make these drill diameter changes in the drd file after

    the gerbers are generated?

     

    cheers,

    Jamie

     

    Hello Jamie,

     

    Im not 100% sure about this but i believe that with versions > 4.12 you

    don't need (want) to use drillcfg.ulp. These values are included in the

    .drd when you run the post 4.12 version of excellon.cam. if you still

    want to use drilcfg.ulp you should try another excellon cam file (that

    doesn't include the drill info). Not sure how that is called though; I'm

    still on 4.09, so i am unable to check that.

     

    I am 100% sure that the subject came up before in this NG of the support

    NG. If you search you should find it.

     

    HTH

    Richard Herman.

     

     

    Thanks Tilmann and Richard, yes drillcfg.ulp isn't used by the

    excellon.cam in 4.16 onwards it looks like.

     

    cheers,

    Jamie