EAGLE User Chat (English) Schematic symbol and outline modification
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
  • Replies 4 replies
  • Subscribers 179 subscribers
  • Views 482 views
  • Users 0 members are here
Related

Schematic symbol and outline modification

autodeskguest
autodeskguest over 17 years ago

Dear,

    I would like to ask you for something. How can I modify the

schematic symbol(and outline) of the part (I mean delete pin, add pin,

move pin)? When I want to modify one its pin, the program writes: "Can't

delete Pin from a Symbol that is in use!". What I should do to modify

(delete, add, move) pin? What I should do to make this symbol not be "in

use!"?

 

Thanks Jefik (jefik.wz.cz)

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Joerg schrieb:

    Ing. J.M. Rafetseder wrote:

    This can be done only in the lib-editor. First you have to remove the

    device, then do your changes & build the device again. Further details

    see the manual.

    r

     

    And if it is used in more than one device the better option may be to

    declare a new symbol, copy the old one over, edit to your heart's

    desire, create a new device, add the new symbol to it, add the old

    package (or a new one if needed) and connect everything. It's a little

    work but becomes routine over time.

     

    IMHO it's not a good thing to mess with devices, packages or symbols if

    they have already been used in a schematic. Even if it was only one

    schematic. Make a new part.

     

    Yes to all. And even make a new library! Modifying an original lib is

    IMHO not a good idea, because in case of an update the old version is

    overwritten and all your work on libs is lost.

     

    --

    Gruß

     

    Jörn

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Joerg schrieb:

    Ing. J.M. Rafetseder wrote:

    This can be done only in the lib-editor. First you have to remove the

    device, then do your changes & build the device again. Further details

    see the manual.

    r

     

    And if it is used in more than one device the better option may be to

    declare a new symbol, copy the old one over, edit to your heart's

    desire, create a new device, add the new symbol to it, add the old

    package (or a new one if needed) and connect everything. It's a little

    work but becomes routine over time.

     

    IMHO it's not a good thing to mess with devices, packages or symbols if

    they have already been used in a schematic. Even if it was only one

    schematic. Make a new part.

     

    Yes to all. And even make a new library! Modifying an original lib is

    IMHO not a good idea, because in case of an update the old version is

    overwritten and all your work on libs is lost.

     

    --

    Gruß

     

    Jörn