EAGLE User Chat (English) Newbie: How do I put component on bottom side of board ?
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
  • Replies 7 replies
  • Subscribers 179 subscribers
  • Views 522 views
  • Users 0 members are here
Related

Newbie: How do I put component on bottom side of board ?

autodeskguest
autodeskguest over 17 years ago

Beginner looking to place a connector on the bottom side of the board.  How

do i do this ?  I intend to sandwich two boards together using a 12 pin SIL

connector (header on one board and plug on the other).

Thanks in advance.

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    John wrote:

    Beginner looking to place a connector on the bottom side of the

    board.  How do i do this ?  I intend to sandwich two boards together

    using a 12 pin SIL connector (header on one board and plug on the

    other). Thanks in advance.

     

    Mirror

     

    --

    Bert

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago in reply to autodeskguest

    On Fri, 24 Oct 2008 08:03:28 -0400, "Bert Menkveld" <bert@betech.biz>

    wrote:

     

    John wrote:

    Beginner looking to place a connector on the bottom side of the

    board.  How do i do this ?  I intend to sandwich two boards together

    using a 12 pin SIL connector (header on one board and plug on the

    other). Thanks in advance.

     

    Mirror

     

    That seems more like a workaround than the proper way.  Is that the

    most appropriate way, within the capabilities of Eagle?  Or is it the

    only way?

     

    I ask this because doing  it that way is problematic.  When you put a

    surface mount on top, and then a surface mount on bottome, you can

    route between the two, and the ratsnests disappear, as if the

    connection was made, but the connections aren't actually made.

     

    To connect a surface layer pad between top and bottom requires a via.

    But when I test this, one can draw a route (not wire) between two

    connecting pads, and the vias disappear.   How does one verify

    connections if this is the case?

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago in reply to autodeskguest

    On Fri, 24 Oct 2008 08:03:28 -0400, "Bert Menkveld" <bert@betech.biz>

    wrote:

     

    John wrote:

    Beginner looking to place a connector on the bottom side of the

    board.  How do i do this ?  I intend to sandwich two boards together

    using a 12 pin SIL connector (header on one board and plug on the

    other). Thanks in advance.

     

    Mirror

     

    That seems more like a workaround than the proper way.  Is that the

    most appropriate way, within the capabilities of Eagle?  Or is it the

    only way?

     

    I ask this because doing  it that way is problematic.  When you put a

    surface mount on top, and then a surface mount on bottome, you can

    route between the two, and the ratsnests disappear, as if the

    connection was made, but the connections aren't actually made.

     

    To connect a surface layer pad between top and bottom requires a via.

    But when I test this, one can draw a route (not wire) between two

    connecting pads, and the vias disappear.   How does one verify

    connections if this is the case?