EAGLE User Chat (English) Newbie: How do I put component on bottom side of board ?
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
  • Replies 7 replies
  • Subscribers 179 subscribers
  • Views 521 views
  • Users 0 members are here
Related

Newbie: How do I put component on bottom side of board ?

autodeskguest
autodeskguest over 17 years ago

Beginner looking to place a connector on the bottom side of the board.  How

do i do this ?  I intend to sandwich two boards together using a 12 pin SIL

connector (header on one board and plug on the other).

Thanks in advance.

 

 

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    John wrote:

    Beginner looking to place a connector on the bottom side of the

    board.  How do i do this ?  I intend to sandwich two boards together

    using a 12 pin SIL connector (header on one board and plug on the

    other). Thanks in advance.

     

    Mirror

     

    --

    Bert

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Mirror reverses, but how does eagle know that the component is now on the

    bottom side of the board?  (it seems to do this automatically with surface

    mounts but how does it know with leaded components) ? ie. if i want to put

    my SIL connector on the bottom, if i just use the mirror command, will the

    connector now be on the bottom ?  Maybe look at it from manufacturing.  If i

    give my design to a boardmaker, how they know if the connector is on top of

    board or bottom ?

     

    Thanks

    "Bert Menkveld" <bert@betech.biz> wrote in message

    news:gdsdio$al0$1@cheetah.cadsoft.de...

    John wrote:

    Beginner looking to place a connector on the bottom side of the

    board.  How do i do this ?  I intend to sandwich two boards together

    using a 12 pin SIL connector (header on one board and plug on the

    other). Thanks in advance.

     

    Mirror

     

    --

    Bert

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    John wrote:

    Mirror reverses, but how does eagle know that the component is now on the

    bottom side of the board?  (it seems to do this automatically with surface

    mounts but how does it know with leaded components) ? ie. if i want to put

    my SIL connector on the bottom, if i just use the mirror command, will the

    connector now be on the bottom ?  Maybe look at it from manufacturing.  If i

    give my design to a boardmaker, how they know if the connector is on top of

    board or bottom ?

     

    Thanks

    You have to add that info to the design notes you use for manufacturing

    or have silkscreen on both sides. I have used a dashed silkscreen on the

    component side for circuit side mounted parts. If you wave solder those

    holes need to be masked and parts added manually later. So adding a new

    layer showing the parts of the board that need solder masking agents

    applied before wave would help make sure the documentation is not

    overlooked.

     

    Paul R.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Great.  Thanks Paul.  Appreciate it.

     

    "Paul Romanyszyn" <pgr@arcelectronicsinc.com> wrote in message

    news:gdsl4p$d8f$1@cheetah.cadsoft.de...

    John wrote:

    Mirror reverses, but how does eagle know that the component is now on the

    bottom side of the board?  (it seems to do this automatically with

    surface mounts but how does it know with leaded components) ? ie. if i

    want to put my SIL connector on the bottom, if i just use the mirror

    command, will the connector now be on the bottom ?  Maybe look at it from

    manufacturing.  If i give my design to a boardmaker, how they know if the

    connector is on top of board or bottom ?

     

    Thanks

    You have to add that info to the design notes you use for manufacturing or

    have silkscreen on both sides. I have used a dashed silkscreen on the

    component side for circuit side mounted parts. If you wave solder those

    holes need to be masked and parts added manually later. So adding a new

    layer showing the parts of the board that need solder masking agents

    applied before wave would help make sure the documentation is not

    overlooked.

     

    Paul R.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago in reply to autodeskguest

    On Fri, 24 Oct 2008 08:03:28 -0400, "Bert Menkveld" <bert@betech.biz>

    wrote:

     

    John wrote:

    Beginner looking to place a connector on the bottom side of the

    board.  How do i do this ?  I intend to sandwich two boards together

    using a 12 pin SIL connector (header on one board and plug on the

    other). Thanks in advance.

     

    Mirror

     

    That seems more like a workaround than the proper way.  Is that the

    most appropriate way, within the capabilities of Eagle?  Or is it the

    only way?

     

    I ask this because doing  it that way is problematic.  When you put a

    surface mount on top, and then a surface mount on bottome, you can

    route between the two, and the ratsnests disappear, as if the

    connection was made, but the connections aren't actually made.

     

    To connect a surface layer pad between top and bottom requires a via.

    But when I test this, one can draw a route (not wire) between two

    connecting pads, and the vias disappear.   How does one verify

    connections if this is the case?

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Mike wrote:

    On Fri, 24 Oct 2008 08:03:28 -0400, "Bert Menkveld" <bert@betech.biz>

    wrote:

     

    John wrote:

    Beginner looking to place a connector on the bottom side of the

    board.  How do i do this ?  I intend to sandwich two boards together

    using a 12 pin SIL connector (header on one board and plug on the

    other). Thanks in advance.

     

    Mirror

     

    That seems more like a workaround than the proper way.  Is that the

    most appropriate way, within the capabilities of Eagle?  Or is it the

    only way?

     

    That really is the "proper" way.  I don't know of any other way to place a

    component on the bottom of the board.

     

    I ask this because doing  it that way is problematic.  When you put a

    surface mount on top, and then a surface mount on bottome, you can

    route between the two, and the ratsnests disappear, as if the

    connection was made, but the connections aren't actually made.

     

    To connect a surface layer pad between top and bottom requires a via.

    But when I test this, one can draw a route (not wire) between two

    connecting pads, and the vias disappear.   How does one verify

    connections if this is the case?

     

    Hmmm, I'm afraid I don't really understand what's happening here.  I have

    routed SMT components on both sides of the board, and have not encountered

    the sort of misbehaviour you're describing.  Things do tend to get more

    confusing when you have parts on both sides of the board.

     

    If you can't figure out what's happening, maybe you could post a small

    sample board so we can see the problem you're describing.

     

    --

    Bert Menkveld

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    On Mon, 15 Dec 2008 07:48:24 -0500, "Bert Menkveld" <bert@betech.biz>

    wrote:

     

    Mike wrote:

    On Fri, 24 Oct 2008 08:03:28 -0400, "Bert Menkveld" <bert@betech.biz>

    wrote:

     

    John wrote:

    Beginner looking to place a connector on the bottom side of the

    board.  How do i do this ?  I intend to sandwich two boards together

    using a 12 pin SIL connector (header on one board and plug on the

    other). Thanks in advance.

     

    Mirror

     

    That seems more like a workaround than the proper way.  Is that the

    most appropriate way, within the capabilities of Eagle?  Or is it the

    only way?

     

    That really is the "proper" way.  I don't know of any other way to place a

    component on the bottom of the board.

     

    I ask this because doing  it that way is problematic.  When you put a

    surface mount on top, and then a surface mount on bottome, you can

    route between the two, and the ratsnests disappear, as if the

    connection was made, but the connections aren't actually made.

     

    To connect a surface layer pad between top and bottom requires a via.

    But when I test this, one can draw a route (not wire) between two

    connecting pads, and the vias disappear.   How does one verify

    connections if this is the case?

     

    Hmmm, I'm afraid I don't really understand what's happening here.  I have

    routed SMT components on both sides of the board, and have not encountered

    the sort of misbehaviour you're describing.  Things do tend to get more

    confusing when you have parts on both sides of the board.

     

    If you can't figure out what's happening, maybe you could post a small

    sample board so we can see the problem you're describing.

     

    Oops! My mistake.  Because you were so sure this would work, I checked

    it again.  There actually still is a ratsnest line.  It's just very

    short, from the end of the top surface part to the pad on the bottom

    surface part.  I was expecting to see the ratsnest from the original

    pin to the 2nd pin. 

     

    The other indication that mirror works is that when I do use the via,

    the trace will auto complete when I end on the 2nd pad.  Doesn't do

    that if I try this without a via. .  I don't use boards with

    components on both sides (yet but have one planned) so I guess I

    jumped to a false conclusion. Sorry.