EAGLE User Chat (English) how do I make ... :)  a via with 2 PAD on Top and on Bottom
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
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 245 views
  • Users 0 members are here
Related

how do I make ... :)  a via with 2 PAD on Top and on Bottom

Former Member
Former Member over 17 years ago

humm... that's a tecnical problem.

 

I have made a board with 2 side. Top and Bottom.

Very well.

Some signals needs to have a PAD on top and bottom.

Very well.

But I can sold only on bottom!!!

 

image that's probably a basic question.

When we sold a pin, very well, the soldery goes though the hole and solds

top and bottom pad and the pin ???

 

Is it the way it works ?

 

Best Pierre.

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Morgan Leijström schrieb:

    Pierre Ghislain wrote:

    humm... that's a tecnical problem.

     

    I have made a board with 2 side. Top and Bottom.

    Very well.

    Some signals needs to have a PAD on top and bottom.

    Very well.

    But I can sold only on bottom!!!

     

    image that's probably a basic question.

    When we sold a pin, very well, the soldery goes though the hole and

    solds top and bottom pad and the pin ???

     

    Is it the way it works ?

     

    Best Pierre.

     

    When a board house make the boards they metallise the inner surface of

    the holes.  This make it easy for solder to flow, and also a makes a

    very strong mechanical joint to the board material.

     

    When you drill a hole in the board you just take material away. So there

    is no metallic connection between the top and bottom layer.

    A pcb manufacturer inserts a tiny metal pipe into this hole, a rivet, as

    Morgan described before.

    So you have to arrange your layout in such a way that connections to

    those parts are allways on the bottom side.

    A way to your own via is to stick a piece of wire throuh the hole and

    solder it to both sides.

    Another way is for DIL-ICs, not to push it in all the way but only that

    far that the pins show about 1mm at the bottom and then solder both

    sides. Of course this trick does not work on everything.

     

    --

    Gruß / regards

     

    Jörn

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Morgan Leijström schrieb:

    Pierre Ghislain wrote:

    humm... that's a tecnical problem.

     

    I have made a board with 2 side. Top and Bottom.

    Very well.

    Some signals needs to have a PAD on top and bottom.

    Very well.

    But I can sold only on bottom!!!

     

    image that's probably a basic question.

    When we sold a pin, very well, the soldery goes though the hole and

    solds top and bottom pad and the pin ???

     

    Is it the way it works ?

     

    Best Pierre.

     

    When a board house make the boards they metallise the inner surface of

    the holes.  This make it easy for solder to flow, and also a makes a

    very strong mechanical joint to the board material.

     

    When you drill a hole in the board you just take material away. So there

    is no metallic connection between the top and bottom layer.

    A pcb manufacturer inserts a tiny metal pipe into this hole, a rivet, as

    Morgan described before.

    So you have to arrange your layout in such a way that connections to

    those parts are allways on the bottom side.

    A way to your own via is to stick a piece of wire throuh the hole and

    solder it to both sides.

    Another way is for DIL-ICs, not to push it in all the way but only that

    far that the pins show about 1mm at the bottom and then solder both

    sides. Of course this trick does not work on everything.

     

    --

    Gruß / regards

     

    Jörn