EAGLE User Chat (English) How to place topside pad over a bottomside pad
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
  • Replies 4 replies
  • Subscribers 179 subscribers
  • Views 374 views
  • Users 0 members are here
Related

How to place topside pad over a bottomside pad

autodeskguest
autodeskguest over 17 years ago

I need to make a new component for an Optek OP124 pill pack diode.  This is

a tiny bullet shaped package designed to be placed in a hole drilled between

the top and bottom sides.  Tthe top side is anode, the bottom side is

cathode.  There must be no plating in the hole.

 

I can place an SMD pad on the bottom layer and another SMD pad on the top

layer.  I can then place a hole of 1.8mm diameter through the pair of pads.

If I place the pads exactly over one another I cannot name the pads.  If  I

displace them 0.1 mm I can then name the pads.

 

When I try to route the component, EAGLE shows the air wires going to the

correct places but it never draws the traces and fails to route.  I have

tried AUTO with grids down to 1 thousandth but it never routes.

 

Any been able to make a component that goes inside the board between solder

and component layers?

 

Cheers

Brian

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    On Tue, 25 Nov 2008, BrianT wrote to us saying :

    I have sent the board to CustomPCB in Malaysia WITHOUT the two drill

    files you mention.

     

    The board house I use don't actually require two separate drill files,

    but they do require that I note which drill numbers are PTH and which

    are not. So far this has worked fine, but I could imagine a potential

    problem if I had the same size hole in both types.

    --

    Rob Pearce                       http://www.bdt-home.demon.co.uk

     

    The contents of this | Windows NT crashed.

    message are purely   | I am the Blue Screen of Death.

    my opinion. Don't    | No one hears your screams.

    believe a word.      |

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    On Tue, 25 Nov 2008, BrianT wrote to us saying :

    I have sent the board to CustomPCB in Malaysia WITHOUT the two drill

    files you mention.

     

    The board house I use don't actually require two separate drill files,

    but they do require that I note which drill numbers are PTH and which

    are not. So far this has worked fine, but I could imagine a potential

    problem if I had the same size hole in both types.

    --

    Rob Pearce                       http://www.bdt-home.demon.co.uk

     

    The contents of this | Windows NT crashed.

    message are purely   | I am the Blue Screen of Death.

    my opinion. Don't    | No one hears your screams.

    believe a word.      |