EAGLE User Chat (English) resistors network
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
  • Replies 5 replies
  • Subscribers 177 subscribers
  • Views 638 views
  • Users 0 members are here
Related

resistors network

autodeskguest
autodeskguest over 17 years ago

Can anybody explain me the difference between RN networks and RNX? I can't

understans which one is bussed network, which one is isolated network...

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Joern Paschedag wrote:

    John Giddy schrieb:

    Kail wrote:

    Can anybody explain me the difference between RN networks and RNX? I

    can't understans which one is bussed network, which one is isolated

    network...

     

    The RNX10 appears to be a series string of resistors. I am not sure

    what the RN10 series represents, as it has only one resistor.

    (This is in the "resistor-net.lbr")

    So I share your confusion.

    Maybe best to make your own library part ?

    John G.

     

    Never heard of a bunch of Transistors on a single chip?

    Now a Resistor Network is almost the same. It just means a certain

    amount of Resistors with equal values in a single device.

    There are usually two different RN-circuits: either single resistors or

    resistors with one side tied together.

    In eagle 5-3.x resistor-net.lbr the first two devices CTS742C083 and

    CTS753DRT16 show an example of the inner circuits.

    Yes and there are diodes networks too.... image

     

     

    I am well aware of what resistor networks usually look like. It is just

    that the schematic for the RN-10 in that library distributed with 4.16

    is very confusing, as it shows only a single resistor connected to pins

    1 and 2, and then pairs of pins with no resistors. "Invoke" comes up

    with a message that there is only one resistor.

    The RNX-10 shows 10 resistors connected to pins in a manner which

    indicates a series string, not a set of resistors with a common connection.

    John G.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Joern Paschedag wrote:

    John Giddy schrieb:

    Kail wrote:

    Can anybody explain me the difference between RN networks and RNX? I

    can't understans which one is bussed network, which one is isolated

    network...

     

    The RNX10 appears to be a series string of resistors. I am not sure

    what the RN10 series represents, as it has only one resistor.

    (This is in the "resistor-net.lbr")

    So I share your confusion.

    Maybe best to make your own library part ?

    John G.

     

    Never heard of a bunch of Transistors on a single chip?

    Now a Resistor Network is almost the same. It just means a certain

    amount of Resistors with equal values in a single device.

    There are usually two different RN-circuits: either single resistors or

    resistors with one side tied together.

    In eagle 5-3.x resistor-net.lbr the first two devices CTS742C083 and

    CTS753DRT16 show an example of the inner circuits.

    Yes and there are diodes networks too.... image

     

     

    I am well aware of what resistor networks usually look like. It is just

    that the schematic for the RN-10 in that library distributed with 4.16

    is very confusing, as it shows only a single resistor connected to pins

    1 and 2, and then pairs of pins with no resistors. "Invoke" comes up

    with a message that there is only one resistor.

    The RNX-10 shows 10 resistors connected to pins in a manner which

    indicates a series string, not a set of resistors with a common connection.

    John G.