Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) How to create a SMD pushbutton device with 2 pins and 4 pads?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 175 subscribers
  • Views 1051 views
  • Users 0 members are here
Related

How to create a SMD pushbutton device with 2 pins and 4 pads?

autodeskguest
autodeskguest over 16 years ago

Hi,

 

I'm relatively new to Eagle and HW design in general. I'm trying to create a

symbol and package for a SMD push button.

 

The pushbutton symbol has 2 pins, while the package has 4 smd pads. Pads 1

and 2 are electrically connected, and so are pads 3 and 4. When I create

the Eagle device, then the number of pins and pads obviously don't match.

 

Now I could:

 

1) leave 2 pads in the package unconnected.

2) generate a symbol with 4 pins and leave 2 pins unconnected in the

schematic.

 

How can I tell Eagle that two pads are always connected together? It would

be nice if I had only two pins but could route to any of the equivalent pads

and leave the other unconnected, but I cannot think of a way to accomplish

this. Is there a way to do so? Alternatively, what is the 'conventional'

way of handling this in Eagle?

 

Thanks,

Thomas

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 16 years ago

    Carsten wrote:

     

    Hi Thomas,

     

    the best way is to create a symbol with four pins and connect all of the to

    the package. If you assign the direction "pas" == passive to them, it will

    cause no DRC error if not all pins are connected. This way leaves you more

    choices. You may come to the point where you want to use the unconnected

    pins. Then you have to go the library again. Better first time right.

     

    There is no way to tell eagle that pins are connected to each other. This

    must be done in the schematic editor.

     

    You may take a look at the switch.lbr there are some parts with internal

    connected pins.

     

    Regards,

    Carsten

     

     

     

    I second this.

     

    It also gives pissibility to use the switch as jumper.

    For example I feed it the net +5V, and on the other side I name the net +5VB

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 16 years ago

    Carsten wrote:

     

    Hi Thomas,

     

    the best way is to create a symbol with four pins and connect all of the to

    the package. If you assign the direction "pas" == passive to them, it will

    cause no DRC error if not all pins are connected. This way leaves you more

    choices. You may come to the point where you want to use the unconnected

    pins. Then you have to go the library again. Better first time right.

     

    There is no way to tell eagle that pins are connected to each other. This

    must be done in the schematic editor.

     

    You may take a look at the switch.lbr there are some parts with internal

    connected pins.

     

    Regards,

    Carsten

     

     

     

    I second this.

     

    It also gives pissibility to use the switch as jumper.

    For example I feed it the net +5V, and on the other side I name the net +5VB