EAGLE User Chat (English) Custom pads...
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
  • Replies 6 replies
  • Subscribers 179 subscribers
  • Views 490 views
  • Users 0 members are here
Related

Custom pads...

autodeskguest
autodeskguest over 17 years ago

Hi there

 

I need to make a pad for this kind of pin:

http://www.pc-elektronik.dk/images/FSP.JPG

 

I have made it like this:

http://www.mespilus.dk/pad.gif

 

Is there a better way to design the pad than this? it is a combination of a

bottom SMD and two pads.

 

Peter

 

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    "Ing. J.M. Rafetseder" <jrafetseder@hotmail.com> wrote in message

    news:gkvppa$88u$1@cheetah.cadsoft.de...

    What about miling 2 short slots (using layer 46)? This was often discussed

    earlier in the groups. Talk to your boardhouse. Individual shape of pads

    is long on our wishlist ...

    r

     

    Yes, this is really needed somewhere down the Eagle versions priorities

    list. I asked about this a while back, and the only solution was to use

    polygons to create the copper layer "drawing" around pads or pins, such as

    might be needed when a custom shaped copper heat sink must be copper

    connected to a pad or pin with or without using a trace (perhaps for

    impedance reasons). The price is having to tell Eagle to ignore the DRC

    "overlap" errors (i.e., "approve" them), but I think the approvals are

    persistent between sessions of a newly loaded existing project unless the

    affected part gets removed and then put back into an existing project.

    Still, I think it best practice if the library designer includes a note in a

    library doc layer, and the library preview itself, indicating which DRC

    "overlap" errors must be approved for a device package used in a project.

     

    ==> It would be nice if the library itself could somehow keep a designer

    specified list of allowed overlap errors and DRC could look at that library

    list and automatically approve them.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    "Ing. J.M. Rafetseder" <jrafetseder@hotmail.com> wrote in message

    news:gkvppa$88u$1@cheetah.cadsoft.de...

    What about miling 2 short slots (using layer 46)? This was often discussed

    earlier in the groups. Talk to your boardhouse. Individual shape of pads

    is long on our wishlist ...

    r

     

    Yes, this is really needed somewhere down the Eagle versions priorities

    list. I asked about this a while back, and the only solution was to use

    polygons to create the copper layer "drawing" around pads or pins, such as

    might be needed when a custom shaped copper heat sink must be copper

    connected to a pad or pin with or without using a trace (perhaps for

    impedance reasons). The price is having to tell Eagle to ignore the DRC

    "overlap" errors (i.e., "approve" them), but I think the approvals are

    persistent between sessions of a newly loaded existing project unless the

    affected part gets removed and then put back into an existing project.

    Still, I think it best practice if the library designer includes a note in a

    library doc layer, and the library preview itself, indicating which DRC

    "overlap" errors must be approved for a device package used in a project.

     

    ==> It would be nice if the library itself could somehow keep a designer

    specified list of allowed overlap errors and DRC could look at that library

    list and automatically approve them.