EAGLE User Chat (English) default via - how to set?
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
  • Replies 1 reply
  • Subscribers 178 subscribers
  • Views 298 views
  • Users 0 members are here
Related

default via - how to set?

autodeskguest
autodeskguest over 16 years ago

I wanted to make the default via placed with a 0.5 mm drill and a round

shape. How / where is this set? The current default is a square pad and 0.6

mm drill.

 

tia - oppie

 

 

  • Sign in to reply
  • Cancel
  • Richard_H
    Richard_H over 16 years ago

    Oppie schrieb:

    I wanted to make the default via placed with a 0.5 mm drill and a round

    shape. How / where is this set? The current default is a square pad and

    0.6 mm drill.

     

    tia - oppie

     

     

     

    You could define it in eagle.scr, BRD: section:

     

    CHANGE SHAPE ROUND;

    CHANGE DRILL 0.6mm;

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm