EAGLE User Chat (English) What was default <CTL>+S
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
  • Replies 2 replies
  • Subscribers 179 subscribers
  • Views 313 views
  • Users 0 members are here
Related

What was default <CTL>+S

autodeskguest
autodeskguest over 16 years ago

This hurts to have to ask, but here it is:

 

I have been using a script file to load optimal linewidth, grid, pad

diameter (etc.) menu choices for the different editors whenever I open a new

file. (This is another method of loading parameters into the "Options

Assign" menu, of course.)

 

This would overwrite any default Eagle commands if they used the same key

combinations. I believe I overwrote the default +S into the "Options Assign" menu?

 

Thanks.

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 16 years ago

    Brett Holden schrieb:

    This hurts to have to ask, but here it is:

     

    I have been using a script file to load optimal linewidth, grid, pad

    diameter (etc.) menu choices for the different editors whenever I open a new

    file. (This is another method of loading parameters into the "Options

    Assign" menu, of course.)

     

    This would overwrite any default Eagle commands if they used the same key

    combinations. I believe I overwrote the default <CTL>+S. Now I can't get it

    back because I can't find the correct syntax.

     

    I think I remember reading about it in the ver 5.0 Readme or Release Notes,

    but I have not been able to find it in documentation of subsequent versions.

    I really do not want to go back and load ver 5.0 just to find the correct

    syntax for default <CTL>+S. Is it "Save File;" "Save File" "Save All;" or

    anything similar? I get error messages with everything I try.

     

    Is or was this a documented feature, or is it something I only imagined? I

    can't find it in current documentation. How do I load the default command

    (if there is one) for <CTL>+S into the "Options Assign" menu?

     

    Thanks.

     

     

     

    If you want to assign Ctrl + S with the Save command:

     

    ASSIGN C+S 'WRITE;';

     

    WRITE is the command that saves the current file.

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 16 years ago

    Brett Holden schrieb:

    This hurts to have to ask, but here it is:

     

    I have been using a script file to load optimal linewidth, grid, pad

    diameter (etc.) menu choices for the different editors whenever I open a new

    file. (This is another method of loading parameters into the "Options

    Assign" menu, of course.)

     

    This would overwrite any default Eagle commands if they used the same key

    combinations. I believe I overwrote the default <CTL>+S. Now I can't get it

    back because I can't find the correct syntax.

     

    I think I remember reading about it in the ver 5.0 Readme or Release Notes,

    but I have not been able to find it in documentation of subsequent versions.

    I really do not want to go back and load ver 5.0 just to find the correct

    syntax for default <CTL>+S. Is it "Save File;" "Save File" "Save All;" or

    anything similar? I get error messages with everything I try.

     

    Is or was this a documented feature, or is it something I only imagined? I

    can't find it in current documentation. How do I load the default command

    (if there is one) for <CTL>+S into the "Options Assign" menu?

     

    Thanks.

     

     

     

    If you want to assign Ctrl + S with the Save command:

     

    ASSIGN C+S 'WRITE;';

     

    WRITE is the command that saves the current file.

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm