Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Eagle Software
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 45 replies
  • Subscribers 191 subscribers
  • Views 5013 views
  • Users 0 members are here
  • eagle
  • software
Related

Eagle Software

e14 Contributor
e14 Contributor over 12 years ago

Greetings

 

My name is Brian, and I am a new user of Eagle, for right now the free version.

 

First question, is there any way to stop Eagle from carrying on point to point connections.   I am sure at times this is a very useful feature, but I need it to stop after automatically after it connects 2 points.   I hope this is possible, as if this is a persistent feature, it will really turn me off to Eagle.

 

But more importantly, I did a practice design and have a problem.

 

I am using a XF2H-3415 surface mount connector, .5 mm spacing.   I have a bit of a problem with the datasheet, as it doesn't clearly state the measurement units, but since the first page notes a measurement in mm, I'm assuming they are smart enough to carry those units throughout the datasheet.

 

Let me describe what I did, and perhaps did not do.

 

I have my board layout done, I have two 12 pin single row headers on each side of the board, and the other connector on the other side.   And I see the Ratsnest.

 

I think the pad color denotes side of board, but I'm not sure how to check or change that.

 

This is where the confusion starts.

 

I can't get the autorouter to start, and I come up with 34 DRC errors.

 

I'm a beginner, probably making a silly mistake, but Eagle also has a much more complicated set of DRC rules than I'm used to.

 

I have attached an image.

 

Help is most appreciated.

 

Thanks

 

Brian K

BKM Engineering

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Thanks for all your help so far.

     

    How do I change the units to Metric.   Is it possible?   Is it possible to make it default?

     

    I made the following changes:   DRC/ Sizes/ Minimum Width/5mil

     

    I got rid of all my errors.

     

    If I run ERC on schematic, 28 warnings, and no errors.

     

    If I run DRC on the board with the setting at 5mils, as mentioned previously, I do not get any errors.   Things are improving.

     

    Now I want to Autoroute, and I have what is referred to as the Freemium version.

     

    If I try to autoroute it appears to try to start, but it flashes momentarily and finishes with 0% routed.

     

    Can somebody identify what I'm obviously doing wrong.

     

    Thanks

     

    Brian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago

    Thanks for all your help so far.

     

    How do I change the units to Metric.   Is it possible?   Is it possible to make it default?

     

    I made the following changes:   DRC/ Sizes/ Minimum Width/5mil

     

    I got rid of all my errors.

     

    If I run ERC on schematic, 28 warnings, and no errors.

     

    If I run DRC on the board with the setting at 5mils, as mentioned previously, I do not get any errors.   Things are improving.

     

    Now I want to Autoroute, and I have what is referred to as the Freemium version.

     

    If I try to autoroute it appears to try to start, but it flashes momentarily and finishes with 0% routed.

     

    Can somebody identify what I'm obviously doing wrong.

     

    Thanks

     

    Brian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • AnalogNotes
    AnalogNotes over 12 years ago in reply to e14 Contributor

    Brian Mcclung wrote:

    How do I change the units to Metric.   Is it possible?

     

    The answer is in the manual: GRID command

     

    Is it possible to make it default?

     

    Please refer to the eagle.scr that I mentioned above.  Second section of the EAGLE manual: Configuring EAGLE  See the subsection on Mode Parameters...

     

    It may help you if you navigate to the bin directory of your EAGLE installation and double click on the file eagle_en.htm.  That will open the EAGLE manual in your web browser.  Sections are hyperlinked together and I have found that the HTML version of the manual is a great resource...