Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Eagle Software
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 45 replies
  • Subscribers 191 subscribers
  • Views 4950 views
  • Users 0 members are here
  • eagle
  • software
Related

Eagle Software

e14 Contributor
e14 Contributor over 12 years ago

Greetings

 

My name is Brian, and I am a new user of Eagle, for right now the free version.

 

First question, is there any way to stop Eagle from carrying on point to point connections.   I am sure at times this is a very useful feature, but I need it to stop after automatically after it connects 2 points.   I hope this is possible, as if this is a persistent feature, it will really turn me off to Eagle.

 

But more importantly, I did a practice design and have a problem.

 

I am using a XF2H-3415 surface mount connector, .5 mm spacing.   I have a bit of a problem with the datasheet, as it doesn't clearly state the measurement units, but since the first page notes a measurement in mm, I'm assuming they are smart enough to carry those units throughout the datasheet.

 

Let me describe what I did, and perhaps did not do.

 

I have my board layout done, I have two 12 pin single row headers on each side of the board, and the other connector on the other side.   And I see the Ratsnest.

 

I think the pad color denotes side of board, but I'm not sure how to check or change that.

 

This is where the confusion starts.

 

I can't get the autorouter to start, and I come up with 34 DRC errors.

 

I'm a beginner, probably making a silly mistake, but Eagle also has a much more complicated set of DRC rules than I'm used to.

 

I have attached an image.

 

Help is most appreciated.

 

Thanks

 

Brian K

BKM Engineering

Attachments:
image
  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 12 years ago in reply to e14 Contributor

    On 14/03/14 11:23, Brian Mcclung wrote:

    Yes Rob, I agree, how stupid of me.

     

    Why would I not expect Eagle to impose a limit on me based upon an

    action I have never performed: Adjusting the rules you carefully worked

    out to suit a component you picked on a whim.

     

    Do me a favor!

     

    Do yourself a favour and READ THE ADVICE YOU ARE GIVEN.

     

    We are not here to waste our time on your personal whinge-fest. If you

    want to know why things are as they are, and somebody answers that

    question, rejecting an answer you don't like with sarcasm is incredibly

    rude and obnoxious. Please grow up.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to AnalogNotes

    Maybe to aid placement, a quick check of board or edge-part spacing.

     

    I just don't see how it can be used for a quick a-b measurement.

     

    It seems to pick its own points automatically, or at least one of them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to dukepro

    Here is where I'm having a problem with the design rules.

     

    This particular part that was giving me problems was obsolete 7 years ago.  It has been replaced with the M model, but the spacing is the same.   This particular obsolete part has been around 10 years.

     

    What legitimate board house could not handle that spacing.

     

    So let me retract my question, why are the DRC rules not self adjusting.   I could further debate the point, but I wont.

     

    I never changed the DRC rules.

     

    Now my question is this.

     

    Why would Eagle default to parameters that don't reflect current manufacturing capabilities.

     

    Is that spacing really beyond typical manufacturing capability?

     

    If it isn't, I was caused unnecessary trouble by the parameters it defaulted to.

     

    Thank you for your response.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • AnalogNotes
    AnalogNotes over 12 years ago in reply to e14 Contributor

    What exactly are you trying to do with the dimensioning tool?  I've never thought of it as anything more than icing on the cake, just a way to put measurements on a page for a human to read...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 12 years ago in reply to e14 Contributor

    On 03/13/2014 08:26 PM, Brian Mcclung wrote:

    Hi Chuck

     

    I'm still having the same problem, but other questions first.

     

    How do you change the units.

    How do you define the grid in such a way that your measurement steps are

    smaller than the area to be measured.

    As Doug mentioned, you can use the grid command.  Try "grid mil 5" to

    set the snap to every 5 mils, or "grid mil 1" to set it to 1 mil.  You

    can go smaller or larger to suit your needs.  You can also append a

    second integer to this that affects the display of the grid.  Try "grid

    mil 1 5".  This will set your snap to 1 mil, and the grid display to

    every 5 snaps (5 mils).  "grid mil 5 5" will set the snap to 5 mils, and

    the display to 5 snaps (25 mils).

     

    You can also specify other units, such as mm or in.

    Back to my original problem.

     

    I checked the parameter I think you specified, and the size is already

    set to 10 mils.

     

    Well, that's the source of the DRC problems.  If the pads are on .5mm

    spacing, and each pad is .25mm wide, that leaves only .25mm of spacing.

    That converts to 9.8 mils.  Try setting the size to 9 mils.

     

    This also means that the wire coming off the pad must be less than 9.8

    mils - a 10 mil trace will create a DRC clearance error.

     

    What I want to know is if these errors are caused by a design rule, why

    is Eagle not self adjusting to what is a standard part.

    That would be making assumptions about the capabilities of the board fab

    house, and your design limitations.

    Why is Eagle not self adjusting, and is this going to be a persistent

    feature when using Eagle.  Is this something that every time I do a

    board, I am going to have to go in adjust my design rules?

    Basically, yes.  If you are using all PTH components, there's no need

    for such tight tolerances.  For SMD designs, obviously the fab

    requirements have small tolerances.  I'm sure you can change the default

    design rules for new designs, but I don't know where that would be done.

     

    HTH,

        - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to autodeskguest

    Hi Warren

     

    I'm actually impressed with this.

     

    SET CONTEXT WIRE STOP ';';

     

    But I would say some of these Eagle features should be more visible to the user.

     

    But here is another problem, and I can't even figure out why anybody would want it to work this way.

     

    If you place a hole or a via or a dimension, once you start, there is nothing you can do with the "mouse" to get it to stop.   WTF?

     

    I can understand why it has been broken down into these discrete steps.   Every designer is a robot trying to do things at the speed of light, and all those things being drug around will disappear as soon as you click on something else, so you learn to ignore it.

     

    I guess I need  a keyboard shortcut to get it to stop under those 3 cases.

     

    After that, where is the 1 hour webcast showing how to use the dimensioning tool, because I don't appear to have any control over what it measures.

     

    EDA software always has that remarkably charming characteristic of making you feel like an idiot trying to do something simple.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to autodeskguest

    Yes Rob, I agree, how stupid of me.

     

    Why would I not expect Eagle to impose a limit on me based upon an action I have never performed: Adjusting the rules you carefully worked out to suit a component you picked on a whim.

     

    Do me a favor!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago in reply to e14 Contributor

    On 14/03/14 06:22, Brian Mcclung wrote:

    The same way I can't understand why Eagle can't auto adjust it's DRC

    rules to standard components,

     

    Because there's no such thing!

     

    The design rules are there to impose limits on what you are allowed to

    do - things like "no tracks thinner than 0.01 inches" or "no gaps

    narrower than 0.005 inches". These are not universal - they depend on

    your chosen board house's capability (and all professional PCB fabs are

    much better than home etch, which Eagle can cope with).

     

    If you are fitting an EM11B rotary encoder with two sets of through-hole

    pins at 0.05" (1.27mm) spacing on a board you intend to etch yourself,

    the only sensible thing for Eagle to do is TELL YOU that it's not going

    to work. Adjusting the rules you carefully worked out to suit a

    component you picked on a whim would be catastrophically stupid.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 12 years ago in reply to e14 Contributor

    Hi Brian,

    please go to the Options/Window positons... menu in the EAGLE Control Panel. There you can adjust the inital size and position of the editor windows.

     

    Concerning the Stop button: Well usually don't have to quit a command. Simply activate the nex command and it works. If you want to stop a command you could also use the  semicolon ;  in the command line.

     

    HTH

    Regards,

    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago in reply to e14 Contributor

    On 14/03/2014 8:44 p.m., Brian Mcclung wrote:

     

     

    Now, the stop function, if I have a button selected, say info, and I

    want to get everything reset so no button along the left hand side is

    active, the only way I see is to go to the upper toolbar and click stop.

     

    There doesn't appear to be a keyboard shortcut, like escape, or a

    de-select function.  I'd even be happy if it was added to the right

    click context menu.

     

     

    There are a lot of different ways to do things in Eagle.

     

    If you don't like using the mouse to click the 'Stop' icon you can type

    a semicolon in the command line and hit enter.

     

    You could activate the default Text menu and click on the semicolon it

    offers

     

    You could add a context menu so you can stop via a right click. Like the

    following one. Type this into the command line

     

     

    SET CONTEXT WIRE STOP ';';

     

    Now when you right click on a wire in the editor you set the context

    menu in you will see the selection 'Stop' . Click that to stop.

     

    You could assign a key to perform the stop

     

    HTH

    Warren

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>