Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Eagle Software
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 45 replies
  • Subscribers 191 subscribers
  • Views 5008 views
  • Users 0 members are here
  • eagle
  • software
Related

Eagle Software

e14 Contributor
e14 Contributor over 12 years ago

Greetings

 

My name is Brian, and I am a new user of Eagle, for right now the free version.

 

First question, is there any way to stop Eagle from carrying on point to point connections.   I am sure at times this is a very useful feature, but I need it to stop after automatically after it connects 2 points.   I hope this is possible, as if this is a persistent feature, it will really turn me off to Eagle.

 

But more importantly, I did a practice design and have a problem.

 

I am using a XF2H-3415 surface mount connector, .5 mm spacing.   I have a bit of a problem with the datasheet, as it doesn't clearly state the measurement units, but since the first page notes a measurement in mm, I'm assuming they are smart enough to carry those units throughout the datasheet.

 

Let me describe what I did, and perhaps did not do.

 

I have my board layout done, I have two 12 pin single row headers on each side of the board, and the other connector on the other side.   And I see the Ratsnest.

 

I think the pad color denotes side of board, but I'm not sure how to check or change that.

 

This is where the confusion starts.

 

I can't get the autorouter to start, and I come up with 34 DRC errors.

 

I'm a beginner, probably making a silly mistake, but Eagle also has a much more complicated set of DRC rules than I'm used to.

 

I have attached an image.

 

Help is most appreciated.

 

Thanks

 

Brian K

BKM Engineering

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • dukepro
    dukepro over 12 years ago

    Good morning, Brian,

     

    On 03/13/2014 01:49 AM, Brian Mcclung wrote:

    ...

    First question, is there any way to stop Eagle from carrying on point to

    point connections.

     

    Not sure of your context here.  If it has to do with the autorouter, I

    can't help.  I don't use it.

     

    I am using a XF2H-3415 surface mount connector, .5 mm spacing.

    ...

    I have my board layout done, I have two 12 pin single row headers on

    each side of the board, and the other connector on the other side.   And

    I see the Ratsnest.

     

    I think the pad color denotes side of board, but I'm not sure how to

    check or change that.

    The default colors are red for the top layer (layer 1), and blue for the

    bottom layer (layer 16).  All SMD parts are designed in the library to

    go on the top.  The part can then be mirrored in the board design to

    place it on the bottom.

     

    This is where the confusion starts.

     

    I can't get the autorouter to start,and I come up with 34 DRC errors.

    The Width error you're getting is because the pads are narrower than the

    minimum width setting in DRC.  Go to DRC=>Sizes and change the minimum

    width.  The datasheet recommends a 0.25mm minimum width.  Go ahead and

    enter "0.25mm" in this field and click Apply.

     

    In general, the DRC settings should be the greater of the limitations of

    the board fabrication house, and your design requirements.  Each fab

    house should publish these limitations, usually under "capabilities".

     

    DRC also pays attention to your Class settings.  Each net can be

    assigned a Class that describes further restrictions on wires of that

    class.  DRC will use the greater of the values assigned in the DRC

    settings and those of the net's class.  For instance, your DRC settings

    may define a minimum trace width of 8 mils, and a minimum clearance of 8

    mils, which is fine for signal level wires.  Our designs sometimes use

    high voltages close to 3,000 V.  I assign HV nets to a "HighVoltage"

    class and force a clearance of 40 mils.

     

    You may wish to add a high current class for power supply wires and give

    them a relatively large width and drill size.

     

    Your board layout alone does not indicate a need for such classes.

     

    As far as not being able to start the auto-router, this problem may be

    related to the fact that there's a DRC error on every pad.

     

    I'm a beginner, probably making a silly mistake, but Eagle also has a

    much more complicated set of DRC rules than I'm used to.

     

    There's one other very important point I need to make.  The hashed black

    and yellow bar across the top indicates that forward and back annotation

    has been severed.  This is caused by closing the schematic while working

    on the board, or vice versa.  When working on a design both the

    schematic and board editors should be open.  This allows changes to in

    one editor to be reflected in the other.

     

    To restore consistency, run "ERC" from .  The resulting report will

    identify the differences between the board and the schematic.  If there

    are any differences, these need to be fixed before consistency is restored.

     

    More of a personal preference, I would suggest using a black background

    on the board editor, and a white background on the schematic editor.

    This can be changed in Options=>User Interface.

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to dukepro

    Hi Chuck

     

    I'm still having the same problem, but other questions first.

     

    How do you change the units.

     

    How do you define the grid in such a way that your measurement steps are smaller than the area to be measured.

     

    Back to my original problem.

     

    I checked the parameter I think you specified, and the size is already set to 10 mils.

     

    But this is even more important, because I tend to be very critical of software.   I'm self taught, with help obviously, but software with a steep learning curve is very distasteful.

     

    What I want to know is if these errors are caused by a design rule, why is Eagle not self adjusting to what is a standard part.

     

    Why is Eagle not self adjusting, and is this going to be a persistent feature when using Eagle.  Is this something that every time I do a board, I am going to have to go in adjust my design rules?

     

    I'm really hoping I'm misunderstanding something here.

     

    Thanks

     

    Brian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 12 years ago in reply to e14 Contributor

    On 03/13/2014 08:26 PM, Brian Mcclung wrote:

    Hi Chuck

     

    I'm still having the same problem, but other questions first.

     

    How do you change the units.

    How do you define the grid in such a way that your measurement steps are

    smaller than the area to be measured.

    As Doug mentioned, you can use the grid command.  Try "grid mil 5" to

    set the snap to every 5 mils, or "grid mil 1" to set it to 1 mil.  You

    can go smaller or larger to suit your needs.  You can also append a

    second integer to this that affects the display of the grid.  Try "grid

    mil 1 5".  This will set your snap to 1 mil, and the grid display to

    every 5 snaps (5 mils).  "grid mil 5 5" will set the snap to 5 mils, and

    the display to 5 snaps (25 mils).

     

    You can also specify other units, such as mm or in.

    Back to my original problem.

     

    I checked the parameter I think you specified, and the size is already

    set to 10 mils.

     

    Well, that's the source of the DRC problems.  If the pads are on .5mm

    spacing, and each pad is .25mm wide, that leaves only .25mm of spacing.

    That converts to 9.8 mils.  Try setting the size to 9 mils.

     

    This also means that the wire coming off the pad must be less than 9.8

    mils - a 10 mil trace will create a DRC clearance error.

     

    What I want to know is if these errors are caused by a design rule, why

    is Eagle not self adjusting to what is a standard part.

    That would be making assumptions about the capabilities of the board fab

    house, and your design limitations.

    Why is Eagle not self adjusting, and is this going to be a persistent

    feature when using Eagle.  Is this something that every time I do a

    board, I am going to have to go in adjust my design rules?

    Basically, yes.  If you are using all PTH components, there's no need

    for such tight tolerances.  For SMD designs, obviously the fab

    requirements have small tolerances.  I'm sure you can change the default

    design rules for new designs, but I don't know where that would be done.

     

    HTH,

        - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    Come a long way since then!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to dukepro

    I really don't understand your response.

     

    I've not ignored, nor have I tried to be unappreciative of any advice or directions directly relevant to a problem I was trying to solve.

     

    But if you want to get into a debate about underlying philosophy and default settings, I'll take this as far you want.

     

    I'll call technical support from now on, open till 7pm est.

     

    I wont have to put up with their attitude, and they get paid to put up with mine.

     

    What do you think you offer that they can't?

     

    And who do you think you are to me.   I have helped plenty of people in my time I wouldn't spend 2 minutes with if I didn't have to.   You think you're any different?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 12 years ago in reply to e14 Contributor

    On 03/17/2014 12:09 PM, Brian Mcclung wrote:

    Hi Chuck

     

    I appreciate your response, but

     

    Nothing is going to make feel better about the way Eagle is defaulted.

    ...

    I appreciate your response, you told me how to change things.   You can

    do nothing more, please don't try.

     

    I won't.  It seems you've pretty much burned all your bridges here.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to dukepro

    Hi Chuck

     

    I appreciate your response, but

     

    Nothing is going to make feel better about the way Eagle is defaulted.   You could spend all day teaching me how to set up my design rules, I would certainly appreciate and learn something from it, but it wouldn't change my opinion about the default parameters.

     

    Perhaps the clue here is right in something you said.

     

    "But many of us use bench-top etching systems to fab our own

    boards.  I used to do this with PTH boards.  Once I moved to surface

    mount, I couldn't achieve the tolerances required so I've had to use a

    real board fab house."

     

    real board fab house?????

     

    Is this what Eagle is initially set up for, amateurs and hobbyists etching their own boards.

     

    Don't be insulted, hear me out.

     

    Perhaps when Eagle initializes, it might try setting itself for default rules according to how the user is going to have his boards made.

     

    Perhaps even a warning that the default rules don't reflect current manufacturing capabilities

     

    I appreciate your response, you told me how to change things.   You can do nothing more, please don't try.

     

    Sincerely

     

    Brian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 12 years ago in reply to e14 Contributor

    On 03/14/2014 02:03 PM, Brian Mcclung wrote:

    Here is where I'm having a problem with the design rules.

     

    This particular part that was giving me problems was obsolete 7 years

    ago.  It has been replaced with the M model, but the spacing is the

    same.   This particular obsolete part has been around 10 years.

     

    What legitimate board house could not handle that spacing.

     

    Most can.  But many of us use bench-top etching systems to fab our own

    boards.  I used to do this with PTH boards.  Once I moved to surface

    mount, I couldn't achieve the tolerances required so I've had to use a

    real board fab house.

     

    So let me retract my question, why are the DRC rules not self

    adjusting.   I could further debate the point, but I wont.

    Self adjusting to what?  Just automatically change the tolerances so DRC

    doesn't produce errors?  That would defeat the purpose of DRC.

     

    I never changed the DRC rules.

     

    Perhaps you should change them to what suits your design.  10 mil

    spacing is fine for PTH boards.  SMD boards clearly need smaller tolerances.

     

    Now my question is this.

     

    Why would Eagle default to parameters that don't reflect current

    manufacturing capabilities.

     

    Is that spacing really beyond typical manufacturing capability?

     

    If it isn't, I was caused unnecessary trouble by the parameters it

    defaulted to.

     

    If you don't like the defaults, change them.  You can do so through the

    control panel.  In the tree, expand Design Rules, double click

    default.dru and edit as necessary.

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to dukepro

    Here is where I'm having a problem with the design rules.

     

    This particular part that was giving me problems was obsolete 7 years ago.  It has been replaced with the M model, but the spacing is the same.   This particular obsolete part has been around 10 years.

     

    What legitimate board house could not handle that spacing.

     

    So let me retract my question, why are the DRC rules not self adjusting.   I could further debate the point, but I wont.

     

    I never changed the DRC rules.

     

    Now my question is this.

     

    Why would Eagle default to parameters that don't reflect current manufacturing capabilities.

     

    Is that spacing really beyond typical manufacturing capability?

     

    If it isn't, I was caused unnecessary trouble by the parameters it defaulted to.

     

    Thank you for your response.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to dukepro

    Here is where I'm having a problem with the design rules.

     

    This particular part that was giving me problems was obsolete 7 years ago.  It has been replaced with the M model, but the spacing is the same.   This particular obsolete part has been around 10 years.

     

    What legitimate board house could not handle that spacing.

     

    So let me retract my question, why are the DRC rules not self adjusting.   I could further debate the point, but I wont.

     

    I never changed the DRC rules.

     

    Now my question is this.

     

    Why would Eagle default to parameters that don't reflect current manufacturing capabilities.

     

    Is that spacing really beyond typical manufacturing capability?

     

    If it isn't, I was caused unnecessary trouble by the parameters it defaulted to.

     

    Thank you for your response.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor

    Come a long way since then!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to dukepro

    I really don't understand your response.

     

    I've not ignored, nor have I tried to be unappreciative of any advice or directions directly relevant to a problem I was trying to solve.

     

    But if you want to get into a debate about underlying philosophy and default settings, I'll take this as far you want.

     

    I'll call technical support from now on, open till 7pm est.

     

    I wont have to put up with their attitude, and they get paid to put up with mine.

     

    What do you think you offer that they can't?

     

    And who do you think you are to me.   I have helped plenty of people in my time I wouldn't spend 2 minutes with if I didn't have to.   You think you're any different?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 12 years ago in reply to e14 Contributor

    On 03/17/2014 12:09 PM, Brian Mcclung wrote:

    Hi Chuck

     

    I appreciate your response, but

     

    Nothing is going to make feel better about the way Eagle is defaulted.

    ...

    I appreciate your response, you told me how to change things.   You can

    do nothing more, please don't try.

     

    I won't.  It seems you've pretty much burned all your bridges here.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to dukepro

    Hi Chuck

     

    I appreciate your response, but

     

    Nothing is going to make feel better about the way Eagle is defaulted.   You could spend all day teaching me how to set up my design rules, I would certainly appreciate and learn something from it, but it wouldn't change my opinion about the default parameters.

     

    Perhaps the clue here is right in something you said.

     

    "But many of us use bench-top etching systems to fab our own

    boards.  I used to do this with PTH boards.  Once I moved to surface

    mount, I couldn't achieve the tolerances required so I've had to use a

    real board fab house."

     

    real board fab house?????

     

    Is this what Eagle is initially set up for, amateurs and hobbyists etching their own boards.

     

    Don't be insulted, hear me out.

     

    Perhaps when Eagle initializes, it might try setting itself for default rules according to how the user is going to have his boards made.

     

    Perhaps even a warning that the default rules don't reflect current manufacturing capabilities

     

    I appreciate your response, you told me how to change things.   You can do nothing more, please don't try.

     

    Sincerely

     

    Brian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 12 years ago in reply to e14 Contributor

    On 03/14/2014 02:03 PM, Brian Mcclung wrote:

    Here is where I'm having a problem with the design rules.

     

    This particular part that was giving me problems was obsolete 7 years

    ago.  It has been replaced with the M model, but the spacing is the

    same.   This particular obsolete part has been around 10 years.

     

    What legitimate board house could not handle that spacing.

     

    Most can.  But many of us use bench-top etching systems to fab our own

    boards.  I used to do this with PTH boards.  Once I moved to surface

    mount, I couldn't achieve the tolerances required so I've had to use a

    real board fab house.

     

    So let me retract my question, why are the DRC rules not self

    adjusting.   I could further debate the point, but I wont.

    Self adjusting to what?  Just automatically change the tolerances so DRC

    doesn't produce errors?  That would defeat the purpose of DRC.

     

    I never changed the DRC rules.

     

    Perhaps you should change them to what suits your design.  10 mil

    spacing is fine for PTH boards.  SMD boards clearly need smaller tolerances.

     

    Now my question is this.

     

    Why would Eagle default to parameters that don't reflect current

    manufacturing capabilities.

     

    Is that spacing really beyond typical manufacturing capability?

     

    If it isn't, I was caused unnecessary trouble by the parameters it

    defaulted to.

     

    If you don't like the defaults, change them.  You can do so through the

    control panel.  In the tree, expand Design Rules, double click

    default.dru and edit as necessary.

     

    HTH,

        - Chuck