Does anyone know if there is a way to create an SCR for a library
part. I would like to use the pci express connector part from the
con-pci_exress(pci-e) library, but need to edit the the
entire dimension layer.
Is there a way to create an SCR from the library component so that the
'device' co-ordinates are extracted and can be edited or merged into
another SCR that also supplies the remaining dimensions.
Without the ability to 'import/build' the layout co-ordinates using
library device, the final layout must be a manual visual drop and
place on the board. I have looked around and talked to people but no
one I have asked seems to know of any scr to do this. Thank you.