EAGLE User Chat (English) is it possible create SCR for library part?
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
  • Replies 2 replies
  • Subscribers 179 subscribers
  • Views 403 views
  • Users 0 members are here
Related

is it possible create SCR for library part?

blewis999
blewis999 over 16 years ago

Does anyone know if there is a way to create an SCR for a library

part. I would like to use the pci express connector part from the

con-pci_exress(pci-e) library,  but need to edit the the

entire dimension layer.

 

Is there a way to create an SCR from the library component so that the

'device' co-ordinates are extracted and can be edited or merged into

another SCR that also supplies the remaining dimensions.

 

Without the ability to 'import/build' the layout co-ordinates using

library device, the final layout must be a manual visual drop and

place on the board. I have looked around and talked to people but no

one I have asked seems to know of any scr to do this. Thank you.

 

  • Sign in to reply
  • Cancel
Parents
  • blewis999
    blewis999 over 16 years ago

    That is perfect! Exactly what I was searching for. Thank you very

    much.

     

    Robert

     

    On Wed, 25 Feb 2009 08:51:51 +0200, Firat Kocak

    <firatkocak@iyte.edu.tr> wrote:

     

    Yes, there is. Run the Library Editor. Open the library file. And then

    use File/Export/Scr item. This will create a script for the entire

    library, not just the one you need.

     

    Firat,

     

    Robert Lewis wrote:

    Does anyone know if there is a way to create an SCR for a library

    part. I would like to use the pci express connector part from the

    con-pci_exress(pci-e) library,  but need to edit the the

    entire dimension layer.

     

    Is there a way to create an SCR from the library component so that the

    'device' co-ordinates are extracted and can be edited or merged into

    another SCR that also supplies the remaining dimensions.

     

    Without the ability to 'import/build' the layout co-ordinates using

    library device, the final layout must be a manual visual drop and

    place on the board. I have looked around and talked to people but no

    one I have asked seems to know of any scr to do this. Thank you.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • blewis999
    blewis999 over 16 years ago

    That is perfect! Exactly what I was searching for. Thank you very

    much.

     

    Robert

     

    On Wed, 25 Feb 2009 08:51:51 +0200, Firat Kocak

    <firatkocak@iyte.edu.tr> wrote:

     

    Yes, there is. Run the Library Editor. Open the library file. And then

    use File/Export/Scr item. This will create a script for the entire

    library, not just the one you need.

     

    Firat,

     

    Robert Lewis wrote:

    Does anyone know if there is a way to create an SCR for a library

    part. I would like to use the pci express connector part from the

    con-pci_exress(pci-e) library,  but need to edit the the

    entire dimension layer.

     

    Is there a way to create an SCR from the library component so that the

    'device' co-ordinates are extracted and can be edited or merged into

    another SCR that also supplies the remaining dimensions.

     

    Without the ability to 'import/build' the layout co-ordinates using

    library device, the final layout must be a manual visual drop and

    place on the board. I have looked around and talked to people but no

    one I have asked seems to know of any scr to do this. Thank you.