Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Eagle Board layout question from newbie
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 188 subscribers
  • Views 1352 views
  • Users 0 members are here
  • tstop
Related

Eagle Board layout question from newbie

e14 Contributor
e14 Contributor over 12 years ago

Hello,

 

When i add a package to my board layout, i got tStop thingies (donno what they are)

that do not move with the package

i can't even select them

 

how could i delete these ?

 

thx

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Hi Rompel,
    Click on the "show" option in the toolbar (denoted by an "eye" symbol) and check for the connectivity. If connectivity is there then it will be seen in light green color , so check whether all the pins are connected properly or not. Also try putting junctions (green dot in toolbar) at junctions. This had helped me many times. Moreover, u can check for pin overlaps bcoz many times pins overlap with wires which are not visible when u see the whole circuit, you have to zoom in to see the components legs and see if they are overlapping.

     

    Regards,
    Dishant Mehta

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago

    Hi Rompel,
    Click on the "show" option in the toolbar (denoted by an "eye" symbol) and check for the connectivity. If connectivity is there then it will be seen in light green color , so check whether all the pins are connected properly or not. Also try putting junctions (green dot in toolbar) at junctions. This had helped me many times. Moreover, u can check for pin overlaps bcoz many times pins overlap with wires which are not visible when u see the whole circuit, you have to zoom in to see the components legs and see if they are overlapping.

     

    Regards,
    Dishant Mehta

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    i am pretty sure that eagle is complaining about two outputs being linked together, witch (in general) is not meant to be in an electronic schema

    it is not a design (junction/wires/pin overlap) issue

     

    but thanks i'll keep your advices in mind :-)