EAGLE User Chat (English) Is is possible to do a 16 position BGA on 4 layer board?
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
  • Replies 3 replies
  • Subscribers 179 subscribers
  • Views 462 views
  • Users 0 members are here
Related

Is is possible to do a 16 position BGA on 4 layer board?

blewis999
blewis999 over 16 years ago

Can someone please advise me on whether it is possible to use a BGA on

a 4 layer board? The center layers ares Vdd and Gnd. So the signal

layers are top and bottom.

 

The Ball Grid Array is only 4x4 or 16 pins, with a .4mm pitch and ball

of .29mm/.26mm/.23mm (I don't understand this either, is that the max,

avg, min size??).

 

I have read through the posts, created the device but can't get it to

route for the two center rows. There is a lot of room on the board.

But just looking at the grid I can't really see how to get the auto

router to do this unless there is a way to do a drill hole in the

center of the Ball and plate that through to the opposite side.

 

But I have no clue on how to get this to work, any advice would be

appreciated. Thank you.

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 16 years ago

    blewis999 schrieb:

     

    The Ball Grid Array is only 4x4 or 16 pins, with a .4mm pitch and ball

    of .29mm/.26mm/.23mm

     

    Even routing this manually has some problems. I use a

    6mil trace and the pitch between the balls is .4mm, the max ball is

    .29mm, therefore there is a maximum of .11mm between the ball edges,

    or 2.7mil. How will this work with a 6 mill or even 5mil trace width?

    I also need clearance around the trace?

     

    I fear you'll need to contact the inner pads by plugged vias.

     

    (Assume a reasonable pad size of 0.3 mm, which gives you 0.1 mm between

    the pads. You could try to route a 40 µm track inbetween, with 30 µm

    clearance to both pads...)

     

    Talk to your board house to select a useful (and producable) technology.

    And/or try to avoid such extremely tiny packages...

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 16 years ago

    blewis999 schrieb:

     

    The Ball Grid Array is only 4x4 or 16 pins, with a .4mm pitch and ball

    of .29mm/.26mm/.23mm

     

    Even routing this manually has some problems. I use a

    6mil trace and the pitch between the balls is .4mm, the max ball is

    .29mm, therefore there is a maximum of .11mm between the ball edges,

    or 2.7mil. How will this work with a 6 mill or even 5mil trace width?

    I also need clearance around the trace?

     

    I fear you'll need to contact the inner pads by plugged vias.

     

    (Assume a reasonable pad size of 0.3 mm, which gives you 0.1 mm between

    the pads. You could try to route a 40 µm track inbetween, with 30 µm

    clearance to both pads...)

     

    Talk to your board house to select a useful (and producable) technology.

    And/or try to avoid such extremely tiny packages...

     

    Tilmann