Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Part on board does not match library
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 187 subscribers
  • Views 467 views
  • Users 0 members are here
Related

Part on board does not match library

autodeskguest
autodeskguest over 17 years ago

Using Eagle 5.5.0 licensed.  There is a through-hole connector in the library.

  Drill size is set then pad diameter adjusted to accommodate 0.18mm minimum

track spacing.  In the library it is fine but once on the board the pad

diameter becomes larger and violates the minimum track spacing.  If a change

is made in the library (e.g. use offset pads instead of square), track spacing

is fine in the library but the pads are again larger when the library is

updated on the board.  The only fix is to specify a smaller drill, marginal at

best.  Any suggestions?

 

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 17 years ago

    Alan schrieb:

    Using Eagle 5.5.0 licensed.  There is a through-hole connector in the

    library.  Drill size is set then pad diameter adjusted to accommodate

    0.18mm minimum track spacing.  In the library it is fine but once on the

    board the pad diameter becomes larger and violates the minimum track

    spacing.  If a change is made in the library (e.g. use offset pads

    instead of square), track spacing is fine in the library but the pads

    are again larger when the library is updated on the board.  The only fix

    is to specify a smaller drill, marginal at best.  Any suggestions?

     

     

    See also  http://www.cadsoft.de/faq.htm.en#06012601

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 17 years ago

    Alan schrieb:

    Using Eagle 5.5.0 licensed.  There is a through-hole connector in the

    library.  Drill size is set then pad diameter adjusted to accommodate

    0.18mm minimum track spacing.  In the library it is fine but once on the

    board the pad diameter becomes larger and violates the minimum track

    spacing.  If a change is made in the library (e.g. use offset pads

    instead of square), track spacing is fine in the library but the pads

    are again larger when the library is updated on the board.  The only fix

    is to specify a smaller drill, marginal at best.  Any suggestions?

     

     

    See also  http://www.cadsoft.de/faq.htm.en#06012601

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm