Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) printing .brd's with 7.0.0 fails
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 188 subscribers
  • Views 966 views
  • Users 0 members are here
Related

printing .brd's with 7.0.0 fails

autodeskguest
autodeskguest over 12 years ago

Just updated to the freebie eagle-7.0.0

 

I have some work last massaged by 6.5.0 about 16 months ago, but my

printouts were incomplete when I looked and compared to the old board that

self-destructed last week, mainly from being made on radio shack pcb.

Fragile crap, poor copper adhesive & sub mill copper.  Very easily

destroyed despite the fact that I have had a soldering iron in one hand and

a scope probe in the other for well over 60 years now.

 

Doing my etching on a mill running linuxcnc, I have to add some stuff to

the pcb2gcode output to facilitate the automatic location and depth of cut.

All that is in o subroutines and once working, isn't germane to

this.

 

But in order to get a complete printout to facilitate parts placement on

the new board I made yesterday, I had to redo the autoroute.  Then I went

to print a copy to take to the shop. 5 passes at printing the new boards

brd image on a color laser printer, and I have 5 notices from the printer

that no data was found.  Gping to the .sch screen, that prints just fine.

 

Anybody have a clue why I cannot print the .brd image?

 

Cheers, Gene

--

Cheers, Gene

--

"There are four boxes to be used in defense of liberty:

soap, ballot, jury, and ammo. Please use in that order."

-Ed Howdershelt (Author)

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 12 years ago

    Chuckle, your mother is chasing me, I'll be 80 in October.  But luck is

    still me friend, I managed to survive a pulmonary embolism at the end of

    May, so now I am on rat poison, and feeling better than I have in a

    decade.

     

    and I found 2.5 square feet of DS 2 oz board on Ebay an hour ago for USD

    12$, free postal shipping.  I should have it the middle of next week.

     

    I tend to do my own for my onsies projects, in this case a spindle encoder

    for a sows ear toy lathe, a 7x12 that was new back in the 90's sometime.

    It now has ball screws and a 1 horse motor, all controlled by LinuxCNC.  No

    handles left, LCNC does it all. At 0.001" accuracy's these days.

     

    When doing a circuit board on the mill, which also has all screws now, run

    by LCNC, I usually drill the thru holes about.045" deep, and drill from

    both sides so the holes meet in the middle of the boards thickness. I think

    I'm doing good when I can look into the hole with an old 16mm projector

    lens for a magnifier, and cannot find a step where the hole pattern was

    miss aligned.  And its not my accuracy being tested, its the mills

    accuracy.  Worst part is I have no facility to make plated thru holes,

    which makes my eagle compositions trickier.  And the traces too darned

    narrow too. And I need to find a v-bit for engraving that is even a

    narrower angle than the 60 degree bits I have the last of in the machine

    right now.  Keeping the board pallet clean so there are no high or low

    spots would also help.  So would a constant temp, my Z screw is about 16"

    between the nut and the head slider, and in that distance, a 5 degree F

    temp change is 4 thou or so at the tip of the bit.  So I load eagles

    pcb2gcode output code up with calls to an automatic Z axis re-calibration,

    inserted at about 1000 line intervals.  But even that does not help if my

    hold-down screws distort the PCB itself because it runs the machine to the

    same spot on the board. I'd be better off to machine the pallet for a

    vacuum to hold it correctly.  Not impossible of course, but the vacuum is

    just more noise I can do w/o.  But I just had another idea on the vacuum

    that would be much quieter.  I forgot I had inherited an AC service pump,

    and I know that puppy can do better than 29.5" HG.  I used it to complete

    the desiccation of a gunstock sized piece of poorly dried maple, and one of

    my 50 cal BP's is now wearing it.  Gets the ohhs and ahhs at the range to,

    twice, the second time when they look at the target. image

     

    I'd better do an Andy Capp here and Saddup.

     

    Cheers, Gene

     

    --

    Cheers, Gene

    --

    "There are four boxes to be used in defense of liberty:

    soap, ballot, jury, and ammo. Please use in that order."

    -Ed Howdershelt (Author)

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago in reply to autodeskguest

    Gene77 wrote:

    Chuckle, your mother is chasing me, I'll be 80 in October.  But luck

    is

    still me friend, I managed to survive a pulmonary embolism at the end

    of

    May, so now I am on rat poison, and feeling better than I have in a

    decade.

     

    Glad you got through that!  I know a couple people who are on the rat

    poison, one is younger than me.  I'm on beta blockers and calcium channel

    blockers myself, along with diclofenac for the arthritis...

    ("arth-a-rite-us!")

     

    and I found 2.5 square feet of DS 2 oz board on Ebay an hour ago for

    USD 12$

     

    Very nice.  eBay sure seems to have turned into a giant store instead of an

    auction house.

     

    I tend to do my own for my onsies projects, in this case a spindle

    encoder

    for a sows ear toy lathe, a 7x12 that was new back in the 90's

    sometime.

    It now has ball screws and a 1 horse motor, all controlled by LinuxCNC.

    No

    handles left, LCNC does it all. At 0.001" accuracy's these days.

     

    Fun!  A thousandth, eh?  Nice.  I used to be a machinist, worked my way up

    to general manager of the shop.  At the time, we pretty much had to

    maintain .0005" accuracy.  At some point, maybe after I retire, I plan to

    get some kind of vertical mill and play with CNC stuff again.

     

    Worst part is I have no facility to make plated thru holes, which

    makes

    my eagle compositions trickier.

     

    I've often wondered if anyone makes any kind of little grommet that could

    be put in a hole and soldered to make a via.  Some day I'll actually get

    around to looking.  Maybe you could get some kind of thin tube and cut

    rings off with your lathe?  Hmm, could probably use some kind of solid

    stock as well if it were small enough.  Might take a lot of heat to solder

    though, but you could try solder paste and a griddle or oven...

     

    Keeping the board pallet clean so there are no high or low spots would

    also help.

     

    In woodworking, we use router bits with guide bearings.  I wonder if you

    could rig up something like that to hold the pcb down...

     

    I'd better do an Andy Capp here and Saddup.

     

    My dad used to love that strip!  I always remember Andy curled up on the

    couch asking Pet for things...

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago in reply to autodeskguest

    Gene77

    wrote:

    Chuckle, your mother is chasing me, I'll be 80 in October.  But luck

    is

    still me friend, I managed to survive a pulmonary embolism at the end

    of

    May, so now I am on rat poison, and feeling better than I have in a

    decade.

     

    Glad you got through that!  I know a couple people who are on the rat

    poison, one is younger than me.  I'm on beta blockers and calcium channel

    blockers myself, along with diclofenac for the arthritis...

    ("arth-a-rite-us!")

     

    I add a bunch of stuff to the rat poison, 20-25 Lisinopril for high blood

    pressure, metformin with my meals because I've been a DM-II for 30 years,

    adding the vitamins that flushes out, copious amounts of B-12 to control

    the leg cramps at night, ant-acid pills for the calcium on demand when the

    B12 doesn't work, and Lutein to prevent the blindness that goes with long

    term diabetic nerve damages.  And of course some OTC stuff in the

    Chondroitan family for the arthritis.  That's my major problem, because of

    collapsed disks etc, I am 6" shorter than 60 years ago, and stand with a

    noticeable tilt.  Scoliosis they call it. But I'm still here and feeling

    pretty good.  I always planned on living forever, and I seem to have made a

    good start so far image

     

    I finished out a career in electronics service with 24 years behind a door

    that said Chief Engineer on it at a tv station. Very little went back to

    the makers for repairs on my watch.  A bit over 18 years at the last

    station, local area, still have the keys to the place.

     

    and I found 2.5 square feet of DS 2 oz board on Ebay an hour ago for

    USD 12$

     

    Very nice.  eBay sure seems to have turned into a giant store instead of an

    auction house.

     

    Yeah, this was buy it now only.

     

    I tend to do my own for my onsies projects, in this case a spindle

    encoder

    for a sows ear toy lathe, a 7x12 that was new back in the 90's

    sometime.

    It now has ball screws and a 1 horse motor, all controlled by LinuxCNC.

    No

    handles left, LCNC does it all. At 0.001" accuracy's these days.

     

    Fun!  A thousandth, eh?  Nice.  I used to be a machinist, worked my way up

    to general manager of the shop.  At the time, we pretty much had to

    maintain .0005" accuracy.

     

    Yeah, but you had good machinery in the first place!  This was the junk I

    could afford. image

     

    At some point, maybe after I retire, I plan to get some kind of vertical

    mill and play with CNC stuff again.

     

    If you don't want to carve really tough stuff, it doesn't have enough iron

    for that, and mills that do cost lots more and weigh 200 kilo's more, the

    Grizzly G0704 is a good choice.  Not what one would call heavy duty, but

    ball screw conversion kits with all the mounting hardware are fairly

    reasonable on this side of the pond.  Just add motors, drivers, like the

    2m542, a 28 to 48 volt motor psu, a parport breakout board like a cnc4pc

    C1G, a dual core atom powered computer, and LCNC and you are off to the

    races.  Carving my last gunstock would have been buckets easier with its

    longer X table as even with the big table kits in my HF mill, I only have a

    12"x4.5"x14" work envelope.  The Go704 would give you about 18 to 19" of x

    motion.  That thing is sold on the other side of the pond with a model

    number like a BF-20 or BF-30 IIRC.

     

    I carve a lot of wood. I got a request from the neighbor for some furniture

    which was best done with a few hundred mortise & tenon joints, and did all

    that carving with my mill by attaching a 1/4" cheapo die grinder to the

    front of it, offset on a big alu arm about 8" left, so a stick could hang

    off clear off the table while getting its tenon milled.  Made stick holder

    jigs & wrote some GCode, had all the joints made in about 2 days.

     

    Worst part is I have no facility to make plated thru holes, which

    makes

    my eagle compositions trickier.

     

    I've often wondered if anyone makes any kind of little grommet that could

    be put in a hole and soldered to make a via.  Some day I'll actually get

    around to looking.

     

    No one does in the sizes we'ed need, I've looked.

     

    Maybe you could get some kind of thin tube and cut rings off with your

    lathe?  Hmm, could probably use some kind of solid stock as well if it were

    small enough.  Might take a lot of heat to solder though, but you could try

    solder paste and a griddle or oven...

     

    Keeping the board pallet clean so there are no high or low spots would

    also help.

     

    In woodworking, we use router bits with guide bearings.  I wonder if you

    could rig up something like that to hold the pcb down...

     

    I suppose a teflon pipe, spring loaded to put 5 lbs on the board could be

    rigged.  With some vent holes it might be possible to rig a small vacuum to

    suck up the debris so the teflon didn't grind it back into the board.  But

    remembering that I had the HV pump, I think a tubing connector drilled into

    the end of the micarta pallet, to intersect with a groove pattern milled

    into the bottom of the pocket, say on 1/4" centers with a 1/16" mill, could

    do it better.  Then I would only need one screw, to hold the electrical

    contact I hook the probing wire up to get a connection to the top copper on

    the board.  But that could also be replaced with a spring wire exerting far

    less pressure on the board that bends it than the present 4-40 hold down

    screw does. I have some hose, and I could recap the 6" white abs pipe I

    used to dry that stick of maple & use it for a vacuum reservoir so the pump

    would only get turned on when I see the gauge below 15" hg.

     

    I'd better do an Andy Capp here and Saddup.

     

    My dad used to love that strip!  I always remember Andy curled up on the

    couch asking Pet for things...

     

    Yeah, like peanuts, those are classic and still being syndicated on this

    side of the pond.

     

    And you were correct, it was the printer refusing to print the hashed

    marked areas. I took those out of the view, and it printed it just fine.

    My thoughts on that subject aren't fit for public display.  The

    repuglycrats are ruining a good country IMO.

     

    Unintended consequences.  The book I believe can be had from my web page.

    image

    --

    Cheers, Gene

    --

    "There are four boxes to be used in defense of liberty:

    soap, ballot, jury, and ammo. Please use in that order."

    -Ed Howdershelt (Author)

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 12 years ago in reply to autodeskguest

    Gene77

    wrote:

    Chuckle, your mother is chasing me, I'll be 80 in October.  But luck

    is

    still me friend, I managed to survive a pulmonary embolism at the end

    of

    May, so now I am on rat poison, and feeling better than I have in a

    decade.

     

    Glad you got through that!  I know a couple people who are on the rat

    poison, one is younger than me.  I'm on beta blockers and calcium channel

    blockers myself, along with diclofenac for the arthritis...

    ("arth-a-rite-us!")

     

    I add a bunch of stuff to the rat poison, 20-25 Lisinopril for high blood

    pressure, metformin with my meals because I've been a DM-II for 30 years,

    adding the vitamins that flushes out, copious amounts of B-12 to control

    the leg cramps at night, ant-acid pills for the calcium on demand when the

    B12 doesn't work, and Lutein to prevent the blindness that goes with long

    term diabetic nerve damages.  And of course some OTC stuff in the

    Chondroitan family for the arthritis.  That's my major problem, because of

    collapsed disks etc, I am 6" shorter than 60 years ago, and stand with a

    noticeable tilt.  Scoliosis they call it. But I'm still here and feeling

    pretty good.  I always planned on living forever, and I seem to have made a

    good start so far image

     

    I finished out a career in electronics service with 24 years behind a door

    that said Chief Engineer on it at a tv station. Very little went back to

    the makers for repairs on my watch.  A bit over 18 years at the last

    station, local area, still have the keys to the place.

     

    and I found 2.5 square feet of DS 2 oz board on Ebay an hour ago for

    USD 12$

     

    Very nice.  eBay sure seems to have turned into a giant store instead of an

    auction house.

     

    Yeah, this was buy it now only.

     

    I tend to do my own for my onsies projects, in this case a spindle

    encoder

    for a sows ear toy lathe, a 7x12 that was new back in the 90's

    sometime.

    It now has ball screws and a 1 horse motor, all controlled by LinuxCNC.

    No

    handles left, LCNC does it all. At 0.001" accuracy's these days.

     

    Fun!  A thousandth, eh?  Nice.  I used to be a machinist, worked my way up

    to general manager of the shop.  At the time, we pretty much had to

    maintain .0005" accuracy.

     

    Yeah, but you had good machinery in the first place!  This was the junk I

    could afford. image

     

    At some point, maybe after I retire, I plan to get some kind of vertical

    mill and play with CNC stuff again.

     

    If you don't want to carve really tough stuff, it doesn't have enough iron

    for that, and mills that do cost lots more and weigh 200 kilo's more, the

    Grizzly G0704 is a good choice.  Not what one would call heavy duty, but

    ball screw conversion kits with all the mounting hardware are fairly

    reasonable on this side of the pond.  Just add motors, drivers, like the

    2m542, a 28 to 48 volt motor psu, a parport breakout board like a cnc4pc

    C1G, a dual core atom powered computer, and LCNC and you are off to the

    races.  Carving my last gunstock would have been buckets easier with its

    longer X table as even with the big table kits in my HF mill, I only have a

    12"x4.5"x14" work envelope.  The Go704 would give you about 18 to 19" of x

    motion.  That thing is sold on the other side of the pond with a model

    number like a BF-20 or BF-30 IIRC.

     

    I carve a lot of wood. I got a request from the neighbor for some furniture

    which was best done with a few hundred mortise & tenon joints, and did all

    that carving with my mill by attaching a 1/4" cheapo die grinder to the

    front of it, offset on a big alu arm about 8" left, so a stick could hang

    off clear off the table while getting its tenon milled.  Made stick holder

    jigs & wrote some GCode, had all the joints made in about 2 days.

     

    Worst part is I have no facility to make plated thru holes, which

    makes

    my eagle compositions trickier.

     

    I've often wondered if anyone makes any kind of little grommet that could

    be put in a hole and soldered to make a via.  Some day I'll actually get

    around to looking.

     

    No one does in the sizes we'ed need, I've looked.

     

    Maybe you could get some kind of thin tube and cut rings off with your

    lathe?  Hmm, could probably use some kind of solid stock as well if it were

    small enough.  Might take a lot of heat to solder though, but you could try

    solder paste and a griddle or oven...

     

    Keeping the board pallet clean so there are no high or low spots would

    also help.

     

    In woodworking, we use router bits with guide bearings.  I wonder if you

    could rig up something like that to hold the pcb down...

     

    I suppose a teflon pipe, spring loaded to put 5 lbs on the board could be

    rigged.  With some vent holes it might be possible to rig a small vacuum to

    suck up the debris so the teflon didn't grind it back into the board.  But

    remembering that I had the HV pump, I think a tubing connector drilled into

    the end of the micarta pallet, to intersect with a groove pattern milled

    into the bottom of the pocket, say on 1/4" centers with a 1/16" mill, could

    do it better.  Then I would only need one screw, to hold the electrical

    contact I hook the probing wire up to get a connection to the top copper on

    the board.  But that could also be replaced with a spring wire exerting far

    less pressure on the board that bends it than the present 4-40 hold down

    screw does. I have some hose, and I could recap the 6" white abs pipe I

    used to dry that stick of maple & use it for a vacuum reservoir so the pump

    would only get turned on when I see the gauge below 15" hg.

     

    I'd better do an Andy Capp here and Saddup.

     

    My dad used to love that strip!  I always remember Andy curled up on the

    couch asking Pet for things...

     

    Yeah, like peanuts, those are classic and still being syndicated on this

    side of the pond.

     

    And you were correct, it was the printer refusing to print the hashed

    marked areas. I took those out of the view, and it printed it just fine.

    My thoughts on that subject aren't fit for public display.  The

    repuglycrats are ruining a good country IMO.

     

    Unintended consequences.  The book I believe can be had from my web page.

    image

    --

    Cheers, Gene

    --

    "There are four boxes to be used in defense of liberty:

    soap, ballot, jury, and ammo. Please use in that order."

    -Ed Howdershelt (Author)

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • autodeskguest
    autodeskguest over 12 years ago in reply to autodeskguest

    Gene77 wrote:

    I add a bunch of stuff to the rat poison, 20-25 Lisinopril

     

    I was on the max dose of Lisinopril myself, but it didn't help the bp and I

    got the dry cough.  I'm on Amlodipine (Norvasc) now.  Between that and the

    Metoprolol, the bp is down to about 130/90.  I'm guessing the doc will add

    some kind of diuretic next.

     

    (LOL, a couple guys comparing meds on an electronics forum!  I'll stop

    now...)

     

    If you don't want to carve really tough stuff, it doesn't have enough

    iron for that, and mills that do cost lots more and weigh 200 kilo's

    more, the Grizzly G0704 is a good choice.

     

    Looks like a nice little unit.  There's a good-sized used machinery

    business here, so I'm looking at a 9x42 Lagun (28"x16"x16" travel)

    actually...  image

     

    I carve a lot of wood. I got a request from the neighbor for some

    furniture

    which was best done with a few hundred mortise & tenon joints, and did

    all that carving with my mill by attaching a 1/4" cheapo die grinder

    to

    the front of it, offset on a big alu arm about 8" left, so a stick

    could

    hang off clear off the table while getting its tenon milled.  Made

    stick

    holder jigs & wrote some GCode, had all the joints made in about 2

    days.

     

    (whistles) 2 days?  Wonder if I could have done that with my Unisaw and

    router tables.  I mostly make boxes and cabinets though, so I spend a lot

    of time with my Leigh and Incra jigs...

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.