EAGLE User Chat (English) Design rules modifying package pad sizes?
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
  • Replies 4 replies
  • Subscribers 179 subscribers
  • Views 520 views
  • Users 0 members are here
Related

Design rules modifying package pad sizes?

autodeskguest
autodeskguest over 16 years ago

I'm pretty new to Eagle or any pcb designing software for that matter. I

was modifying a TO-220 3 pin package into a TO-220 5 pin (straight &

vertical) when I noticed the old pads (dia=auto, drill = 0.04, long)

were quite close together when all 5 are arranged. I need to keep the

drill size at 0.04 but I changed the diameter to 0.05". When I insert

the device with my custom package, the schematic editor alerts that the

library has modified my board and that I need to run the DRC. When I

look at the TO-220-5 package in the board view and compare it to the

TO-220-3 package, the TO-220-5 packge is using the old pad size and not

my new narrower pads. Any ideas on what is going on?

 

Also, any suggestions for a tutorial that explains the DRC settings? I'm

having a difficult time understanding some of the parameters.

 

Have a good one,

Matt

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 16 years ago

    looks like you've run into the "restring" problem. you can search the

    help or forums for more info, but this is a "VFAQ" topic.

     

    basically, in the DRC dialogs there are also settings for "restring"

    which determines the pad size on parts in a board. the library pads are

    (if I remember) the minimum sizes or something, check the help for real

    info.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 16 years ago

    looks like you've run into the "restring" problem. you can search the

    help or forums for more info, but this is a "VFAQ" topic.

     

    basically, in the DRC dialogs there are also settings for "restring"

    which determines the pad size on parts in a board. the library pads are

    (if I remember) the minimum sizes or something, check the help for real

    info.
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
An Avnet Company © 2025 Premier Farnell Limited. All Rights Reserved.