Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Two Eagle 7.1 Issues
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 188 subscribers
  • Views 584 views
  • Users 0 members are here
Related

Two Eagle 7.1 Issues

e14 Contributor
e14 Contributor over 11 years ago

OS=Win 8.1

 

#1) I have downloaded several additional libraries and they are showing in the listing of libraries folders. I have also selected the "Use All" function to activate them... However, when searching the libraries for a device, these new libraries are not being included... That is to say, I know the device I am looking for is included in the new libraries, but the device that I want is not showing as an option in the search results to select to add on the schematic.

 

#2) I have created a separate library folder for cataloging new devices that I build. I have created a new device with a package layer and a symbol layer. I have tied these layers to the new device. I have tried to connect the symbol layer to the package layer, but they just won't connect. I can find this new device in the in the libraries, but when I add it to the schematic, I only get the package without the symbols.

 

I have uninstalled and reinstalled.

 

Any suggestions?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    Thanks for the information, guys... #1 The solution was to use the browse feature to identify the location of the new libraries... I had cut and pasted the addresses... Seems Eagle didn't like that...#2 I will have to rebuild the library that I created and identify it with the browse feature.

     

    I appreciate your help.

     

    t1d

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 11 years ago

    Thanks for the information, guys... #1 The solution was to use the browse feature to identify the location of the new libraries... I had cut and pasted the addresses... Seems Eagle didn't like that...#2 I will have to rebuild the library that I created and identify it with the browse feature.

     

    I appreciate your help.

     

    t1d