Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Two Eagle 7.1 Issues
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 188 subscribers
  • Views 582 views
  • Users 0 members are here
Related

Two Eagle 7.1 Issues

e14 Contributor
e14 Contributor over 11 years ago

OS=Win 8.1

 

#1) I have downloaded several additional libraries and they are showing in the listing of libraries folders. I have also selected the "Use All" function to activate them... However, when searching the libraries for a device, these new libraries are not being included... That is to say, I know the device I am looking for is included in the new libraries, but the device that I want is not showing as an option in the search results to select to add on the schematic.

 

#2) I have created a separate library folder for cataloging new devices that I build. I have created a new device with a package layer and a symbol layer. I have tied these layers to the new device. I have tried to connect the symbol layer to the package layer, but they just won't connect. I can find this new device in the in the libraries, but when I add it to the schematic, I only get the package without the symbols.

 

I have uninstalled and reinstalled.

 

Any suggestions?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to autodeskguest

    I have found that if I open that library up and click on the schematic (at the top) and redraw the symbol (and save).

    Then open the library and select the symbol (on the left). It should come up and associate with the library. I had to

    redraw several library symbols. Some trashing of libraries occurs with updates.

     

    Yes, keep your libraries in a sub-folder -- you will have to use the "USE * " command line upon many re-entries to

    the program. (Sometimes it remembers = bonus). It is important to save off a copy of your "mylibrary" to somewhere

    else as often as you have made significant changes.

     

    I also have to often go and select individual libraries with the Library --> Use... command.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    Thanks for the information, guys... #1 The solution was to use the browse feature to identify the location of the new libraries... I had cut and pasted the addresses... Seems Eagle didn't like that...#2 I will have to rebuild the library that I created and identify it with the browse feature.

     

    I appreciate your help.

     

    t1d

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago

    On 29/10/2014 3:16 p.m., Tee Dunn wrote:

     

    #2) I have created a separate library folder for cataloging new

    items/packages that I build myself. I have created a new component with

    a package layer and a symbol layer. I have tied them to a device. I have

    tried to connect the symbol layer to the package layer, but they just

    won't connect. I can find this new device in the in the libraries, but

    when I add it to the schematic, I only get the package without the

    symbols.

     

    I have uninstalled and reinstalled.

     

    Any suggestions?

     

    The quickest way to a solution would be to upload your library so we can

    check it out.

     

    Warren

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago

    Tee Dunn wrote:

    OS=Win 8.1

     

     

    Only over my dead body could anyone ever install Win 8 on my PC image

     

     

     

    #1) I have downloaded several additional libraries and they are showing

    in the listing of libraries folders. I have also selected the "Use All"

    function to activate them... However, when searching the libraries for a

    device, these new libraries are not being included... That is to say, I

    know the device I am looking for is included in the new libraries, but

    the device that I want is not showing as an option in the search results

    to select to add on the schematic.

     

     

    That has been a problem with Eagle forever, that is easily "forgets"

    libraries. I am testing 7.1 right now and it does the same thing, ever

    since I tried a LTSpice export it only shows LTSpice libraries. You can

    get missing libraries back this way:

     

    Library -> Use -> look in the file and directory structure where they

    are, then highlight all the ones you want and click open.

     

    Quite likely you'll have to do that again the next time you steart Eagle.

     

     

    #2) I have created a separate library folder for cataloging new

    items/packages that I build myself. I have created a new component with

    a package layer and a symbol layer. I have tied them to a device. I have

    tried to connect the symbol layer to the package layer, but they just

    won't connect. I can find this new device in the in the libraries, but

    when I add it to the schematic, I only get the package without the

    symbols.

     

     

    That I'll have to leave to others to answer.

     

     

    I have uninstalled and reinstalled.

     

     

    Probably that keeps some sort of preference file.

     

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/