Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Changing signal names to pads on board
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 187 subscribers
  • Views 1723 views
  • Users 0 members are here
Related

Changing signal names to pads on board

autodeskguest
autodeskguest over 16 years ago

After duplicating a circuit many times (12), I am working on cleaning up

the inconsistencies (thank you Ing. J.M. Rafetseder for your Dec 7th

post on circuit duplication!).

 

At this point, the inconsistencies that remain are board trace

related.  There are a few common bus signals that are connected in the

schematic, but no traces were routed from the board pads prior to

duplication. To make the schematic and board consistent, the board

signal needs to be renamed the same as the schematic, but I am unable to

click and highlight on the pad with NAME, as there are no air wires

coming from the pad.

 

How can the signal on the board pad, with no air wires or connected

trace be renamed?

 

The alternative is to ignore the inconsistencies, and the overlap board

errors when connecting the pad with the appropriate trace???

 

Thanks

 

KR

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 16 years ago

    Olin,

     

    Thanks for the tip!

     

    Ken

     

     

     

    Olin Lathrop wrote:

    Ken wrote on Tue, 29 December 2009 10:30

    Turns out the solution was pretty simple.

    1. Add a wire (not route) on the appropriate layer near the pad needing

     

    an air wire connection to it.

    2. Rename the wire to the pad name, and an air wire is made.

     

    This technique also worked well to force an air wire to the center of a

     

    pad to thus provide for a clean routed trace: If the air wire is not on

     

    the pad center, add a wire, rename, and the rip it up.  An air wire is

     

    left behind, ready for the final routing operation.

     

    You can start routing at any point on a existing track by holding down CTRL

    while cliking there.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 16 years ago

    Olin,

     

    Thanks for the tip!

     

    Ken

     

     

     

    Olin Lathrop wrote:

    Ken wrote on Tue, 29 December 2009 10:30

    Turns out the solution was pretty simple.

    1. Add a wire (not route) on the appropriate layer near the pad needing

     

    an air wire connection to it.

    2. Rename the wire to the pad name, and an air wire is made.

     

    This technique also worked well to force an air wire to the center of a

     

    pad to thus provide for a clean routed trace: If the air wire is not on

     

    the pad center, add a wire, rename, and the rip it up.  An air wire is

     

    left behind, ready for the final routing operation.

     

    You can start routing at any point on a existing track by holding down CTRL

    while cliking there.