Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Layers in Standard (Hobbyist) Edition
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 188 subscribers
  • Views 1424 views
  • Users 0 members are here
  • 4_layer
  • layers
Related

Layers in Standard (Hobbyist) Edition

garylaoffice
garylaoffice over 11 years ago

I cannot manage to enable or select Route2, Route3, Route14 or Route15. My "About" shows I have the Standard Edition. It is my understanding that this version allows 6 signal layers, yet I can access only Top and Bottom.

 

Anyone know how I can enable the four inner layers?

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 11 years ago

    Am 16.12.2014 um 09:49 schrieb Rob Pearce:

    On 16/12/14 01:12, Gary La wrote:

    It has no mechanism to get past this. So that's the end of that

    schematic, I guess. Very unprofessional. No excuse for this type of

    behavior. A pro would've fixed the file with a placeholder or temporary

    tag so that the work could be recovered. Or at the very least, prompted

    the user to enter a value. Or opened the schematic but deleted the part

    associated with the fault. Or about 10 other things. But not this

    product -- end of schematic.

     

    Your faith in this mystical "pro" astonishes me. I've used Microsoft

    tools! And Orcad, and Matlab/Simulink, and all those other very

    expensive professional tools. None of them do any better at this than

    Eagle - most worse.

     

    You can accuse me of temper tantrums all you like - without the

    slightest justification, since you were the first to throw one - but it

    makes no difference to the fact that the holy grail you seem to expect

    from over-priced software does not exist in the real world. In my many

    years of using computer software the one thing I have absolutely found

    is that

     

         You DON'T get what you pay for

     

    You want a program that allows a recovery mechanism for a corrupted file

    (which clearly is what you had)? Use one with a plain text format

    (Eagle's is now XML, which isn't perfect but...) and/or open source.

    Yes, that's right, the most likely programs to survive bad files are the

    FREE ones!

     

     

    Bob, Morten and others imho you should stop the discussion.

    You are just feeding a troll.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • garylaoffice
    garylaoffice over 11 years ago in reply to autodeskguest

    I fixed it myself by digging into the XML file.

     

    The group function and cut-to-clipboard need to be streamlined.

     

    Often clicking on objects with the anticipation that the currently-selected part will be affected by the currently-selected operation often yields no action. For example: move. Clicking on an object and dragging usually fixes the object to the mouse and the move is performed. But very often it only highlights the object.

     

    The library manager needs to be completely rewritten. It's a disaster.

     

    I will agree that most CAD/PCB programs are grossly over-priced. However, when I use the library manager in Eagle, I desperately wish I was using my over-priced tools.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • garylaoffice
    garylaoffice over 11 years ago in reply to autodeskguest

    I fixed it myself by digging into the XML file.

     

    The group function and cut-to-clipboard need to be streamlined.

     

    Often clicking on objects with the anticipation that the currently-selected part will be affected by the currently-selected operation often yields no action. For example: move. Clicking on an object and dragging usually fixes the object to the mouse and the move is performed. But very often it only highlights the object.

     

    The library manager needs to be completely rewritten. It's a disaster.

     

    I will agree that most CAD/PCB programs are grossly over-priced. However, when I use the library manager in Eagle, I desperately wish I was using my over-priced tools.