EAGLE User Chat (English) gerbv, the free and opensrc gerber viewer
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
  • Replies 11 replies
  • Subscribers 180 subscribers
  • Views 2743 views
  • Users 0 members are here
Related

gerbv, the free and opensrc gerber viewer

autodeskguest
autodeskguest over 16 years ago

Not all of you may know this, but I found this free open source gerber

viewer that seems to work nice.

http://gerbv.gpleda.org/index.html

 

From the overview:

-Gerbv is a viewer for Gerber RS-274X files, Excellon drill files, and CSV

pick-and-place files.

-Gerbv is a native Linux application, and it runs on many common unix

platforms.

-Gerbv is free/ open-source software.

-You may download the source code from this page.

-The core functionality of gerbv is located in a separate library

(libgerbv), allowing developers to include Gerber

parsing/editing/exporting/rendering into other programs. Documentation for

libgerbv is here.

-Gerbv is one of the utilities affiliated with the gEDA project, an umbrella

organization dedicated to producing free software tools for electronic

design.

-The latest official gerbv release is version 2.3.0, released on 2009-07-11.

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 16 years ago

    On 1/8/10 9:05 AM, James Morrison wrote:

    And for all the Mac users out there, I recently got gerbv running on my

    Intel Mac using a package called fink. The version I have has an older

    version of gerbv but I think I saw that the latest fink has 2.3 of gerbv.

     

    I second the use of gerbv (also available from MacPorts on Mac) and

    GC-Prevue for Windows.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 16 years ago

    On 1/8/10 9:05 AM, James Morrison wrote:

    And for all the Mac users out there, I recently got gerbv running on my

    Intel Mac using a package called fink. The version I have has an older

    version of gerbv but I think I saw that the latest fink has 2.3 of gerbv.

     

    I second the use of gerbv (also available from MacPorts on Mac) and

    GC-Prevue for Windows.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • autodeskguest
    autodeskguest over 16 years ago in reply to Former Member

    Andrew Sterian wrote on Fri, 08 January 2010 10:02

    On 1/8/10 9:05 AM, James Morrison wrote:

    And for all the Mac users out there, I recently got gerbv running

    on my

    Intel Mac using a package called fink. The version I have has an

    older

    version of gerbv but I think I saw that the latest fink has 2.3 of

    gerbv.

     

    I second the use of gerbv (also available from MacPorts on Mac) and

    GC-Prevue for Windows.

     

     

    Thanks for the MacPorts hint.  I think I'll try that out.

     

    If anyone is involved with the gerbv development, it would be highly useful

    to have the layer manipulation buttons to turn all layers ON or OFF and to

    toggle all layer visibility.  ViewMate has these and I use them all the

    time.  Usually I am looking at one layer relative to another.  So the first

    thing I do is turn them all OFF then turn on a specific layer.  In gerbv, I

    have to uncheck every layer first to get to a blank slate.  With a 10 layer

    board that is a lot of checking.

     

    Cheers,

     

    James.

     

    --

    James Morrison  ~~~  Stratford Digital

     

    email:  james@eaglecentral.ca

    web: http://www.eaglecentral.ca

     

    Specialising in CadSoft EAGLE

    • Online Sales to North America

    • Electronic Design Services

    • EAGLE Enterprise Toolkit

    --

    Browser access to CadSoft Support Forums at http://www.eaglecentral.ca

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 16 years ago in reply to Former Member

    Andrew Sterian wrote on Fri, 08 January 2010 10:02

    I second the use of gerbv (also available from MacPorts on Mac) and

    GC-Prevue for Windows.

     

     

    I was using GC-Prevue for years. I was fed up last year. They keep pushing

    upgrades on me for no reason whatsoever. I was quite content with the free

    version from around 2003, and I don't need all the latest additions.

     

    Plus it was a bit of pain to load drill files with a separate tool rack

    file.

     

    Now I use ViewMate, which of course sucks in comparison, but is enough for

    what I need. And I don't have to reinstall it every couple of month as with

    GCPrevue.

     

    --

    Browser access to CadSoft Support Forums at http://www.eaglecentral.ca