Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Preferred power supply connections?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 188 subscribers
  • Views 1983 views
  • Users 0 members are here
Related

Preferred power supply connections?

e14 Contributor
e14 Contributor over 16 years ago

The schematic I am "capturing" are based on public domain circuits for

audio processing modules in a modular analog synthesizer. There are some

standard power connection schemes which I intend to follow consisting of

+/- 15 Vdc and ground. Typically, the +/- supplies go through a ferrite

bead and a couple of filtering capacitors before hitting the PCB's power

nets.

 

What is the best way to make a power net for the PCB components bcause it

is separated from the power input jack by the ferrite bead? If I connect

the connector pins to the supply +15 and -15 nets, I can't use them on the

PCB. So, what is the best net to use to PCB components to the other side of

the ferrite beads? Should use one of the other available supply nets or

make a unique power net?

 

I have played with different ways to do it, and they seem to work, but as

I'm new at this capture stuff, I'd like to know if there are standard or

preferred ways to accomplish this.

 

This image kind of shows what I mean.

 

Thanks

David

 

 

 

--

Browser access to CadSoft Support Forums at http://www.eaglecentral.ca

 

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 16 years ago

    dingebre wrote on Wed, 24 February 2010 21:57

    The schematic I am "capturing" are based on public domain circuits for

    audio processing modules in a modular analog synthesizer. There are some

    standard power connection schemes which I intend to follow consisting of

    +/- 15 Vdc and ground. Typically, the +/- supplies go through a ferrite

    bead and a couple of filtering capacitors before hitting the PCB's power

    nets.

     

    What is the best way to make a power net for the PCB components bcause

    it is separated from the power input jack by the ferrite bead? If I

    connect the connector pins to the supply +15 and -15 nets, I can't use

    them on the PCB. So, what is the best net to use to PCB components to the

    other side of the ferrite beads? Should use one of the other available

    supply nets or make a unique power net?

     

    I have played with different ways to do it, and they seem to work, but

    as I'm new at this capture stuff, I'd like to know if there are standard

    or preferred ways to accomplish this.

     

    This image kind of shows what I mean.

     

     

    Hi David,

     

    There are a few ways to do it.  First, every signal name in EAGLE is

    global.  So if you simply name a net to a signal name it will be connected

    to any other net with the same name whether it looks like it or not.  So

    watch yourself there.

     

    So you have a pin connected to a ferrite that goes to a plane then you can

    do a few things:

     

    1)  name (and label) the net between the pin and the ferrite.  That can be

    helpful.

     

    2)  create a custom supply symbol that indicates  it's function.  This can

    work too and can help with readability if that net goes somewhere else

    (like a raw power bus).

     

    My rule is that I should be able to tell 100% what is happening in the

    schematic when I print it out.  If you have to use EAGLE itself (by using

    the info command for instance) to figure out what is going on then the

    schematic is incomplete.

     

    I also have a preference for labels over spaghetti nets that are hard to

    follow when printed out.  Hope that helps.

     

    Cheers,

     

    James.

    --

    James Morrison  ~~~  Stratford Digital

     

    email:  james@eaglecentral.ca

    web: http://www.eaglecentral.ca

     

    Specializing in CadSoft EAGLE

    • Online Sales to North America

    • Electronic Design Services

    • EAGLE Enterprise Toolkit

    --

    Browser access to CadSoft Support Forums at http://www.eaglecentral.ca

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to autodeskguest

    James Morrison wrote on Thu, 25 February 2010 09:52

    dingebre wrote on Wed, 24 February 2010 21:57

    The schematic I am "capturing" are based on public domain circuits

    for audio processing modules in a modular analog synthesizer. There are

    some standard power connection schemes which I intend to follow

    consisting of +/- 15 Vdc and ground. Typically, the +/- supplies go

    through a ferrite bead and a couple of filtering capacitors before

    hitting the PCB's power nets.

     

    What is the best way to make a power net for the PCB components

    bcause it is separated from the power input jack by the ferrite bead?

    If I connect the connector pins to the supply +15 and -15 nets, I can't

    use them on the PCB. So, what is the best net to use to PCB components

    to the other side of the ferrite beads? Should use one of the other

    available supply nets or make a unique power net?

     

    I have played with different ways to do it, and they seem to work,

    but as I'm new at this capture stuff, I'd like to know if there are

    standard or preferred ways to accomplish this.

     

    This image kind of shows what I mean.

     

    Hi David,

     

    There are a few ways to do it.  First, every signal name in EAGLE is

    global.  So if you simply name a net to a signal name it will be

    connected to any other net with the same name whether it looks like it or

    not.  So watch yourself there.

     

    So you have a pin connected to a ferrite that goes to a plane then you

    can do a few things:

     

    1)  name (and label) the net between the pin and the ferrite.  That can

    be helpful.

     

    2)  create a custom supply symbol that indicates  it's function.  This

    can work too and can help with readability if that net goes somewhere

    else (like a raw power bus).

     

    My rule is that I should be able to tell 100% what is happening in the

    schematic when I print it out.  If you have to use EAGLE itself (by using

    the info command for instance) to figure out what is going on then the

    schematic is incomplete.

     

    I also have a preference for labels over spaghetti nets that are hard

    to follow when printed out.  Hope that helps.

     

    Cheers,

     

    James.

     

     

    Yes, it helps a lot. Thanks James. In the software I have been using

    (competing commercial application), it was a real chore to do this kind of

    connection and I was a litte nervous as it seems so easy to do in Eagle image

    I wanted to make sure I wasn't missing something.

     

    David

    --

    Browser access to CadSoft Support Forums at http://www.eaglecentral.ca

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to autodeskguest

    James Morrison wrote on Thu, 25 February 2010 09:52

    dingebre wrote on Wed, 24 February 2010 21:57

    The schematic I am "capturing" are based on public domain circuits

    for audio processing modules in a modular analog synthesizer. There are

    some standard power connection schemes which I intend to follow

    consisting of +/- 15 Vdc and ground. Typically, the +/- supplies go

    through a ferrite bead and a couple of filtering capacitors before

    hitting the PCB's power nets.

     

    What is the best way to make a power net for the PCB components

    bcause it is separated from the power input jack by the ferrite bead?

    If I connect the connector pins to the supply +15 and -15 nets, I can't

    use them on the PCB. So, what is the best net to use to PCB components

    to the other side of the ferrite beads? Should use one of the other

    available supply nets or make a unique power net?

     

    I have played with different ways to do it, and they seem to work,

    but as I'm new at this capture stuff, I'd like to know if there are

    standard or preferred ways to accomplish this.

     

    This image kind of shows what I mean.

     

    Hi David,

     

    There are a few ways to do it.  First, every signal name in EAGLE is

    global.  So if you simply name a net to a signal name it will be

    connected to any other net with the same name whether it looks like it or

    not.  So watch yourself there.

     

    So you have a pin connected to a ferrite that goes to a plane then you

    can do a few things:

     

    1)  name (and label) the net between the pin and the ferrite.  That can

    be helpful.

     

    2)  create a custom supply symbol that indicates  it's function.  This

    can work too and can help with readability if that net goes somewhere

    else (like a raw power bus).

     

    My rule is that I should be able to tell 100% what is happening in the

    schematic when I print it out.  If you have to use EAGLE itself (by using

    the info command for instance) to figure out what is going on then the

    schematic is incomplete.

     

    I also have a preference for labels over spaghetti nets that are hard

    to follow when printed out.  Hope that helps.

     

    Cheers,

     

    James.

     

     

    Yes, it helps a lot. Thanks James. In the software I have been using

    (competing commercial application), it was a real chore to do this kind of

    connection and I was a litte nervous as it seems so easy to do in Eagle image

    I wanted to make sure I wasn't missing something.

     

    David

    --

    Browser access to CadSoft Support Forums at http://www.eaglecentral.ca