Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Preferred power supply connections?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 188 subscribers
  • Views 1984 views
  • Users 0 members are here
Related

Preferred power supply connections?

e14 Contributor
e14 Contributor over 16 years ago

The schematic I am "capturing" are based on public domain circuits for

audio processing modules in a modular analog synthesizer. There are some

standard power connection schemes which I intend to follow consisting of

+/- 15 Vdc and ground. Typically, the +/- supplies go through a ferrite

bead and a couple of filtering capacitors before hitting the PCB's power

nets.

 

What is the best way to make a power net for the PCB components bcause it

is separated from the power input jack by the ferrite bead? If I connect

the connector pins to the supply +15 and -15 nets, I can't use them on the

PCB. So, what is the best net to use to PCB components to the other side of

the ferrite beads? Should use one of the other available supply nets or

make a unique power net?

 

I have played with different ways to do it, and they seem to work, but as

I'm new at this capture stuff, I'd like to know if there are standard or

preferred ways to accomplish this.

 

This image kind of shows what I mean.

 

Thanks

David

 

 

 

--

Browser access to CadSoft Support Forums at http://www.eaglecentral.ca

 

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 16 years ago

    Olin wrote on Thu, 25 February 2010 07:16

    dingebre wrote on Wed, 24 February 2010 21:57

    This image kind of shows what I mean.

     

    No, it shows a mess.  There is rotated text all over the place, labels

    overlapping other labels and parts, and missing values.  If you don't

    care about your design, there is no reason I should either.

     

     

    Hi Olin, you're reading too much into the "design". This is not a real

    schematic.

     

    I'm only illustrating the power connections. I am showing the +/-15 volts

    to the plug, and one way I was thinking to do the other power nets. I don't

    even know if this design is electrically "real" image

     

    I only ask a little patience. I'm very new to using Eagle and want to learn

    good habits. Would you maybe take a second look? I'd like some advice about

    how to handle the power nets on the "real" circuits I'd like to work on.

     

    Should I do it kind of like in that illustration? Use the supply library

    +/- 15 for the plug and then a generic supply symbol to connect the +/-

    supplies on the components? Or is there a better way?

     

    Thanks for looking Olin.

     

    David

    --

    Browser access to CadSoft Support Forums at http://www.eaglecentral.ca

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 16 years ago in reply to e14 Contributor

    dingebre wrote on Thu, 25 February 2010 11:42

    Hi Olin, you're reading too much into the "design". This is not a real

    schematic.

     

    I'm only illustrating the power connections.

     

    It is still a good idea to keep in mind that neatness counts, especially

    when you are presenting to others.  Some may look past that, but why allow

    it to be a issue when it would only have taken a extra minute to make

    things more readable?

     

    Quote:

    I only ask a little patience. I'm very new to using Eagle and want to

    learn good habits. Would you maybe take a second look? I'd like some

    advice about how to handle the power nets on the "real" circuits I'd like

    to work on.

     

    I don't use specific parts at all to label power nets.  I don't treat power

    nets any different from other nets that are drawn in separate pieces,

    although I've seen others use explicit power symbols commonly.  In Eagle,

    nets in the schematic are automatically connected if they have the same

    name.  To show airwires in a Eagle schematic, I name the nets and then use

    DRAW LABEL to show the net name in the schematic.  It's important to use

    DRAW LABEL instead of TEXT because DRAW LABEL shows the true net name as

    Eagle understands it.  If you change the net name, the text drawn with DRAW

    LABEL will automatically change.

     

    For power nets I use names like "5V", "-12V", "BATT", or whatever I think

    will be most descriptive in context of that schematic.  I also like to show

    power connections on top, ground on the bottom, with signal from left to

    right to the extent this can be reasonably done.  Keep in mind that the

    schematic is not only to define the machine readable connections to Eagle,

    but it is also the primary documentation of your circuit to humans.  As

    such, neatness and clarity are very important considerations.

     

    Quote:

    Should I do it kind of like in that illustration? Use the supply

    library  +/- 15 for the plug and then a generic supply symbol to connect

    the +/- supplies on the components? Or is there a better way?

     

    You'll probably find as many opinions as people.  There are several

    reasonably "right" ways.  I've tried to explain what I do, but I recognize

    there are other ways that others prefer.  As long as Eagle understands the

    connections, there aren't hidden gotchas for making changes, and your

    circuit is easy to understand from the schematic, then it's a acceptable

    method.

     

    You can take a look at http://www.embedinc.com/products/usbprog/eusb3.pdf

    as a example of how I do things.  The first page is the main power supply.

    Note all the named wires ending at the right side because the logical flow

    is out from the power supply.  You can see various other places in the

    schematic that connect to these power rails, usually coming in from the top

    or left as a simple visual reference that the power is coming in instead of

    being produced there.  Note that no explicit power symbols were used, just

    named nets with carefully placed labels.

    --

    Browser access to CadSoft Support Forums at http://www.eaglecentral.ca

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 16 years ago in reply to e14 Contributor

    dingebre wrote on Thu, 25 February 2010 11:42

    Hi Olin, you're reading too much into the "design". This is not a real

    schematic.

     

    I'm only illustrating the power connections.

     

    It is still a good idea to keep in mind that neatness counts, especially

    when you are presenting to others.  Some may look past that, but why allow

    it to be a issue when it would only have taken a extra minute to make

    things more readable?

     

    Quote:

    I only ask a little patience. I'm very new to using Eagle and want to

    learn good habits. Would you maybe take a second look? I'd like some

    advice about how to handle the power nets on the "real" circuits I'd like

    to work on.

     

    I don't use specific parts at all to label power nets.  I don't treat power

    nets any different from other nets that are drawn in separate pieces,

    although I've seen others use explicit power symbols commonly.  In Eagle,

    nets in the schematic are automatically connected if they have the same

    name.  To show airwires in a Eagle schematic, I name the nets and then use

    DRAW LABEL to show the net name in the schematic.  It's important to use

    DRAW LABEL instead of TEXT because DRAW LABEL shows the true net name as

    Eagle understands it.  If you change the net name, the text drawn with DRAW

    LABEL will automatically change.

     

    For power nets I use names like "5V", "-12V", "BATT", or whatever I think

    will be most descriptive in context of that schematic.  I also like to show

    power connections on top, ground on the bottom, with signal from left to

    right to the extent this can be reasonably done.  Keep in mind that the

    schematic is not only to define the machine readable connections to Eagle,

    but it is also the primary documentation of your circuit to humans.  As

    such, neatness and clarity are very important considerations.

     

    Quote:

    Should I do it kind of like in that illustration? Use the supply

    library  +/- 15 for the plug and then a generic supply symbol to connect

    the +/- supplies on the components? Or is there a better way?

     

    You'll probably find as many opinions as people.  There are several

    reasonably "right" ways.  I've tried to explain what I do, but I recognize

    there are other ways that others prefer.  As long as Eagle understands the

    connections, there aren't hidden gotchas for making changes, and your

    circuit is easy to understand from the schematic, then it's a acceptable

    method.

     

    You can take a look at http://www.embedinc.com/products/usbprog/eusb3.pdf

    as a example of how I do things.  The first page is the main power supply.

    Note all the named wires ending at the right side because the logical flow

    is out from the power supply.  You can see various other places in the

    schematic that connect to these power rails, usually coming in from the top

    or left as a simple visual reference that the power is coming in instead of

    being produced there.  Note that no explicit power symbols were used, just

    named nets with carefully placed labels.

    --

    Browser access to CadSoft Support Forums at http://www.eaglecentral.ca